Matter Wi-Fi Direct Internet Connectivity#
Direct Internet Connectivity (DIC) is a Silicon Labs-only feature to connect Matter devices to proprietary cloud solutions (AWS,GCP,APPLE ...) directly. As such, a Matter Wi-Fi device must support connecting locally on the Matter Fabric, via IPv6, and connecting to the Internet via IPv4.
Matter devices can be controlled by chip-tool or controller and the respective status of the attribute modified will be published to the cloud.
Remote user can install the cloud specific application to get the notifications on the attribute status and to control the device.
Feature Design#


End-to-End Set-Up Bring Up#
Message Queuing Telemetry Transport (MQTT)#
MQTT is an OASIS standard messaging protocol for the Internet of Things (IoT). It is designed as an extremely lightweight publish/subscribe messaging transport that is ideal for connecting remote devices with a small code footprint and minimal network bandwidth. Refer https://mqtt.org/ for more details
Configuring the MQTT server#
To set up and configure AWS or Mosquitto for DIC support see the following documentation:
Remote User Setup (MQTT Explorer)#
A remote user is used to check the state of device. In this context MQTT explorer is used as a remote user.
MQTT explorer setup and configuration
DUT Setup#
Software and Hardware prerequisites for working with Silicon Labs Matter:
Use the build command for DIC instead of the normal build command in the Software Setup documentation.
End-to-End Test of DIC Application#
User Setup (MQTT Explorer):
Sharing status of device to cloud
End-to-end command to be executed from chip-tool, refer Running the Matter Demo on EFR32 hosts
Below is the application specific attribute/s information or state shared to the cloud through Direct Internet Connectivity Solution
For Lighting App, On/Off Attributes
For Lock App, lock/unlock Attributes
For Windows App, lift/tilt Attributes
For Thermostat App, SystemMode/CurrentTemp/LocalTemperature/OccupiedCoolingSetpoint/OccupiedHeatingSetpoint Attributes
For On/off Plug App, On/Off Attributes
Application status would be updated on the mqtt_explorer UI, as shown in below image.


Control of the device through cloud interface
Make sure matter device is up and commissioned successfully, refer Running the Matter Demo on EFR32 hosts
For Controlling the device, set topic name and the commands to be executed in the mqtt_explorer for below applications.
Lighting App
Topic: command
Commands:
toggle
on
off
Onoff-plug App
Topic: command
Commands:
toggle
on
off
Lock App
Topic: command
Commands:
lock
unlock
Thermostat App
Topic: command
Commands:
SetMode/value(value need to provide 1,2,3,4 ex:SetMode/1)
Heating/value(value need to provide 2500,2600 ex:HeatingSetPoint/2500)
Cooling/value(value need to provide 2500,2600 ex:CoolingSetPoint/2500)
Then click
publishbutton to execute the command.

Download AWS OTA Image through cloud interface
Make sure matter device is up and commissioned successfully, refer Running the Matter Demo on EFR32 hosts
Make sure device is connected to MQTT Server successfully.
Then Create a AWS OTA Job in the AWS Website, refer How to create AWS OTA JOB
Trigger OTA Command through MQTT Explorer like below.
Then click
publishbutton to execute the AWS OTA command.