GPIO_TypeDef Struct ReferenceDevices > GPIO
GPIO Register Declaration
Definition at line 49
of file efm32pg1b_gpio.h
.
#include <
efm32pg1b_gpio.h
>
Data Fields | |
__IOM uint32_t | EM4WUEN |
__IOM uint32_t | EXTIFALL |
__IOM uint32_t | EXTILEVEL |
__IOM uint32_t | EXTIPINSELH |
__IOM uint32_t | EXTIPINSELL |
__IOM uint32_t | EXTIPSELH |
__IOM uint32_t | EXTIPSELL |
__IOM uint32_t | EXTIRISE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INSENSE |
__IOM uint32_t | LOCK |
GPIO_P_TypeDef | P [6] |
uint32_t | RESERVED0 [184] |
uint32_t | RESERVED1 [4] |
uint32_t | RESERVED2 [2] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTEPEN |
Field Documentation
__IOM uint32_t GPIO_TypeDef::EM4WUEN |
EM4 Wake Up Enable Register
Definition at line 64
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIFALL |
External Interrupt Falling Edge Trigger Register
Definition at line 58
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTILEVEL |
External Interrupt Level Register
Definition at line 59
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPINSELH |
External Interrupt Pin Select High Register
Definition at line 56
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPINSELL |
External Interrupt Pin Select Low Register
Definition at line 55
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPSELH |
External Interrupt Port Select High Register
Definition at line 54
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPSELL |
External Interrupt Port Select Low Register
Definition at line 53
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIRISE |
External Interrupt Rising Edge Trigger Register
Definition at line 57
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IEN |
Interrupt Enable Register
Definition at line 63
of file efm32pg1b_gpio.h
.
__IM uint32_t GPIO_TypeDef::IF |
Interrupt Flag Register
Definition at line 60
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 62
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 61
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::INSENSE |
Input Sense Register
Definition at line 71
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::LOCK |
Configuration Lock Register
Definition at line 72
of file efm32pg1b_gpio.h
.
GPIO_P_TypeDef GPIO_TypeDef::P[6] |
Port configuration bits
Definition at line 50
of file efm32pg1b_gpio.h
.
uint32_t GPIO_TypeDef::RESERVED0[184] |
Reserved for future use
Definition at line 52
of file efm32pg1b_gpio.h
.
uint32_t GPIO_TypeDef::RESERVED1[4] |
Reserved for future use
Definition at line 66
of file efm32pg1b_gpio.h
.
uint32_t GPIO_TypeDef::RESERVED2[2] |
Reserved for future use
Definition at line 70
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 68
of file efm32pg1b_gpio.h
.
__IOM uint32_t GPIO_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 67
of file efm32pg1b_gpio.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG1B/Include/
efm32pg1b_gpio.h