LETIMER_TypeDef Struct ReferenceDevices > LETIMER

LETIMER Register Declaration

Definition at line 49 of file efm32pg1b_letimer.h .

#include < efm32pg1b_letimer.h >

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CNT
__IOM uint32_t COMP0
__IOM uint32_t COMP1
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t PRSSEL
__IOM uint32_t REP0
__IOM uint32_t REP1
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [2]
uint32_t RESERVED2 [2]
__IOM uint32_t ROUTELOC0
__IOM uint32_t ROUTEPEN
__IM uint32_t STATUS
__IM uint32_t SYNCBUSY

Field Documentation

__IOM uint32_t LETIMER_TypeDef::CMD

Command Register

Definition at line 51 of file efm32pg1b_letimer.h .

Referenced by LETIMER_Enable() , LETIMER_Init() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::CNT

Counter Value Register

Definition at line 53 of file efm32pg1b_letimer.h .

Referenced by LETIMER_CounterGet() .

__IOM uint32_t LETIMER_TypeDef::COMP0

Compare Value Register 0

Definition at line 54 of file efm32pg1b_letimer.h .

Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::COMP1

Compare Value Register 1

Definition at line 55 of file efm32pg1b_letimer.h .

Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32pg1b_letimer.h .

Referenced by LETIMER_Init() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 61 of file efm32pg1b_letimer.h .

Referenced by LETIMER_IntDisable() , LETIMER_IntEnable() , LETIMER_IntGetEnabled() , and LETIMER_Reset() .

__IM uint32_t LETIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 58 of file efm32pg1b_letimer.h .

Referenced by LETIMER_IntGet() , and LETIMER_IntGetEnabled() .

__IOM uint32_t LETIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 60 of file efm32pg1b_letimer.h .

Referenced by LETIMER_IntClear() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 59 of file efm32pg1b_letimer.h .

Referenced by LETIMER_IntSet() .

__IOM uint32_t LETIMER_TypeDef::PRSSEL

PRS Input Select Register

Definition at line 71 of file efm32pg1b_letimer.h .

__IOM uint32_t LETIMER_TypeDef::REP0

Repeat Counter Register 0

Definition at line 56 of file efm32pg1b_letimer.h .

Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::REP1

Repeat Counter Register 1

Definition at line 57 of file efm32pg1b_letimer.h .

Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .

uint32_t LETIMER_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 63 of file efm32pg1b_letimer.h .

uint32_t LETIMER_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 66 of file efm32pg1b_letimer.h .

uint32_t LETIMER_TypeDef::RESERVED2[2]

Reserved for future use

Definition at line 70 of file efm32pg1b_letimer.h .

__IOM uint32_t LETIMER_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 68 of file efm32pg1b_letimer.h .

__IOM uint32_t LETIMER_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 67 of file efm32pg1b_letimer.h .

__IM uint32_t LETIMER_TypeDef::STATUS

Status Register

Definition at line 52 of file efm32pg1b_letimer.h .

Referenced by LETIMER_Init() .

__IM uint32_t LETIMER_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 64 of file efm32pg1b_letimer.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG1B/Include/ efm32pg1b_letimer.h