ACMP_CapsenseInit_TypeDef Struct ReferenceEMLIB > ACMP

Capsense initialization structure.

Definition at line 525 of file em_acmp.h.

#include <em_acmp.h>

Data Fields

uint32_t biasProg
 
bool enable
 
bool fullBias
 
ACMP_HysteresisLevel_TypeDef hysteresisLevel_0
 
ACMP_HysteresisLevel_TypeDef hysteresisLevel_1
 
ACMP_CapsenseResistor_TypeDef resistor
 
uint32_t vddLevelHigh
 
uint32_t vddLevelLow
 

Field Documentation

uint32_t ACMP_CapsenseInit_TypeDef::biasProg

Bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 538 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

bool ACMP_CapsenseInit_TypeDef::enable

If true, ACMP is being enabled after configuration.

Definition at line 592 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

bool ACMP_CapsenseInit_TypeDef::fullBias

Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 528 of file em_acmp.h.

Referenced by ACMP_CapsenseInit(), and CAPLESENSE_setupACMP().

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_0

Hysteresis level when ACMP output is 0

Definition at line 551 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_1

Hysteresis level when ACMP output is 1

Definition at line 554 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor

Resistor used in the capacative sensing circuit. For values see your device datasheet.

Definition at line 559 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

uint32_t ACMP_CapsenseInit_TypeDef::vddLevelHigh

This value configures the upper voltage threshold of the capsense oscillation rail.

The voltage threshold is calculated as Vdd * (vddLevelHigh + 1) / 64

Definition at line 579 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().

uint32_t ACMP_CapsenseInit_TypeDef::vddLevelLow

This value configures the lower voltage threshold of the capsense oscillation rail.

The voltage threshold is calculated as Vdd * (vddLevelLow + 1) / 64

Definition at line 588 of file em_acmp.h.

Referenced by ACMP_CapsenseInit().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_acmp.h