SMU_Init_TypeDef Struct ReferenceEMLIB > SMU
SMU initialization structure.
Definition at line 588
of file em_smu.h
.
#include <
em_smu.h
>
Data Fields | |
bool | enable |
union { | |
SMU_PrivilegedAccess_TypeDef access | |
uint32_t reg [2] | |
} | ppu |
Field Documentation
SMU_PrivilegedAccess_TypeDef SMU_Init_TypeDef::access |
Periperal access control array.
Definition at line 591
of file em_smu.h
.
bool SMU_Init_TypeDef::enable |
SMU enable flag, when set SMU_Init() will enable SMU.
Definition at line 593
of file em_smu.h
.
Referenced by SMU_Init().
uint32_t SMU_Init_TypeDef::reg[2] |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_smu.h