ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line
636
of file
em_acmp.h
.
#include <
em_acmp.h
>
Field Documentation
ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
Definition at line
667
of file
em_acmp.h
.
Referenced by ACMP_Init() .
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line
649
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::enable |
If true, ACMP is being enabled after configuration.
Definition at line
714
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::fullBias |
Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
639
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0 |
Hysteresis when ACMP output is 0
Definition at line
686
of file
em_acmp.h
.
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1 |
Hysteresis when ACMP output is 1
Definition at line
689
of file
em_acmp.h
.
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by the ACMP during warmup
Definition at line
699
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range. Adjust this setting to optimize the performance for a given input voltage range.
Definition at line
660
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on falling edge
Definition at line
652
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on rising edge
Definition at line
655
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource |
Select the power source for the ACMP.
Definition at line
672
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput |
VLP Input source. Select between using VADIV or VBDIV as the VLP source.
Definition at line
695
of file
em_acmp.h
.
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_acmp.h