PCNTEMLIB

Detailed Description

Pulse Counter (PCNT) Peripheral API.

This module contains functions to control the PCNT peripheral of Silicon Labs 32-bit MCUs and SoCs. The PCNT decodes incoming pulses. The module has a quadrature mode which may be used to decode the speed and direction of a mechanical shaft.

Data Structures

struct PCNT_Filter_TypeDef
struct PCNT_Init_TypeDef
struct PCNT_TCC_TypeDef

Macros

#define PCNT0_CNT_SIZE (16) /* PCNT0 counter is 16 bits. */
#define PCNT_FILTER_DEFAULT
#define PCNT_INIT_DEFAULT
#define PCNT_TCC_DEFAULT

Enumerations

enum PCNT_CntEvent_TypeDef {
pcntCntEventBoth = _PCNT_CTRL_CNTEV_BOTH,
pcntCntEventUp = _PCNT_CTRL_CNTEV_UP,
pcntCntEventDown = _PCNT_CTRL_CNTEV_DOWN,
pcntCntEventNone = _PCNT_CTRL_CNTEV_NONE
}
enum PCNT_Mode_TypeDef {
pcntModeDisable = _PCNT_CTRL_MODE_DISABLE,
pcntModeOvsSingle = _PCNT_CTRL_MODE_OVSSINGLE,
pcntModeExtSingle = _PCNT_CTRL_MODE_EXTCLKSINGLE,
pcntModeExtQuad = _PCNT_CTRL_MODE_EXTCLKQUAD,
pcntModeOvsQuad1 = _PCNT_CTRL_MODE_OVSQUAD1X,
pcntModeOvsQuad2 = _PCNT_CTRL_MODE_OVSQUAD2X,
pcntModeOvsQuad4 = _PCNT_CTRL_MODE_OVSQUAD4X
}
enum PCNT_PRSInput_TypeDef {
pcntPRSInputS0 = 0,
pcntPRSInputS1 = 1
}
enum PCNT_PRSSel_TypeDef {
pcntPRSCh0 = 0,
pcntPRSCh1 = 1,
pcntPRSCh2 = 2,
pcntPRSCh3 = 3,
pcntPRSCh4 = 4,
pcntPRSCh5 = 5,
pcntPRSCh6 = 6,
pcntPRSCh7 = 7,
pcntPRSCh8 = 8,
pcntPRSCh9 = 9,
pcntPRSCh10 = 10,
pcntPRSCh11 = 11
}
enum PCNT_TCCComp_Typedef {
tccCompLTOE = _PCNT_CTRL_TCCCOMP_LTOE,
tccCompGTOE = _PCNT_CTRL_TCCCOMP_GTOE,
tccCompRange = _PCNT_CTRL_TCCCOMP_RANGE
}
enum PCNT_TCCMode_TypeDef {
tccModeDisabled = _PCNT_CTRL_TCCMODE_DISABLED,
tccModeLFA = _PCNT_CTRL_TCCMODE_LFA,
tccModePRS = _PCNT_CTRL_TCCMODE_PRS
}
enum PCNT_TCCPresc_Typedef {
tccPrescDiv1 = _PCNT_CTRL_TCCPRESC_DIV1,
tccPrescDiv2 = _PCNT_CTRL_TCCPRESC_DIV2,
tccPrescDiv4 = _PCNT_CTRL_TCCPRESC_DIV4,
tccPrescDiv8 = _PCNT_CTRL_TCCPRESC_DIV8
}

Functions

__STATIC_INLINE uint32_t PCNT_AuxCounterGet ( PCNT_TypeDef *pcnt)
Get auxiliary counter value.
__STATIC_INLINE uint32_t PCNT_CounterGet ( PCNT_TypeDef *pcnt)
Get pulse counter value.
void PCNT_CounterReset ( PCNT_TypeDef *pcnt)
Reset PCNT counters and TOP register.
__STATIC_INLINE void PCNT_CounterSet ( PCNT_TypeDef *pcnt, uint32_t count)
Set counter value.
void PCNT_CounterTopSet ( PCNT_TypeDef *pcnt, uint32_t count, uint32_t top)
Set counter and top values.
void PCNT_Enable ( PCNT_TypeDef *pcnt, PCNT_Mode_TypeDef mode)
Set PCNT operational mode.
void PCNT_FilterConfiguration ( PCNT_TypeDef *pcnt, const PCNT_Filter_TypeDef *config, bool enable)
Set filter configuration.
void PCNT_FreezeEnable ( PCNT_TypeDef *pcnt, bool enable)
PCNT register synchronization freeze control.
void PCNT_Init ( PCNT_TypeDef *pcnt, const PCNT_Init_TypeDef *init)
Init pulse counter.
__STATIC_INLINE void PCNT_IntClear ( PCNT_TypeDef *pcnt, uint32_t flags)
Clear one or more pending PCNT interrupts.
__STATIC_INLINE void PCNT_IntDisable ( PCNT_TypeDef *pcnt, uint32_t flags)
Disable one or more PCNT interrupts.
__STATIC_INLINE void PCNT_IntEnable ( PCNT_TypeDef *pcnt, uint32_t flags)
Enable one or more PCNT interrupts.
__STATIC_INLINE uint32_t PCNT_IntGet ( PCNT_TypeDef *pcnt)
Get pending PCNT interrupt flags.
__STATIC_INLINE uint32_t PCNT_IntGetEnabled ( PCNT_TypeDef *pcnt)
Get enabled and pending PCNT interrupt flags.
__STATIC_INLINE void PCNT_IntSet ( PCNT_TypeDef *pcnt, uint32_t flags)
Set one or more pending PCNT interrupts from SW.
void PCNT_PRSInputEnable ( PCNT_TypeDef *pcnt, PCNT_PRSInput_TypeDef prsInput, bool enable)
Enable/disable the selected PRS input of PCNT.
void PCNT_Reset ( PCNT_TypeDef *pcnt)
Reset PCNT to same state as after a HW reset.
void PCNT_TCCConfiguration ( PCNT_TypeDef *pcnt, const PCNT_TCC_TypeDef *config)
Set Triggered Compare and Clear configuration.
__STATIC_INLINE uint32_t PCNT_TopBufferGet ( PCNT_TypeDef *pcnt)
Get pulse counter top buffer value.
void PCNT_TopBufferSet ( PCNT_TypeDef *pcnt, uint32_t val)
Set top buffer value.
__STATIC_INLINE uint32_t PCNT_TopGet ( PCNT_TypeDef *pcnt)
Get pulse counter top value.
void PCNT_TopSet ( PCNT_TypeDef *pcnt, uint32_t val)
Set top value.

Macro Definition Documentation

#define PCNT0_CNT_SIZE   (16) /* PCNT0 counter is 16 bits. */

PCNT0 Counter register size.

Definition at line 62 of file em_pcnt.h .

Referenced by PCNT_CounterTopSet() , PCNT_Init() , and PCNT_TopSet() .

#define PCNT_FILTER_DEFAULT
Value:
{ \
0, /* Default length is 5 LFACLK cycles */ \
false /* No flutter removal */ \
}

Default config for PCNT init structure.

Definition at line 270 of file em_pcnt.h .

#define PCNT_INIT_DEFAULT
Value:
{ \
pcntModeDisable, /* Disabled by default. */ \
_PCNT_CNT_RESETVALUE, /* Default counter HW reset value. */ \
_PCNT_TOP_RESETVALUE, /* Default counter HW reset value. */ \
false, /* Use positive edge. */ \
false, /* Up-counting. */ \
false, /* Filter disabled. */ \
false, /* Hysteresis disabled. */ \
true, /* Counter direction is given by CNTDIR. */ \
pcntCntEventUp, /* Regular counter counts up on upcount events. */ \
pcntCntEventNone, /* Auxiliary counter doesn't respond to events. */ \
pcntPRSCh0, /* PRS channel 0 selected as S0IN. */ \
pcntPRSCh0 /* PRS channel 0 selected as S1IN. */ \
}

Default config for PCNT init structure.

Definition at line 238 of file em_pcnt.h .

#define PCNT_TCC_DEFAULT
Value:
{ \
tccModeDisabled, /* Disabled by default */ \
tccPrescDiv1, /* Do not prescale LFA clock in LFA mode */ \
tccCompLTOE, /* Clear when CNT <= TOP */ \
pcntPRSCh0, /* Select PRS channel 0 as input to TCC */ \
false, /* PRS polarity is rising edge, and gate when 1 */ \
false /* Do not gate the PCNT counter input */ \
}

Definition at line 343 of file em_pcnt.h .

Enumeration Type Documentation

Counter event selection. Note: unshifted values are being used for enumeration because multiple configuration structure members use this type definition.

Enumerator
pcntCntEventBoth

Counts up on up-count and down on down-count events.

pcntCntEventUp

Only counts up on up-count events.

pcntCntEventDown

Only counts down on down-count events.

pcntCntEventNone

Never counts.

Definition at line 109 of file em_pcnt.h .

Mode selection.

Enumerator
pcntModeDisable

Disable pulse counter.

pcntModeOvsSingle

Single input LFACLK oversampling mode (available in EM0-EM2).

pcntModeExtSingle

Externally clocked single input counter mode (available in EM0-EM3).

pcntModeExtQuad

Externally clocked quadrature decoder mode (available in EM0-EM3).

pcntModeOvsQuad1

LFACLK oversampling quadrature decoder 1X mode (available in EM0-EM2).

pcntModeOvsQuad2

LFACLK oversampling quadrature decoder 2X mode (available in EM0-EM2).

pcntModeOvsQuad4

LFACLK oversampling quadrature decoder 4X mode (available in EM0-EM2).

Definition at line 80 of file em_pcnt.h .

PRS inputs of PCNT.

Enumerator
pcntPRSInputS1

PRS input 0.

Definition at line 158 of file em_pcnt.h .

PRS sources for s0PRS and s1PRS .

Enumerator
pcntPRSCh0

PRS channel 0.

pcntPRSCh1

PRS channel 1.

pcntPRSCh2

PRS channel 2.

pcntPRSCh3

PRS channel 3.

pcntPRSCh4

PRS channel 4.

pcntPRSCh5

PRS channel 5.

pcntPRSCh6

PRS channel 6.

pcntPRSCh7

PRS channel 7.

pcntPRSCh8

PRS channel 8.

pcntPRSCh9

PRS channel 9.

pcntPRSCh10

PRS channel 10.

pcntPRSCh11

PRS channel 11.

Definition at line 126 of file em_pcnt.h .

Compare modes for TCC module

Enumerator
tccCompLTOE

Compare match if PCNT_CNT is less than, or equal to PCNT_TOP.

tccCompGTOE

Compare match if PCNT_CNT is greater than or equal to PCNT_TOP.

tccCompRange

Compare match if PCNT_CNT is less than, or equal to PCNT_TOP[15:8]], and greater than, or equal to PCNT_TOP[7:0].

Definition at line 307 of file em_pcnt.h .

Modes for Triggered Compare and Clear module

Enumerator
tccModeDisabled

Triggered compare and clear not enabled.

tccModeLFA

Compare and clear performed on each (optionally prescaled) LFA clock cycle.

tccModePRS

Compare and clear performed on PRS edges. Polarity defined by prsPolarity.

Definition at line 280 of file em_pcnt.h .

Prescaler values for LFA compare and clear events. Only has effect when TCC mode is LFA.

Enumerator
tccPrescDiv1

Compare and clear event each LFA cycle.

tccPrescDiv2

Compare and clear event every other LFA cycle.

tccPrescDiv4

Compare and clear event every 4th LFA cycle.

tccPrescDiv8

Compare and clear event every 8th LFA cycle.

Definition at line 292 of file em_pcnt.h .

Function Documentation

__STATIC_INLINE uint32_t PCNT_AuxCounterGet ( PCNT_TypeDef * pcnt )

Get auxiliary counter value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current auxiliary counter value.

Definition at line 386 of file em_pcnt.h .

References PCNT_TypeDef::AUXCNT .

__STATIC_INLINE uint32_t PCNT_CounterGet ( PCNT_TypeDef * pcnt )

Get pulse counter value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter value.

Definition at line 370 of file em_pcnt.h .

References PCNT_TypeDef::CNT .

void PCNT_CounterReset ( PCNT_TypeDef * pcnt )

Reset PCNT counters and TOP register.

Note
Notice that special SYNCBUSY handling is not applicable for the RSTEN bit of the control register, so we don't need to wait for it when only modifying RSTEN. (It would mean undefined wait time if clocked by external clock.) The SYNCBUSY bit will however be set, leading to a synchronization in the LF domain, with in reality no changes.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.

Definition at line 142 of file em_pcnt.c .

References _PCNT_CTRL_RSTEN_SHIFT , BUS_RegBitWrite() , and PCNT_TypeDef::CTRL .

__STATIC_INLINE void PCNT_CounterSet ( PCNT_TypeDef * pcnt,
uint32_t count
)

Set counter value.

The pulse counter is disabled while changing counter value, and reenabled (if originally enabled) when counter value has been set.

Note
This function will stall until synchronization to low frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module, since stall time may be undefined in that case. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] count Value to set in counter register.

Definition at line 416 of file em_pcnt.h .

References PCNT_CounterTopSet() , and PCNT_TypeDef::TOP .

void PCNT_CounterTopSet ( PCNT_TypeDef * pcnt,
uint32_t count,
uint32_t top
)

Set counter and top values.

The pulse counter is disabled while changing these values, and reenabled (if originally enabled) when values have been set.

Note
This function will stall until synchronization to low frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module, since stall time may be undefined in that case. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] count Value to set in counter register.
[in] top Value to set in top register.

Definition at line 177 of file em_pcnt.c .

References _PCNT_CTRL_MODE_MASK , PCNT_TypeDef::CMD , PCNT_TypeDef::CTRL , PCNT0 , PCNT0_CNT_SIZE , PCNT_CMD_LCNTIM , PCNT_CMD_LTOPBIM , PCNT_CTRL_MODE_DISABLE , PCNT_SYNCBUSY_CMD , PCNT_SYNCBUSY_CTRL , PCNT_SYNCBUSY_TOPB , and PCNT_TypeDef::TOPB .

Referenced by PCNT_CounterSet() , and PCNT_Init() .

void PCNT_Enable ( PCNT_TypeDef * pcnt,
PCNT_Mode_TypeDef mode
)

Set PCNT operational mode.

Notice that this function does not do any configuration. Setting operational mode is normally only required after initialization is done, and if not done as part of initialization. Or if requiring to disable/reenable pulse counter.

Note
This function may stall until synchronization to low frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module, since stall time may be undefined in that case.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] mode Operational mode to use for PCNT.

Definition at line 272 of file em_pcnt.c .

References _PCNT_CTRL_MODE_MASK , _PCNT_CTRL_MODE_SHIFT , PCNT_TypeDef::CTRL , and PCNT_SYNCBUSY_CTRL .

void PCNT_FilterConfiguration ( PCNT_TypeDef * pcnt,
const PCNT_Filter_TypeDef * config,
bool enable
)

Set filter configuration.

This function will configure the PCNT input filter, when the PCNT mode is configured to take an LFA-derived clock as input clock.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] config Pointer to configuration structure to be applied.
[in] enable Whether to enable or disable filtering

Definition at line 667 of file em_pcnt.c .

References _PCNT_OVSCFG_FILTLEN_MASK , _PCNT_OVSCFG_FILTLEN_SHIFT , _PCNT_OVSCFG_FLUTTERRM_SHIFT , PCNT_TypeDef::CTRL , PCNT_Filter_TypeDef::filtLen , PCNT_Filter_TypeDef::flutterrm , PCNT_TypeDef::OVSCFG , PCNT_CTRL_FILT , PCNT_SYNCBUSY_CTRL , and PCNT_SYNCBUSY_OVSCFG .

void PCNT_FreezeEnable ( PCNT_TypeDef * pcnt,
bool enable
)

PCNT register synchronization freeze control.

Some PCNT registers require synchronization into the low frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).

Note
When enabling freeze mode, this function will wait for all current ongoing PCNT synchronization to LF domain to complete (Normally synchronization will not be in progress.) However for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unecessary stalling.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] enable
  • true - enable freeze, modified registers are not propagated to the LF domain
  • false - disables freeze, modified registers are propagated to LF domain

Definition at line 357 of file em_pcnt.c .

References PCNT_TypeDef::FREEZE , PCNT_FREEZE_REGFREEZE , and PCNT_TypeDef::SYNCBUSY .

void PCNT_Init ( PCNT_TypeDef * pcnt,
const PCNT_Init_TypeDef * init
)

Init pulse counter.

This function will configure the pulse counter. The clock selection is configured as follows, depending on operational mode:

Notice that the LFACLK must be enabled in all modes, since some basic setup is done with this clock even if external pin clock usage mode is chosen. The pulse counter clock for the selected instance must also be enabled prior to init.

Notice that pins used by the PCNT module must be properly configured by the user explicitly through setting the ROUTE register, in order for the PCNT to work as intended.

Writing to CNT will not occur in external clock modes (EXTCLKQUAD and EXTCLKSINGLE) because the external clock rate is unknown. The user should handle it manually depending on the application

TOPB is written for all modes but in external clock mode it will take 3 external clock cycles to sync to TOP

Note
Initializing requires synchronization into the low frequency domain. This may cause some delay.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] init Pointer to initialization structure used to initialize.

Definition at line 417 of file em_pcnt.c .

References _PCNT_CTRL_AUXCNTEV_SHIFT , _PCNT_CTRL_CNTEV_SHIFT , _PCNT_CTRL_MODE_MASK , _PCNT_CTRL_MODE_SHIFT , _PCNT_CTRL_RSTEN_SHIFT , _PCNT_INPUT_S0PRSSEL_MASK , _PCNT_INPUT_S0PRSSEL_SHIFT , _PCNT_INPUT_S1PRSSEL_MASK , _PCNT_INPUT_S1PRSSEL_SHIFT , PCNT_Init_TypeDef::auxCntEvent , BUS_RegBitWrite() , PCNT_TypeDef::CMD , CMU_PCNTClockExternalSet() , PCNT_Init_TypeDef::cntEvent , PCNT_Init_TypeDef::countDown , PCNT_Init_TypeDef::counter , PCNT_TypeDef::CTRL , PCNT_Init_TypeDef::filter , PCNT_Init_TypeDef::hyst , PCNT_TypeDef::INPUT , PCNT_Init_TypeDef::mode , PCNT_Init_TypeDef::negEdge , PCNT0 , PCNT0_CNT_SIZE , PCNT_CMD_LTOPBIM , PCNT_CounterTopSet() , PCNT_CTRL_CNTDIR_DOWN , PCNT_CTRL_EDGE_NEG , PCNT_CTRL_FILT , PCNT_CTRL_HYST , PCNT_CTRL_MODE_DISABLE , PCNT_CTRL_RSTEN , PCNT_CTRL_S1CDIR , PCNT_SYNCBUSY_CTRL , pcntCntEventBoth , pcntCntEventDown , pcntCntEventNone , pcntCntEventUp , pcntModeExtQuad , pcntModeExtSingle , pcntModeOvsSingle , PCNT_Init_TypeDef::s0PRS , PCNT_Init_TypeDef::s1CntDir , PCNT_Init_TypeDef::s1PRS , PCNT_Init_TypeDef::top , and PCNT_TypeDef::TOPB .

__STATIC_INLINE void PCNT_IntClear ( PCNT_TypeDef * pcnt,
uint32_t flags
)

Clear one or more pending PCNT interrupts.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags Pending PCNT interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 449 of file em_pcnt.h .

References PCNT_TypeDef::IFC .

__STATIC_INLINE void PCNT_IntDisable ( PCNT_TypeDef * pcnt,
uint32_t flags
)

Disable one or more PCNT interrupts.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 465 of file em_pcnt.h .

References PCNT_TypeDef::IEN .

__STATIC_INLINE void PCNT_IntEnable ( PCNT_TypeDef * pcnt,
uint32_t flags
)

Enable one or more PCNT interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using PCNT_IntClear() prior to enabling if such a pending interrupt should be ignored.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 486 of file em_pcnt.h .

References PCNT_TypeDef::IEN .

__STATIC_INLINE uint32_t PCNT_IntGet ( PCNT_TypeDef * pcnt )

Get pending PCNT interrupt flags.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
PCNT interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 505 of file em_pcnt.h .

References PCNT_TypeDef::IF .

__STATIC_INLINE uint32_t PCNT_IntGetEnabled ( PCNT_TypeDef * pcnt )

Get enabled and pending PCNT interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Pending and enabled PCNT interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in PCNT_IEN_nnn register (PCNT_IEN_nnn) and
  • the OR combination of valid interrupt flags of the PCNT module (PCNT_IF_nnn).

Definition at line 531 of file em_pcnt.h .

References PCNT_TypeDef::IEN , and PCNT_TypeDef::IF .

__STATIC_INLINE void PCNT_IntSet ( PCNT_TypeDef * pcnt,
uint32_t flags
)

Set one or more pending PCNT interrupts from SW.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 554 of file em_pcnt.h .

References PCNT_TypeDef::IFS .

void PCNT_PRSInputEnable ( PCNT_TypeDef * pcnt,
PCNT_PRSInput_TypeDef prsInput,
bool enable
)

Enable/disable the selected PRS input of PCNT.

Notice that this function does not do any configuration.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] prsInput PRS input (S0 or S1) of the selected PCNT module.
[in] enable Set to true to enable, false to disable the selected PRS input.

Definition at line 304 of file em_pcnt.c .

References _PCNT_INPUT_S0PRSEN_SHIFT , _PCNT_INPUT_S1PRSEN_SHIFT , BUS_RegBitWrite() , PCNT_TypeDef::INPUT , and pcntPRSInputS1 .

void PCNT_Reset ( PCNT_TypeDef * pcnt )

Reset PCNT to same state as after a HW reset.

Notice the LFACLK must be enabled, since some basic reset is done with this clock. The pulse counter clock for the selected instance must also be enabled prior to init.

Note
The ROUTE register is NOT reset by this function, in order to allow for centralized setup of this feature.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.

Definition at line 613 of file em_pcnt.c .

References _PCNT_CTRL_RESETVALUE , _PCNT_CTRL_RSTEN_SHIFT , _PCNT_IEN_RESETVALUE , _PCNT_IFC_MASK , _PCNT_TOPB_RESETVALUE , BUS_RegBitWrite() , CMU_PCNTClockExternalSet() , PCNT_TypeDef::CTRL , PCNT_TypeDef::IEN , PCNT_TypeDef::IFC , PCNT_CTRL_RSTEN , PCNT_SYNCBUSY_CTRL , and PCNT_TopBufferSet() .

void PCNT_TCCConfiguration ( PCNT_TypeDef * pcnt,
const PCNT_TCC_TypeDef * config
)

Set Triggered Compare and Clear configuration.

This function will configure the PCNT TCC (Triggered Compare and Clear) module. This module can, upon a configurable trigger source, compare the current counter value with the configured TOP value. Upon match, the counter will be reset, and the TCC PRS output and TCC interrupt flag will be set.

Since there is a comparison with the TOP value, the counter will not stop counting nor wrap when hitting the TOP value, but it will keep on counting until its maximum value. Then, it will not wrap, but instead stop counting and set the overflow flag.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] config Pointer to configuration structure to be applied.

Definition at line 713 of file em_pcnt.c .

References _PCNT_CTRL_PRSGATEEN_MASK , _PCNT_CTRL_PRSGATEEN_SHIFT , _PCNT_CTRL_TCCCOMP_MASK , _PCNT_CTRL_TCCCOMP_SHIFT , _PCNT_CTRL_TCCMODE_MASK , _PCNT_CTRL_TCCMODE_SHIFT , _PCNT_CTRL_TCCPRESC_MASK , _PCNT_CTRL_TCCPRESC_SHIFT , _PCNT_CTRL_TCCPRSPOL_MASK , _PCNT_CTRL_TCCPRSPOL_SHIFT , _PCNT_CTRL_TCCPRSSEL_MASK , _PCNT_CTRL_TCCPRSSEL_SHIFT , PCNT_TCC_TypeDef::compare , PCNT_TypeDef::CTRL , PCNT_TCC_TypeDef::mode , PCNT_SYNCBUSY_CTRL , PCNT_TCC_TypeDef::prescaler , PCNT_TCC_TypeDef::prsGateEnable , PCNT_TCC_TypeDef::prsPolarity , and PCNT_TCC_TypeDef::tccPRS .

__STATIC_INLINE uint32_t PCNT_TopBufferGet ( PCNT_TypeDef * pcnt )

Get pulse counter top buffer value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter top buffer value.

Definition at line 571 of file em_pcnt.h .

References PCNT_TypeDef::TOPB .

void PCNT_TopBufferSet ( PCNT_TypeDef * pcnt,
uint32_t val
)

Set top buffer value.

Note
This function may stall until synchronization to low frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module, since stall time may be undefined in that case.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] val Value to set in top buffer register.

Definition at line 755 of file em_pcnt.c .

References PCNT_SYNCBUSY_TOPB , and PCNT_TypeDef::TOPB .

Referenced by PCNT_Reset() .

__STATIC_INLINE uint32_t PCNT_TopGet ( PCNT_TypeDef * pcnt )

Get pulse counter top value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter top value.

Definition at line 588 of file em_pcnt.h .

References PCNT_TypeDef::TOP .

void PCNT_TopSet ( PCNT_TypeDef * pcnt,
uint32_t val
)

Set top value.

Note
This function will stall until synchronization to low frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module, since stall time may be undefined in that case.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] val Value to set in top register.

Definition at line 780 of file em_pcnt.c .

References PCNT_TypeDef::CMD , PCNT0 , PCNT0_CNT_SIZE , PCNT_CMD_LTOPBIM , PCNT_SYNCBUSY_CMD , PCNT_SYNCBUSY_TOPB , and PCNT_TypeDef::TOPB .