PRS_TypeDef Struct ReferenceDevices > PRS

PRS Register Declaration

Definition at line 49 of file efr32mg14p_prs.h .

#include < efr32mg14p_prs.h >

Data Fields

PRS_CH_TypeDef CH [12]
__IOM uint32_t CTRL
__IOM uint32_t DMAREQ0
__IOM uint32_t DMAREQ1
__IM uint32_t PEEK
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [5]
uint32_t RESERVED2 [1]
uint32_t RESERVED3 [3]
__IOM uint32_t ROUTELOC0
__IOM uint32_t ROUTELOC1
__IOM uint32_t ROUTELOC2
__IOM uint32_t ROUTEPEN
__IOM uint32_t SWLEVEL
__IOM uint32_t SWPULSE

Field Documentation

PRS_CH_TypeDef PRS_TypeDef::CH[12]

Channel registers

Definition at line 66 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::CTRL

Control Register

Definition at line 59 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::DMAREQ0

DMA Request 0 Register

Definition at line 60 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::DMAREQ1

DMA Request 1 Register

Definition at line 61 of file efr32mg14p_prs.h .

__IM uint32_t PRS_TypeDef::PEEK

PRS Channel Values

Definition at line 63 of file efr32mg14p_prs.h .

uint32_t PRS_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 53 of file efr32mg14p_prs.h .

uint32_t PRS_TypeDef::RESERVED1[5]

Reserved for future use

Definition at line 58 of file efr32mg14p_prs.h .

uint32_t PRS_TypeDef::RESERVED2[1]

Reserved for future use

Definition at line 62 of file efr32mg14p_prs.h .

uint32_t PRS_TypeDef::RESERVED3[3]

Reserved registers

Definition at line 65 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 54 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::ROUTELOC1

I/O Routing Location Register

Definition at line 55 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::ROUTELOC2

I/O Routing Location Register

Definition at line 56 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 52 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::SWLEVEL

Software Level Register

Definition at line 51 of file efr32mg14p_prs.h .

__IOM uint32_t PRS_TypeDef::SWPULSE

Software Pulse Register

Definition at line 50 of file efr32mg14p_prs.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/ efr32mg14p_prs.h