VDAC_TypeDef Struct ReferenceDevices > VDAC

VDAC Register Declaration

Definition at line 49 of file efr32mg14p_vdac.h .

#include < efr32mg14p_vdac.h >

Data Fields

__IOM uint32_t CAL
__IOM uint32_t CH0CTRL
__IOM uint32_t CH0DATA
__IOM uint32_t CH1CTRL
__IOM uint32_t CH1DATA
__IOM uint32_t CMD
__IOM uint32_t COMBDATA
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
VDAC_OPA_TypeDef OPA [2]
uint32_t RESERVED0 [27]
__IM uint32_t STATUS

Field Documentation

__IOM uint32_t VDAC_TypeDef::CAL

Calibration Register

Definition at line 62 of file efr32mg14p_vdac.h .

Referenced by VDAC_Init() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::CH0CTRL

Channel 0 Control Register

Definition at line 52 of file efr32mg14p_vdac.h .

Referenced by VDAC_InitChannel() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::CH0DATA

Channel 0 Data Register

Definition at line 59 of file efr32mg14p_vdac.h .

Referenced by VDAC_Channel0OutputSet() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::CH1CTRL

Channel 1 Control Register

Definition at line 53 of file efr32mg14p_vdac.h .

Referenced by VDAC_InitChannel() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::CH1DATA

Channel 1 Data Register

Definition at line 60 of file efr32mg14p_vdac.h .

Referenced by VDAC_Channel1OutputSet() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::CMD

Command Register

Definition at line 54 of file efr32mg14p_vdac.h .

Referenced by VDAC_Enable() , VDAC_Init() , VDAC_InitChannel() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::COMBDATA

Combined Data Register

Definition at line 61 of file efr32mg14p_vdac.h .

__IOM uint32_t VDAC_TypeDef::CTRL

Control Register

Definition at line 50 of file efr32mg14p_vdac.h .

Referenced by VDAC_Init() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::IEN

Interrupt Enable Register

Definition at line 58 of file efr32mg14p_vdac.h .

Referenced by VDAC_IntDisable() , VDAC_IntEnable() , VDAC_IntGetEnabled() , and VDAC_Reset() .

__IM uint32_t VDAC_TypeDef::IF

Interrupt Flag Register

Definition at line 55 of file efr32mg14p_vdac.h .

Referenced by VDAC_IntGet() , and VDAC_IntGetEnabled() .

__IOM uint32_t VDAC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 57 of file efr32mg14p_vdac.h .

Referenced by VDAC_IntClear() , and VDAC_Reset() .

__IOM uint32_t VDAC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 56 of file efr32mg14p_vdac.h .

Referenced by VDAC_IntSet() .

VDAC_OPA_TypeDef VDAC_TypeDef::OPA[2]

OPA Registers

Definition at line 65 of file efr32mg14p_vdac.h .

uint32_t VDAC_TypeDef::RESERVED0[27]

Reserved registers

Definition at line 64 of file efr32mg14p_vdac.h .

__IM uint32_t VDAC_TypeDef::STATUS

Status Register

Definition at line 51 of file efr32mg14p_vdac.h .

Referenced by VDAC_Enable() , VDAC_Init() , VDAC_InitChannel() , and VDAC_Reset() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/ efr32mg14p_vdac.h