nvm.h File Reference

Non-Volatile Memory Wear-Leveling driver API.

Version
5.4.0

License

(C) Copyright 2014 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file nvm.h.

#include <stdint.h>
#include <stdbool.h>
#include "em_device.h"
#include "nvm_hal.h"
#include "nvm_config.h"
#include "ecode.h"

Macros

#define ECODE_EMDRV_NVM_ADDR_INVALID   (ECODE_EMDRV_NVM_BASE | 0x00000001)
 Invalid address.
 
#define ECODE_EMDRV_NVM_ALIGNMENT_INVALID   (ECODE_EMDRV_NVM_BASE | 0x00000002)
 Invalid data alignment.
 
#define ECODE_EMDRV_NVM_DATA_INVALID   (ECODE_EMDRV_NVM_BASE | 0x00000003)
 Invalid input data or format.
 
#define ECODE_EMDRV_NVM_ERROR   (ECODE_EMDRV_NVM_BASE | 0x00000007)
 General error.
 
#define ECODE_EMDRV_NVM_NO_PAGES_AVAILABLE   (ECODE_EMDRV_NVM_BASE | 0x00000005)
 Initialization didn't find any pages available to allocate.
 
#define ECODE_EMDRV_NVM_OK   (ECODE_OK)
 Success return value.
 
#define ECODE_EMDRV_NVM_PAGE_INVALID   (ECODE_EMDRV_NVM_BASE | 0x00000006)
 Could not find the page specified.
 
#define ECODE_EMDRV_NVM_WRITE_LOCK   (ECODE_EMDRV_NVM_BASE | 0x00000004)
 A write is currently in progress.
 
#define NVM_ERASE_RETAINCOUNT   0xffffffffUL
 
#define NVM_PAGE_TERMINATION   { NULL, 0, (NVM_Object_Ids) 0 }
 
#define NVM_READ_ALL_CMD   0xff
 
#define NVM_WRITE_ALL_CMD   0xff
 
#define NVM_WRITE_NONE_CMD   0xfe
 

Functions

Ecode_t NVM_Erase (uint32_t eraseCount)
 Erase the entire allocated NVM area.
 
Ecode_t NVM_Init (NVM_Config_t const *nvmConfig)
 Initialize the NVM manager.
 
Ecode_t NVM_Read (uint16_t pageId, uint8_t objectId)
 Read an object or an entire page.
 
Ecode_t NVM_Write (uint16_t pageId, uint8_t objectId)
 Write an object or a page.