ustimer.h File Reference
Microsecond delay function API definition.
- Version
- 5.4.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file ustimer.h
.
#include <stdint.h>
#include "ecode.h
"
#include "ustimer_config.h"
Macros | |
#define | ECODE_EMDRV_USTIMER_OK ( ECODE_OK ) |
Success return value. | |
Functions | |
Ecode_t | USTIMER_DeInit (void) |
Deinitialize USTIMER driver. | |
Ecode_t | USTIMER_Delay (uint32_t usec) |
Delay a given number of microseconds. | |
Ecode_t | USTIMER_DelayIntSafe (uint32_t usec) |
Delay a given number of microseconds. | |
Ecode_t | USTIMER_Init (void) |
Activate and initialize the hardware timer used to pace the 1 microsecond delay functions. | |