LESENSE_BUF_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_BUF LESENSE BUF Register

.

Definition at line 47 of file efm32pg12b_lesense_buf.h.

#include <efm32pg12b_lesense_buf.h>

Data Fields

__IOM uint32_t DATA
 

Field Documentation

__IOM uint32_t LESENSE_BUF_TypeDef::DATA

Scan Results

Definition at line 48 of file efm32pg12b_lesense_buf.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/efm32pg12b_lesense_buf.h