VDAC_TypeDef Struct ReferenceDevices > VDAC
VDAC Register Declaration
Definition at line 49
of file efm32pg12b_vdac.h
.
#include <
efm32pg12b_vdac.h
>
Data Fields | |
__IOM uint32_t | CAL |
__IOM uint32_t | CH0CTRL |
__IOM uint32_t | CH0DATA |
__IOM uint32_t | CH1CTRL |
__IOM uint32_t | CH1DATA |
__IOM uint32_t | CMD |
__IOM uint32_t | COMBDATA |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
VDAC_OPA_TypeDef | OPA [3] |
uint32_t | RESERVED0 [27] |
__IM uint32_t | STATUS |
Field Documentation
__IOM uint32_t VDAC_TypeDef::CAL |
Calibration Register
Definition at line 62
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Init(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::CH0CTRL |
Channel 0 Control Register
Definition at line 52
of file efm32pg12b_vdac.h
.
Referenced by VDAC_InitChannel(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::CH0DATA |
Channel 0 Data Register
Definition at line 59
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Channel0OutputSet(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::CH1CTRL |
Channel 1 Control Register
Definition at line 53
of file efm32pg12b_vdac.h
.
Referenced by VDAC_InitChannel(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::CH1DATA |
Channel 1 Data Register
Definition at line 60
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Channel1OutputSet(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::CMD |
Command Register
Definition at line 54
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Enable(), VDAC_Init(), VDAC_InitChannel(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::COMBDATA |
Combined Data Register
Definition at line 61
of file efm32pg12b_vdac.h
.
__IOM uint32_t VDAC_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Init(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 58
of file efm32pg12b_vdac.h
.
Referenced by VDAC_IntDisable(), VDAC_IntEnable(), VDAC_IntGetEnabled(), and VDAC_Reset().
__IM uint32_t VDAC_TypeDef::IF |
Interrupt Flag Register
Definition at line 55
of file efm32pg12b_vdac.h
.
Referenced by VDAC_IntGet(), and VDAC_IntGetEnabled().
__IOM uint32_t VDAC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 57
of file efm32pg12b_vdac.h
.
Referenced by VDAC_IntClear(), and VDAC_Reset().
__IOM uint32_t VDAC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 56
of file efm32pg12b_vdac.h
.
Referenced by VDAC_IntSet().
VDAC_OPA_TypeDef VDAC_TypeDef::OPA[3] |
OPA Registers
Definition at line 65
of file efm32pg12b_vdac.h
.
uint32_t VDAC_TypeDef::RESERVED0[27] |
Reserved registers
Definition at line 64
of file efm32pg12b_vdac.h
.
__IM uint32_t VDAC_TypeDef::STATUS |
Status Register
Definition at line 51
of file efm32pg12b_vdac.h
.
Referenced by VDAC_Enable(), VDAC_Init(), VDAC_InitChannel(), and VDAC_Reset().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/
efm32pg12b_vdac.h