USART_InitIrDA_TypeDef Struct ReferenceEMLIB > USART

IrDA mode initialization structure. Inherited from asynchronous mode initialization structure.

Definition at line 560 of file em_usart.h.

#include <em_usart.h>

Data Fields

USART_InitAsync_TypeDef async
 
bool irFilt
 
bool irPrsEn
 
USART_IrDAPrsSel_Typedef irPrsSel
 
USART_IrDAPw_Typedef irPw
 
bool irRxInv
 

Field Documentation

USART_InitAsync_TypeDef USART_InitIrDA_TypeDef::async

General Asynchronous initialization structure.

Definition at line 562 of file em_usart.h.

Referenced by USARTn_InitIrDA().

bool USART_InitIrDA_TypeDef::irFilt

Set to enable filter on IrDA demodulator.

Definition at line 568 of file em_usart.h.

Referenced by USARTn_InitIrDA().

bool USART_InitIrDA_TypeDef::irPrsEn

Enable the PRS channel selected by irPrsSel as input to IrDA module instead of TX.

Definition at line 576 of file em_usart.h.

Referenced by USARTn_InitIrDA().

USART_IrDAPrsSel_Typedef USART_InitIrDA_TypeDef::irPrsSel

PRS can be used as input to the pulse modulator instead of TX. This value selects the channel to use.

Definition at line 580 of file em_usart.h.

Referenced by USARTn_InitIrDA().

USART_IrDAPw_Typedef USART_InitIrDA_TypeDef::irPw

Configure the pulse width generated by the IrDA modulator as a fraction of the configured USART bit period.

Definition at line 572 of file em_usart.h.

Referenced by USARTn_InitIrDA().

bool USART_InitIrDA_TypeDef::irRxInv

Set to invert Rx signal before IrDA demodulator.

Definition at line 565 of file em_usart.h.

Referenced by USARTn_InitIrDA().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_usart.h