TRNG_TypeDef Struct ReferenceDevices > TRNG

TRNG Register Declaration

Definition at line 49 of file efm32pg12b_trng.h.

#include <efm32pg12b_trng.h>

Data Fields

__IOM uint32_t CONTROL
 
__IM uint32_t FIFO
 
__IM uint32_t FIFODEPTH
 
__IM uint32_t FIFOLEVEL
 
__IOM uint32_t INITWAITVAL
 
__IOM uint32_t KEY0
 
__IOM uint32_t KEY1
 
__IOM uint32_t KEY2
 
__IOM uint32_t KEY3
 
uint32_t RESERVED0 [1]
 
uint32_t RESERVED1 [3]
 
uint32_t RESERVED2 [50]
 
__IOM uint32_t STATUS
 
__IOM uint32_t TESTDATA
 

Field Documentation

__IOM uint32_t TRNG_TypeDef::CONTROL

Main Control Register

Definition at line 50 of file efm32pg12b_trng.h.

__IM uint32_t TRNG_TypeDef::FIFO

FIFO Data

Definition at line 64 of file efm32pg12b_trng.h.

__IM uint32_t TRNG_TypeDef::FIFODEPTH

FIFO Depth Register

Definition at line 53 of file efm32pg12b_trng.h.

__IM uint32_t TRNG_TypeDef::FIFOLEVEL

FIFO Level Register

Definition at line 51 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::INITWAITVAL

Initial Wait Counter

Definition at line 62 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::KEY0

Key Register 0

Definition at line 54 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::KEY1

Key Register 1

Definition at line 55 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::KEY2

Key Register 2

Definition at line 56 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::KEY3

Key Register 3

Definition at line 57 of file efm32pg12b_trng.h.

uint32_t TRNG_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 52 of file efm32pg12b_trng.h.

uint32_t TRNG_TypeDef::RESERVED1[3]

Reserved for future use

Definition at line 60 of file efm32pg12b_trng.h.

uint32_t TRNG_TypeDef::RESERVED2[50]

Reserved for future use

Definition at line 63 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::STATUS

Status Register

Definition at line 61 of file efm32pg12b_trng.h.

__IOM uint32_t TRNG_TypeDef::TESTDATA

Test Data Register

Definition at line 58 of file efm32pg12b_trng.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/efm32pg12b_trng.h