dmadrv.h File Reference
DMADRV API definition.
- Version
- 5.5.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        dmadrv.h
       
       .
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        ecode.h
       
       "
      
      
       #include "
       
        em_ldma.h
       
       "
      
      
       #include "dmadrv_config.h"
      
      
| Macros | |
| #define | DMADRV_MAX_XFER_COUNT ((int)(( _LDMA_CH_CTRL_XFERCNT_MASK >> _LDMA_CH_CTRL_XFERCNT_SHIFT ) + 1)) | 
| Maximum length of one DMA transfer. | |
| #define | ECODE_EMDRV_DMADRV_ALREADY_FREED ( ECODE_EMDRV_DMADRV_BASE | 0x00000006) | 
| A DMA channel was free. | |
| #define | ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED ( ECODE_EMDRV_DMADRV_BASE | 0x00000003) | 
| DMA has already been initialized. | |
| #define | ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED ( ECODE_EMDRV_DMADRV_BASE | 0x00000007) | 
| A channel is not reserved. | |
| #define | ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED ( ECODE_EMDRV_DMADRV_BASE | 0x00000004) | 
| No DMA channels available. | |
| #define | ECODE_EMDRV_DMADRV_IN_USE ( ECODE_EMDRV_DMADRV_BASE | 0x00000005) | 
| DMA is in use. | |
| #define | ECODE_EMDRV_DMADRV_NOT_INITIALIZED ( ECODE_EMDRV_DMADRV_BASE | 0x00000002) | 
| DMA is not initialized. | |
| #define | ECODE_EMDRV_DMADRV_OK ( ECODE_OK ) | 
| A successful return value. | |
| #define | ECODE_EMDRV_DMADRV_PARAM_ERROR ( ECODE_EMDRV_DMADRV_BASE | 0x00000001) | 
| An illegal input parameter. | |
| #define | EMDRV_DMADRV_DMA_PRESENT | 
| #define | EMDRV_DMADRV_LDMA | 
| Typedefs | |
| typedef bool(* | DMADRV_Callback_t ) (unsigned int channel, unsigned int sequenceNo, void *userParam) | 
| DMADRV transfer completion callback function. | |
| Enumerations | |
| enum | DMADRV_DataSize_t
         
         { dmadrvDataSize1 = ldmaCtrlSizeByte, dmadrvDataSize2 = ldmaCtrlSizeHalf, dmadrvDataSize4 = ldmaCtrlSizeWord } | 
| Data size of one LDMA transfer item. | |
| enum | DMADRV_PeripheralSignal_t
         
         { dmadrvPeripheralSignal_NONE = LDMA_CH_REQSEL_SOURCESEL_NONE, dmadrvPeripheralSignal_ADC0_SCAN = LDMA_CH_REQSEL_SIGSEL_ADC0SCAN | LDMA_CH_REQSEL_SOURCESEL_ADC0, dmadrvPeripheralSignal_ADC0_SINGLE = LDMA_CH_REQSEL_SIGSEL_ADC0SINGLE | LDMA_CH_REQSEL_SOURCESEL_ADC0, dmadrvPeripheralSignal_CRYPTO_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, dmadrvPeripheralSignal_CRYPTO_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, dmadrvPeripheralSignal_CRYPTO_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, dmadrvPeripheralSignal_CRYPTO_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, dmadrvPeripheralSignal_CRYPTO_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, dmadrvPeripheralSignal_I2C0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C0, dmadrvPeripheralSignal_I2C0_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C0TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C0, dmadrvPeripheralSignal_LEUART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_LEUART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_LEUART0_TXBL = LDMA_CH_REQSEL_SIGSEL_LEUART0TXBL | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_LEUART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_LEUART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_MSC_WDATA = LDMA_CH_REQSEL_SIGSEL_MSCWDATA | LDMA_CH_REQSEL_SOURCESEL_MSC, dmadrvPeripheralSignal_PRS_REQ0 = LDMA_CH_REQSEL_SIGSEL_PRSREQ0 | LDMA_CH_REQSEL_SOURCESEL_PRS, dmadrvPeripheralSignal_PRS_REQ1 = LDMA_CH_REQSEL_SIGSEL_PRSREQ1 | LDMA_CH_REQSEL_SOURCESEL_PRS, dmadrvPeripheralSignal_TIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER1_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC3 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC3 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER1UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_USART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART0_TXBL = LDMA_CH_REQSEL_SIGSEL_USART0TXBL | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_RXDATAVRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAVRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXBL = LDMA_CH_REQSEL_SIGSEL_USART1TXBL | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXBLRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1TXBLRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART1TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART1 } | 
| Peripherals that can trigger LDMA transfers. | |
| Functions | |
| Ecode_t | DMADRV_AllocateChannel (unsigned int *channelId, void *capabilities) | 
| Allocate (reserve) a DMA channel. | |
| Ecode_t | DMADRV_DeInit (void) | 
| Deinitialize DMADRV. | |
| Ecode_t | DMADRV_FreeChannel (unsigned int channelId) | 
| Free an allocated (reserved) DMA channel. | |
| Ecode_t | DMADRV_Init (void) | 
| Initialize DMADRV. | |
| Ecode_t | DMADRV_LdmaStartTransfer (int channelId, LDMA_TransferCfg_t *transfer, LDMA_Descriptor_t *descriptor, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start an LDMA transfer. | |
| Ecode_t | DMADRV_MemoryPeripheral (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a memory to a peripheral DMA transfer. | |
| Ecode_t | DMADRV_MemoryPeripheralPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src0, void *src1, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a memory to a peripheral ping-pong DMA transfer. | |
| Ecode_t | DMADRV_PauseTransfer (unsigned int channelId) | 
| Pause an ongoing DMA transfer. | |
| Ecode_t | DMADRV_PeripheralMemory (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a peripheral to memory DMA transfer. | |
| Ecode_t | DMADRV_PeripheralMemoryPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst0, void *dst1, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) | 
| Start a peripheral to memory ping-pong DMA transfer. | |
| Ecode_t | DMADRV_ResumeTransfer (unsigned int channelId) | 
| Resume an ongoing DMA transfer. | |
| Ecode_t | DMADRV_StopTransfer (unsigned int channelId) | 
| Stop an ongoing DMA transfer. | |
| Ecode_t | DMADRV_TransferActive (unsigned int channelId, bool *active) | 
| Check if a transfer is running. | |
| Ecode_t | DMADRV_TransferCompletePending (unsigned int channelId, bool *pending) | 
| Check if a transfer complete is pending. | |
| Ecode_t | DMADRV_TransferDone (unsigned int channelId, bool *done) | 
| Check if a transfer has completed. | |
| Ecode_t | DMADRV_TransferRemainingCount (unsigned int channelId, int *remaining) | 
| Get number of items remaining in a transfer. | |