HidKeyboardKit Drivers

Detailed Description

Implements a USB HID class keyboard.

HIDKBD implementation.

The source code of the HIDKBD implementation resides in kits/common/drivers/hidkbd.c and hidkbd.h . This driver implements a basic USB keyboard. Refer to hidkbd examples for STK3700 and DK3750 for examples using this driver.

HIDKBD device configuration options.

This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko STK3700 hidbkd example.

// USB interface number. Interfaces are numbered from zero to one less than
// the number of concurrent interfaces supported by the configuration.
// The interfac numbers must be 0 standalone HID device, for a
// composite device which includes a HID interface it must not be in conflict
// with other device interfaces.
#define HIDKBD_INTERFACE_NO     0

// Endpoint address for HID input reports.
#define HIDKBD_INTR_IN_EP_ADDR  0x81

// The bInterval reported with the interrupt IN endpoint descriptor.
#define HIDKBD_POLL_RATE        24

// Timer id, see USBTIMER in the USB device stack documentation.
// The HID driver use a timer to implement the idle-rate defined in the HID class spec.
#define HIDKBD_IDLE_TIMER       0

Data Structures

struct HIDKBD_Init_t
struct HIDKBD_KeyReport_t

Typedefs

typedef void(* HIDKBD_SetReportFunc_t ) (uint8_t report)
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.

Functions

void HIDKBD_Init ( HIDKBD_Init_t *init)
Initialize HID Keyboard driver.
void HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report)
Report a keyboard press/release event.
int HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup)
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
void HIDKBD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState)
Handle USB state change events, this function must be called each time the USB device state is changed.

Variables

const char HIDKBD_ReportDescriptor [69]

Typedef Documentation

typedef void(* HIDKBD_SetReportFunc_t) (uint8_t report)

Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.

Parameters
[in] report Output report byte.
Bit 0 : State of keyboard NumLock LED.
Bit 1 : State of keyboard CapsLock LED.
Bit 2 : State of keyboard ScrollLock LED.

Definition at line 57 of file hidkbd.h .

Function Documentation

void HIDKBD_Init ( HIDKBD_Init_t * init )

Initialize HID Keyboard driver.

Parameters
[in] init Pointer to a HIDKBD_Init_t struct with configuration options.

Definition at line 187 of file hidkbd.c .

References HIDKBD_Init_t::hidDescriptor , and HIDKBD_Init_t::setReportFunc .

void HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t * report )

Report a keyboard press/release event.

Parameters
[in] report Pointer to a HIDKBD_KeyReport_t struct with new key pressed information.

Definition at line 202 of file hidkbd.c .

int HIDKBD_SetupCmd ( const USB_Setup_TypeDef * setup )

Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.

Parameters
[in] setup Pointer to the setup packet received.
Returns
USB_STATUS_OK if command accepted, USB_STATUS_REQ_UNHANDLED when command is unknown. In the latter case the USB device stack will handle the request.

Definition at line 229 of file hidkbd.c .

References SL_MIN .

void HIDKBD_StateChangeEvent ( USBD_State_TypeDef oldState,
USBD_State_TypeDef newState
)

Handle USB state change events, this function must be called each time the USB device state is changed.

Parameters
[in] oldState The device state the device has just left.
[in] newState The new device state.

Definition at line 326 of file hidkbd.c .

References DEFAULT_IDLE_RATE .