DEVINFO_TypeDef Struct ReferenceDevices > EZR32HG_DEVINFO

Definition at line 47 of file ezr32hg_devinfo.h .

Data Fields

__IM uint32_t ADC0CAL0
__IM uint32_t ADC0CAL1
__IM uint32_t ADC0CAL2
__IM uint32_t AUXHFRCOCAL0
__IM uint32_t AUXHFRCOCAL1
__IM uint32_t CAL
__IM uint32_t HFRCOCAL0
__IM uint32_t HFRCOCAL1
__IM uint32_t IDAC0CAL0
__IM uint32_t MEMINFO
__IM uint32_t MSIZE
__IM uint32_t PART
__IM uint32_t RADIO0
__IM uint32_t RADIO1
__IM uint32_t RADIO2
uint32_t RESERVED0 [2]
uint32_t RESERVED1 [1]
uint32_t RESERVED2
__IM uint32_t UNIQUEH
__IM uint32_t UNIQUEL
__IM uint32_t USHFRCOCAL0

Field Documentation

__IM uint32_t DEVINFO_TypeDef::ADC0CAL0

ADC0 Calibration register 0

Definition at line 51 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL1

ADC0 Calibration register 1

Definition at line 52 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL2

ADC0 Calibration register 2

Definition at line 53 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL0

AUXHFRCO calibration register 0

Definition at line 58 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL1

AUXHFRCO calibration register 1

Definition at line 59 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::CAL

Calibration temperature and checksum

Definition at line 50 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL0

HFRCO calibration register 0

Definition at line 60 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL1

HFRCO calibration register 1

Definition at line 61 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::IDAC0CAL0

IDAC0 calibration register

Definition at line 55 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MEMINFO

Memory information

Definition at line 62 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MSIZE

Flash and SRAM Memory size in KiloBytes

Definition at line 67 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::PART

Part description

Definition at line 68 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::RADIO0

Radio information 0

Definition at line 48 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::RADIO1

Radio information 1

Definition at line 49 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::RADIO2

Radio information 2

Definition at line 64 of file ezr32hg_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED0[2]

Reserved

Definition at line 54 of file ezr32hg_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED1[1]

Reserved

Definition at line 57 of file ezr32hg_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED2

Reserved

Definition at line 63 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEH

High 32 bits of device unique number

Definition at line 66 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEL

Low 32 bits of device unique number

Definition at line 65 of file ezr32hg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::USHFRCOCAL0

USHFRCO calibration register

Definition at line 56 of file ezr32hg_devinfo.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/ ezr32hg_devinfo.h