DMADRVEMDRV
Detailed Description
DMADRV Direct Memory Access Driver.
Introduction
The DMADRV driver supports writing code using DMA which will work regardless of the type of the DMA controller on the underlying microcontroller. Additionally, DMA can be used in several modules that are completely unaware of each other. The driver does not preclude use of the native emlib API of the underlying DMA controller. On the contrary, it will often result in more efficient code and is necessary for complex DMA operations. The housekeeping functions of this driver are valuable even in this use-case.
The dmadrv.c and dmadrv.h
source files are in the emdrv/dmadrv folder.
- Note
- DMA transfer completion callback functions are called from within the DMA interrupt handler.
Configuration Options
Some properties of the DMADRV driver are compile-time configurable. These properties are stored in a file named dmadrv_config.h. A template for this file, containing default values, is in the emdrv/config folder. Currently the configuration options are as follows:
- The interrupt priority of the DMA peripheral.
- A number of DMA channels to support.
- Use the native emlib API belonging to the underlying DMA hardware in combination with the DMADRV API.
Both configuration options will help reduce the driver's RAM footprint.
To configure DMADRV, provide a custom configuration file. This is an example dmadrv_config.h file:
#ifndef __SILICON_LABS_DMADRV_CONFIG_H__ #define __SILICON_LABS_DMADRV_CONFIG_H__ // DMADRV DMA interrupt priority configuration option. // Set DMA interrupt priority. Range is 0..7, 0 is the highest priority. #define EMDRV_DMADRV_DMA_IRQ_PRIORITY 4 // DMADRV channel count configuration option. // A number of DMA channels to support. A lower DMA channel count will reduce // RAM footprint. #define EMDRV_DMADRV_DMA_CH_COUNT 4 // DMADRV native API configuration option. // Use the native emlib API of the DMA controller in addition to DMADRV // housekeeping functions, such as AllocateChannel/FreeChannel, and so on. #define EMDRV_DMADRV_USE_NATIVE_API #endif
The API
This section contains brief descriptions of the API functions. For more information about input and output parameters and return values, click on the hyperlinked function names. Most functions return an error code, ECODE_EMDRV_DMADRV_OK is returned on success, see ecode.h
and dmadrv.h
for other error codes.
The application code must include dmadrv.h
header file.
DMADRV_Init(), DMADRV_DeInit()
These functions initialize or deinitialize the DMADRV driver. Typically, DMADRV_Init() is called once in the startup code.
DMADRV_AllocateChannel(), DMADRV_FreeChannel()
DMA channel reserve and release functions. It is recommended that application code check that DMADRV_AllocateChannel() returns ECODE_EMDRV_DMADRV_OK before starting a DMA transfer.
DMADRV_MemoryPeripheral()
Start a DMA transfer from memory to a peripheral.
DMADRV_PeripheralMemory()
Start a DMA transfer from a peripheral to memory.
DMADRV_MemoryPeripheralPingPong()
Start a DMA ping-pong transfer from memory to a peripheral.
DMADRV_PeripheralMemoryPingPong()
Start a DMA ping-pong transfer from a peripheral to memory.
DMADRV_LdmaStartTransfer()
Start a DMA transfer on an LDMA controller. This function can only be used when configuration option EMDRV_DMADRV_USE_NATIVE_API is defined. It is a wrapper similar to the emlib LDMA function, but adds support for completion callback and user-defined callback function parameter.
DMADRV_StopTransfer()
Stop an ongoing DMA transfer.
DMADRV_TransferActive()
Check if a transfer is ongoing.
DMADRV_TransferCompletePending()
Check if a transfer completion is pending.
DMADRV_TransferDone()
Check if a transfer has completed.
DMADRV_TransferRemainingCount()
Get number of items remaining in a transfer.
Example
Transfer a text string to USART1.
#include "dmadrv.h" char str[] = "Hello DMA !"; unsigned int channel; int main( void ) { // Initialize DMA. DMADRV_Init(); // Request a DMA channel. DMADRV_AllocateChannel( &channel, NULL ); // Start the DMA transfer. DMADRV_MemoryPeripheral( channel, dmadrvPeripheralSignal_USART1_TXBL, (void*)&(USART1->TXDATA), str, true, sizeof( str ), dmadrvDataSize1, NULL, NULL ); return 0; }
Macros | |
#define | DMADRV_MAX_XFER_COUNT ((int)((_LDMA_CH_CTRL_XFERCNT_MASK >> _LDMA_CH_CTRL_XFERCNT_SHIFT) + 1)) |
Maximum length of one DMA transfer. | |
#define | ECODE_EMDRV_DMADRV_ALREADY_FREED (ECODE_EMDRV_DMADRV_BASE | 0x00000006) |
A DMA channel was free. | |
#define | ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED (ECODE_EMDRV_DMADRV_BASE | 0x00000003) |
DMA has already been initialized. | |
#define | ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED (ECODE_EMDRV_DMADRV_BASE | 0x00000007) |
A channel is not reserved. | |
#define | ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED (ECODE_EMDRV_DMADRV_BASE | 0x00000004) |
No DMA channels available. | |
#define | ECODE_EMDRV_DMADRV_IN_USE (ECODE_EMDRV_DMADRV_BASE | 0x00000005) |
DMA is in use. | |
#define | ECODE_EMDRV_DMADRV_NOT_INITIALIZED (ECODE_EMDRV_DMADRV_BASE | 0x00000002) |
DMA is not initialized. | |
#define | ECODE_EMDRV_DMADRV_OK (ECODE_OK) |
A successful return value. | |
#define | ECODE_EMDRV_DMADRV_PARAM_ERROR (ECODE_EMDRV_DMADRV_BASE | 0x00000001) |
An illegal input parameter. | |
Typedefs | |
typedef bool(* | DMADRV_Callback_t) (unsigned int channel, unsigned int sequenceNo, void *userParam) |
DMADRV transfer completion callback function. | |
Enumerations | |
enum | DMADRV_DataSize_t { dmadrvDataSize1 = ldmaCtrlSizeByte, dmadrvDataSize2 = ldmaCtrlSizeHalf, dmadrvDataSize4 = ldmaCtrlSizeWord } |
Data size of one LDMA transfer item. | |
enum | DMADRV_PeripheralSignal_t { dmadrvPeripheralSignal_NONE = LDMA_CH_REQSEL_SOURCESEL_NONE, dmadrvPeripheralSignal_ADC0_SCAN = LDMA_CH_REQSEL_SIGSEL_ADC0SCAN | LDMA_CH_REQSEL_SOURCESEL_ADC0, dmadrvPeripheralSignal_ADC0_SINGLE = LDMA_CH_REQSEL_SIGSEL_ADC0SINGLE | LDMA_CH_REQSEL_SOURCESEL_ADC0, dmadrvPeripheralSignal_VDAC0_CH0 = LDMA_CH_REQSEL_SIGSEL_VDAC0CH0 | LDMA_CH_REQSEL_SOURCESEL_VDAC0, dmadrvPeripheralSignal_VDAC0_CH1 = LDMA_CH_REQSEL_SIGSEL_VDAC0CH1 | LDMA_CH_REQSEL_SOURCESEL_VDAC0, dmadrvPeripheralSignal_CRYPTO0_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0, dmadrvPeripheralSignal_CRYPTO0_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0, dmadrvPeripheralSignal_CRYPTO0_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0, dmadrvPeripheralSignal_CRYPTO0_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0, dmadrvPeripheralSignal_CRYPTO0_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO0DATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO0, dmadrvPeripheralSignal_CRYPTO1_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1, dmadrvPeripheralSignal_CRYPTO1_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1, dmadrvPeripheralSignal_CRYPTO1_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1, dmadrvPeripheralSignal_CRYPTO1_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1, dmadrvPeripheralSignal_CRYPTO1_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTO1DATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO1, dmadrvPeripheralSignal_CSEN_DATA = LDMA_CH_REQSEL_SIGSEL_CSENDATA | LDMA_CH_REQSEL_SOURCESEL_CSEN, dmadrvPeripheralSignal_CSEN_BSLN = LDMA_CH_REQSEL_SIGSEL_CSENBSLN | LDMA_CH_REQSEL_SOURCESEL_CSEN, dmadrvPeripheralSignal_I2C0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C0, dmadrvPeripheralSignal_I2C0_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C0TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C0, dmadrvPeripheralSignal_I2C1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C1, dmadrvPeripheralSignal_I2C1_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C1TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C1, dmadrvPeripheralSignal_LEUART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_LEUART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_LEUART0_TXBL = LDMA_CH_REQSEL_SIGSEL_LEUART0TXBL | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_LEUART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_LEUART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_LEUART0, dmadrvPeripheralSignal_MSC_WDATA = LDMA_CH_REQSEL_SIGSEL_MSCWDATA | LDMA_CH_REQSEL_SOURCESEL_MSC, dmadrvPeripheralSignal_PRS_REQ0 = LDMA_CH_REQSEL_SIGSEL_PRSREQ0 | LDMA_CH_REQSEL_SOURCESEL_PRS, dmadrvPeripheralSignal_PRS_REQ1 = LDMA_CH_REQSEL_SIGSEL_PRSREQ1 | LDMA_CH_REQSEL_SOURCESEL_PRS, dmadrvPeripheralSignal_TIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER0, dmadrvPeripheralSignal_TIMER1_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_CC3 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC3 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_TIMER1_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER1UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER1, dmadrvPeripheralSignal_WTIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0, dmadrvPeripheralSignal_WTIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0, dmadrvPeripheralSignal_WTIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_WTIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_WTIMER0, dmadrvPeripheralSignal_WTIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_WTIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_WTIMER0, dmadrvPeripheralSignal_WTIMER1_CC0 = LDMA_CH_REQSEL_SIGSEL_WTIMER1CC0 | LDMA_CH_REQSEL_SOURCESEL_WTIMER1, dmadrvPeripheralSignal_WTIMER1_CC1 = LDMA_CH_REQSEL_SIGSEL_WTIMER1CC1 | LDMA_CH_REQSEL_SOURCESEL_WTIMER1, dmadrvPeripheralSignal_WTIMER1_CC2 = LDMA_CH_REQSEL_SIGSEL_WTIMER1CC2 | LDMA_CH_REQSEL_SOURCESEL_WTIMER1, dmadrvPeripheralSignal_WTIMER1_CC3 = LDMA_CH_REQSEL_SIGSEL_WTIMER1CC3 | LDMA_CH_REQSEL_SOURCESEL_WTIMER1, dmadrvPeripheralSignal_WTIMER1_UFOF = LDMA_CH_REQSEL_SIGSEL_WTIMER1UFOF | LDMA_CH_REQSEL_SOURCESEL_WTIMER1, dmadrvPeripheralSignal_USART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART0_TXBL = LDMA_CH_REQSEL_SIGSEL_USART0TXBL | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART0, dmadrvPeripheralSignal_USART1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_RXDATAVRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAVRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXBL = LDMA_CH_REQSEL_SIGSEL_USART1TXBL | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXBLRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1TXBLRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART1_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART1TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART1, dmadrvPeripheralSignal_USART2_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART2RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART2, dmadrvPeripheralSignal_USART2_TXBL = LDMA_CH_REQSEL_SIGSEL_USART2TXBL | LDMA_CH_REQSEL_SOURCESEL_USART2, dmadrvPeripheralSignal_USART2_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART2TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART2, dmadrvPeripheralSignal_USART3_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART3RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART3, dmadrvPeripheralSignal_USART3_RXDATAVRIGHT = LDMA_CH_REQSEL_SIGSEL_USART3RXDATAVRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART3, dmadrvPeripheralSignal_USART3_TXBL = LDMA_CH_REQSEL_SIGSEL_USART3TXBL | LDMA_CH_REQSEL_SOURCESEL_USART3, dmadrvPeripheralSignal_USART3_TXBLRIGHT = LDMA_CH_REQSEL_SIGSEL_USART3TXBLRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART3, dmadrvPeripheralSignal_USART3_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART3TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART3 } |
Peripherals that can trigger LDMA transfers. | |
Functions | |
Ecode_t | DMADRV_AllocateChannel (unsigned int *channelId, void *capabilities) |
Allocate (reserve) a DMA channel. | |
Ecode_t | DMADRV_DeInit (void) |
Deinitialize DMADRV. | |
Ecode_t | DMADRV_FreeChannel (unsigned int channelId) |
Free an allocated (reserved) DMA channel. | |
Ecode_t | DMADRV_Init (void) |
Initialize DMADRV. | |
Ecode_t | DMADRV_LdmaStartTransfer (int channelId, LDMA_TransferCfg_t *transfer, LDMA_Descriptor_t *descriptor, DMADRV_Callback_t callback, void *cbUserParam) |
Start an LDMA transfer. | |
Ecode_t | DMADRV_MemoryPeripheral (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) |
Start a memory to a peripheral DMA transfer. | |
Ecode_t | DMADRV_MemoryPeripheralPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src0, void *src1, bool srcInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) |
Start a memory to a peripheral ping-pong DMA transfer. | |
Ecode_t | DMADRV_PauseTransfer (unsigned int channelId) |
Pause an ongoing DMA transfer. | |
Ecode_t | DMADRV_PeripheralMemory (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) |
Start a peripheral to memory DMA transfer. | |
Ecode_t | DMADRV_PeripheralMemoryPingPong (unsigned int channelId, DMADRV_PeripheralSignal_t peripheralSignal, void *dst0, void *dst1, void *src, bool dstInc, int len, DMADRV_DataSize_t size, DMADRV_Callback_t callback, void *cbUserParam) |
Start a peripheral to memory ping-pong DMA transfer. | |
Ecode_t | DMADRV_ResumeTransfer (unsigned int channelId) |
Resume an ongoing DMA transfer. | |
Ecode_t | DMADRV_StopTransfer (unsigned int channelId) |
Stop an ongoing DMA transfer. | |
Ecode_t | DMADRV_TransferActive (unsigned int channelId, bool *active) |
Check if a transfer is running. | |
Ecode_t | DMADRV_TransferCompletePending (unsigned int channelId, bool *pending) |
Check if a transfer complete is pending. | |
Ecode_t | DMADRV_TransferDone (unsigned int channelId, bool *done) |
Check if a transfer has completed. | |
Ecode_t | DMADRV_TransferRemainingCount (unsigned int channelId, int *remaining) |
Get number of items remaining in a transfer. | |
Typedef Documentation
typedef bool(* DMADRV_Callback_t) (unsigned int channel, unsigned int sequenceNo, void *userParam) |
DMADRV transfer completion callback function.
The callback function is called when a transfer is complete.
- Parameters
-
[in] channel
The DMA channel number. [in] sequenceNo
The number of times the callback was called. Useful on long chains of linked transfers or on endless ping-pong type transfers. [in] userParam
Optional user parameter supplied on DMA invocation.
- Returns
- When doing ping-pong transfers, return true to continue or false to stop transfers.
Definition at line 80
of file dmadrv.h
.
Enumeration Type Documentation
enum DMADRV_DataSize_t |
Peripherals that can trigger LDMA transfers.
Definition at line 463
of file dmadrv.h
.
Function Documentation
Ecode_t DMADRV_AllocateChannel | ( | unsigned int * | channelId, |
void * | capabilities |
||
) |
Allocate (reserve) a DMA channel.
- Parameters
-
[out] channelId
The channel ID assigned by DMADRV. [in] capabilities
Not used.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 125
of file dmadrv.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_CHANNELS_EXHAUSTED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, and initialized.
Referenced by MIC_init(), and SPIDRV_Init().
Ecode_t DMADRV_DeInit | ( | void |
| ) |
Deinitialize DMADRV.
If DMA channels are not currently allocated, it will disable DMA hardware and mask associated interrupts.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 167
of file dmadrv.c
.
References CMU_ClockEnable(), CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_IN_USE, ECODE_EMDRV_DMADRV_OK, initialized, and LDMA_DeInit().
Referenced by SPIDRV_DeInit(), and UARTDRV_DeInit().
Ecode_t DMADRV_FreeChannel | ( | unsigned int | channelId | ) |
Free an allocated (reserved) DMA channel.
- Parameters
-
[in] channelId
The channel ID to free.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 212
of file dmadrv.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_ALREADY_FREED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, and initialized.
Referenced by MIC_deInit(), SPIDRV_DeInit(), and UARTDRV_DeInit().
Ecode_t DMADRV_Init | ( | void |
| ) |
Initialize DMADRV.
The DMA hardware is initialized.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 246
of file dmadrv.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, ECODE_EMDRV_DMADRV_ALREADY_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, LDMA_Init(), LDMA_INIT_DEFAULT, LDMA_Init_t::ldmaInitCtrlNumFixed, and LDMA_Init_t::ldmaInitIrqPriority.
Referenced by MIC_init(), and SPIDRV_Init().
Ecode_t DMADRV_LdmaStartTransfer | ( | int | channelId, |
LDMA_TransferCfg_t * | transfer, |
||
LDMA_Descriptor_t * | descriptor, |
||
DMADRV_Callback_t | callback, |
||
void * | cbUserParam |
||
) |
Start an LDMA transfer.
This function can only be used on LDMA when EMDRV_DMADRV_USE_NATIVE_API is defined. It is a wrapper similar to emlib LDMA function.
- Parameters
-
[in] channelId
The channel ID to use. [in] transfer
A DMA transfer configuration data structure. [in] descriptor
A DMA transfer descriptor, can be an array of descriptors linked together. [in] callback
An optional callback function for signalling completion. May be NULL if not needed. [in] cbUserParam
An optional user parameter to feed to the callback function. May be NULL if not needed.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 316
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_StartTransfer().
Referenced by MIC_init().
Ecode_t DMADRV_MemoryPeripheral | ( | unsigned int | channelId, |
DMADRV_PeripheralSignal_t | peripheralSignal, |
||
void * | dst, |
||
void * | src, |
||
bool | srcInc, |
||
int | len, |
||
DMADRV_DataSize_t | size, |
||
DMADRV_Callback_t | callback, |
||
void * | cbUserParam |
||
) |
Start a memory to a peripheral DMA transfer.
- Parameters
-
[in] channelId
The channel ID to use for the transfer. [in] peripheralSignal
Selects which peripheral/peripheralsignal to use. [in] dst
A destination (peripheral register) memory address. [in] src
A source memory address. [in] srcInc
Set to true to enable source address increment (increments according to size parameter). [in] len
A number of items (of size size) to transfer. [in] size
An item size, byte, halfword or word. [in] callback
A function to call on DMA completion, use NULL if not needed. [in] cbUserParam
An optional user parameter to feed to the callback function. Use NULL if not needed.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 384
of file dmadrv.c
.
Ecode_t DMADRV_MemoryPeripheralPingPong | ( | unsigned int | channelId, |
DMADRV_PeripheralSignal_t | peripheralSignal, |
||
void * | dst, |
||
void * | src0, |
||
void * | src1, |
||
bool | srcInc, |
||
int | len, |
||
DMADRV_DataSize_t | size, |
||
DMADRV_Callback_t | callback, |
||
void * | cbUserParam |
||
) |
Start a memory to a peripheral ping-pong DMA transfer.
- Parameters
-
[in] channelId
The channel ID to use for the transfer. [in] peripheralSignal
Selects which peripheral/peripheralsignal to use. [in] dst
A destination (peripheral register) memory address. [in] src0
A source memory address of the first (ping) buffer. [in] src1
A source memory address of the second (pong) buffer. [in] srcInc
Set to true to enable source address increment (increments according to size parameter). [in] len
A number of items (of size size) to transfer. [in] size
An item size, byte, halfword or word. [in] callback
A function to call on DMA completion, use NULL if not needed. [in] cbUserParam
An optional user parameter to feed to the callback function. Use NULL if not needed.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 451
of file dmadrv.c
.
Ecode_t DMADRV_PauseTransfer | ( | unsigned int | channelId | ) |
Pause an ongoing DMA transfer.
- Parameters
-
[in] channelId
The channel ID of the transfer to pause.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 623
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_EnableChannelRequest().
Referenced by UARTDRV_PauseTransmit().
Ecode_t DMADRV_PeripheralMemory | ( | unsigned int | channelId, |
DMADRV_PeripheralSignal_t | peripheralSignal, |
||
void * | dst, |
||
void * | src, |
||
bool | dstInc, |
||
int | len, |
||
DMADRV_DataSize_t | size, |
||
DMADRV_Callback_t | callback, |
||
void * | cbUserParam |
||
) |
Start a peripheral to memory DMA transfer.
- Parameters
-
[in] channelId
The channel ID to use for the transfer. [in] peripheralSignal
Selects which peripheral/peripheralsignal to use. [in] dst
A destination memory address. [in] src
A source memory (peripheral register) address. [in] dstInc
Set to true to enable destination address increment (increments according to size parameter). [in] len
A number of items (of size size) to transfer. [in] size
An item size, byte, halfword or word. [in] callback
A function to call on DMA completion, use NULL if not needed. [in] cbUserParam
An optional user parameter to feed to the callback function. Use NULL if not needed.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 517
of file dmadrv.c
.
Referenced by MIC_start().
Ecode_t DMADRV_PeripheralMemoryPingPong | ( | unsigned int | channelId, |
DMADRV_PeripheralSignal_t | peripheralSignal, |
||
void * | dst0, |
||
void * | dst1, |
||
void * | src, |
||
bool | dstInc, |
||
int | len, |
||
DMADRV_DataSize_t | size, |
||
DMADRV_Callback_t | callback, |
||
void * | cbUserParam |
||
) |
Start a peripheral to memory ping-pong DMA transfer.
- Parameters
-
[in] channelId
The channel ID to use for the transfer. [in] peripheralSignal
Selects which peripheral/peripheralsignal to use. [in] dst0
A destination memory address of the first (ping) buffer. [in] dst1
A destination memory address of the second (pong) buffer. [in] src
A source memory (peripheral register) address. [in] dstInc
Set to true to enable destination address increment (increments according to size parameter). [in] len
A number of items (of size size) to transfer. [in] size
An item size, byte, halfword or word. [in] callback
A function to call on DMA completion, use NULL if not needed. [in] cbUserParam
An optional user parameter to feed to the callback function. Use NULL if not needed.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 584
of file dmadrv.c
.
Ecode_t DMADRV_ResumeTransfer | ( | unsigned int | channelId | ) |
Resume an ongoing DMA transfer.
- Parameters
-
[in] channelId
The channel ID of the transfer to resume.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 657
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_EnableChannelRequest().
Referenced by UARTDRV_ResumeTransmit().
Ecode_t DMADRV_StopTransfer | ( | unsigned int | channelId | ) |
Stop an ongoing DMA transfer.
- Parameters
-
[in] channelId
The channel ID of the transfer to stop.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 691
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_StopTransfer().
Referenced by MIC_deInit(), SPIDRV_AbortTransfer(), SPIDRV_DeInit(), and UARTDRV_Abort().
Ecode_t DMADRV_TransferActive | ( | unsigned int | channelId, |
bool * | active |
||
) |
Check if a transfer is running.
- Parameters
-
[in] channelId
The channel ID of the transfer to check. [out] active
True if transfer is running, false otherwise.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 728
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_ChannelEnabled().
Ecode_t DMADRV_TransferCompletePending | ( | unsigned int | channelId, |
bool * | pending |
||
) |
Check if a transfer complete is pending.
Will check the channel interrupt flag. This assumes that the DMA is configured to give a completion interrupt.
- Parameters
-
[in] channelId
The channel ID of the transfer to check. [out] pending
True if a transfer complete is pending, false otherwise.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 775
of file dmadrv.c
.
References ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA.
Ecode_t DMADRV_TransferDone | ( | unsigned int | channelId, |
bool * | done |
||
) |
Check if a transfer has completed.
- Note
- This function should be used in a polled environment. Will only work reliably for transfers NOT using the completion interrupt. On UDMA, it will only work on basic transfers on the primary channel.
- Parameters
-
[in] channelId
The channel ID of the transfer to check. [out] done
True if a transfer has completed, false otherwise.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 823
of file dmadrv.c
.
References CORE_ATOMIC_SECTION, ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_TransferDone().
Ecode_t DMADRV_TransferRemainingCount | ( | unsigned int | channelId, |
int * | remaining |
||
) |
Get number of items remaining in a transfer.
- Note
- This function does not take into account that a DMA transfer with a chain of linked transfers might be ongoing. It will only check the count for the current transfer. On UDMA, it will only work on the primary channel.
- Parameters
-
[in] channelId
The channel ID of the transfer to check. [out] remaining
A number of items remaining in the transfer.
- Returns
- ECODE_EMDRV_DMADRV_OK on success. On failure, an appropriate DMADRV Ecode_t is returned.
Definition at line 883
of file dmadrv.c
.
References CORE_ATOMIC_SECTION, ECODE_EMDRV_DMADRV_CH_NOT_ALLOCATED, ECODE_EMDRV_DMADRV_NOT_INITIALIZED, ECODE_EMDRV_DMADRV_OK, ECODE_EMDRV_DMADRV_PARAM_ERROR, initialized, and LDMA_TransferRemainingCount().
Referenced by SPIDRV_AbortTransfer(), UARTDRV_Abort(), UARTDRV_GetReceiveStatus(), and UARTDRV_GetTransmitStatus().