CRYOTIMER_TypeDef Struct ReferenceDevices > CRYOTIMER
CRYOTIMER Register Declaration
Definition at line 49
of file efm32pg12b_cryotimer.h
.
#include <
efm32pg12b_cryotimer.h
>
Data Fields | |
__IM uint32_t | CNT |
__IOM uint32_t | CTRL |
__IOM uint32_t | EM4WUEN |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PERIODSEL |
Field Documentation
__IM uint32_t CRYOTIMER_TypeDef::CNT |
Counter Value
Definition at line 52
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::EM4WUEN |
Wake Up Enable
Definition at line 53
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::IEN |
Interrupt Enable Register
Definition at line 57
of file efm32pg12b_cryotimer.h
.
__IM uint32_t CRYOTIMER_TypeDef::IF |
Interrupt Flag Register
Definition at line 54
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 56
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 55
of file efm32pg12b_cryotimer.h
.
__IOM uint32_t CRYOTIMER_TypeDef::PERIODSEL |
Interrupt Duration
Definition at line 51
of file efm32pg12b_cryotimer.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG12B/Include/
efm32pg12b_cryotimer.h