HidKeyboardKit Drivers
Detailed Description
Implements a USB HID class keyboard.
HIDKBD implementation.
The source code of the HIDKBD implementation resides in kits/common/drivers/hidkbd.c and hidkbd.h
. This driver implements a basic USB keyboard. Refer to hidkbd examples for STK3700 and DK3750 for examples using this driver.
HIDKBD device configuration options.
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko STK3700 hidbkd example.
// USB interface number. Interfaces are numbered from zero to one less than // the number of concurrent interfaces supported by the configuration. // The interfac numbers must be 0 standalone HID device, for a // composite device which includes a HID interface it must not be in conflict // with other device interfaces. #define HIDKBD_INTERFACE_NO 0 // Endpoint address for HID input reports. #define HIDKBD_INTR_IN_EP_ADDR 0x81 // The bInterval reported with the interrupt IN endpoint descriptor. #define HIDKBD_POLL_RATE 24 // Timer id, see USBTIMER in the USB device stack documentation. // The HID driver use a timer to implement the idle-rate defined in the HID class spec. #define HIDKBD_IDLE_TIMER 0
Data Structures | |
struct | HIDKBD_Init_t |
struct | HIDKBD_KeyReport_t |
Typedefs | |
typedef void(* | HIDKBD_SetReportFunc_t) (uint8_t report) |
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device. | |
Functions | |
void | HIDKBD_Init (HIDKBD_Init_t *init) |
Initialize HID Keyboard driver. | |
void | HIDKBD_KeyboardEvent (HIDKBD_KeyReport_t *report) |
Report a keyboard press/release event. | |
int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) |
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command. | |
void | HIDKBD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
Handle USB state change events, this function must be called each time the USB device state is changed. | |
Variables | |
const char | HIDKBD_ReportDescriptor [69] |
Typedef Documentation
typedef void(* HIDKBD_SetReportFunc_t) (uint8_t report) |
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
- Parameters
-
[in] report
Output report byte.
Bit 0 : State of keyboard NumLock LED.
Bit 1 : State of keyboard CapsLock LED.
Bit 2 : State of keyboard ScrollLock LED.
Definition at line 57
of file hidkbd.h
.
Function Documentation
void HIDKBD_Init | ( | HIDKBD_Init_t * | init | ) |
Initialize HID Keyboard driver.
- Parameters
-
[in] init
Pointer to a HIDKBD_Init_t struct with configuration options.
Definition at line 187
of file hidkbd.c
.
References HIDKBD_Init_t::hidDescriptor, and HIDKBD_Init_t::setReportFunc.
void HIDKBD_KeyboardEvent | ( | HIDKBD_KeyReport_t * | report | ) |
Report a keyboard press/release event.
- Parameters
-
[in] report
Pointer to a HIDKBD_KeyReport_t struct with new key pressed information.
Definition at line 202
of file hidkbd.c
.
int HIDKBD_SetupCmd | ( | const USB_Setup_TypeDef * | setup | ) |
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
- Parameters
-
[in] setup
Pointer to the setup packet received.
- Returns
- USB_STATUS_OK if command accepted, USB_STATUS_REQ_UNHANDLED when command is unknown. In the latter case the USB device stack will handle the request.
Definition at line 229
of file hidkbd.c
.
References SL_MIN.
void HIDKBD_StateChangeEvent | ( | USBD_State_TypeDef | oldState, |
USBD_State_TypeDef | newState |
||
) |
Handle USB state change events, this function must be called each time the USB device state is changed.
- Parameters
-
[in] oldState
The device state the device has just left. [in] newState
The new device state.
Definition at line 326
of file hidkbd.c
.
References DEFAULT_IDLE_RATE.