DMA_DESCRIPTOR_TypeDef Struct ReferenceDevices > DMA Descriptor

DMA_DESCRIPTOR Register Declaration

Definition at line 48 of file efr32fg1p_dma_descriptor.h .

#include < efr32fg1p_dma_descriptor.h >

Data Fields

__IOM uint32_t CTRL
__IOM void *__IOM DST
__IOM void *__IOM LINK
__IOM void *__IOM SRC

Field Documentation

__IOM uint32_t DMA_DESCRIPTOR_TypeDef::CTRL

DMA control register

Definition at line 51 of file efr32fg1p_dma_descriptor.h .

__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::DST

DMA destination address

Definition at line 53 of file efr32fg1p_dma_descriptor.h .

__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::LINK

DMA link address

Definition at line 54 of file efr32fg1p_dma_descriptor.h .

__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::SRC

DMA source address

Definition at line 52 of file efr32fg1p_dma_descriptor.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG1P/Include/ efr32fg1p_dma_descriptor.h