TempSensorKit Drivers
         Data Structures | 
       |
| struct | TEMPSENS_Temp_TypeDef | 
         Macros | 
       |
| #define | TEMPSENS_DK_ADDR 0x90 | 
         Enumerations | 
       |
| enum | 
         
          TEMPSENS_Register_TypeDef
         
         {
          tempsensRegTemp = 0, tempsensRegConfig = 1, tempsensRegHysteresis = 2, tempsensRegShutdown = 3 }  | 
       
         Functions | 
       |
| void | TEMPSENS_Celsius2Fahrenheit ( TEMPSENS_Temp_TypeDef *temp) | 
| 
         Convert temperature from Celsius to Fahrenheit.
          | 
       |
| int | TEMPSENS_RegisterGet ( I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t *val) | 
| 
         Read sensor register content.
          | 
       |
| int | TEMPSENS_RegisterSet ( I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t val) | 
| 
         Write to sensor register.
          | 
       |
| int | TEMPSENS_TemperatureGet ( I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Temp_TypeDef *temp) | 
| 
         Fetch current temperature from temperature sensor (in Celsius).
          | 
       |
Macro Definition Documentation
| #define TEMPSENS_DK_ADDR 0x90 | 
I2C device address for temperature sensor on DK
        Definition at line
        
         41
        
        of file
        
         tempsens.h
        
        .
       
Enumeration Type Documentation
Function Documentation
| void TEMPSENS_Celsius2Fahrenheit | ( | TEMPSENS_Temp_TypeDef * | 
           
            temp
           
           | 
          ) | 
Convert temperature from Celsius to Fahrenheit.
- Parameters
 - 
         
[in,out] tempReference to structure to holding temperature in Celsius to convert. Upon return, it has been changed to Fahrenheit.  
        Definition at line
        
         32
        
        of file
        
         tempsens.c
        
        .
       
References TEMPSENS_Temp_TypeDef::f , and TEMPSENS_Temp_TypeDef::i .
| int TEMPSENS_RegisterGet | ( | I2C_TypeDef * | 
           
            i2c,
           
           | 
         
| uint8_t | 
           
            addr,
           
           | 
         ||
| TEMPSENS_Register_TypeDef | 
           
            reg,
           
           | 
         ||
| uint16_t * | 
           
            val
           
           | 
         ||
| ) | 
Read sensor register content.
If reading the temperature register, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Parameters
 - 
         
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to read. [out] valReference to place register read.  
- Returns
 - Returns 0 if register read, <0 if unable to read register.
 
        Definition at line
        
         73
        
        of file
        
         tempsens.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_READ , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , and tempsensRegConfig .
Referenced by TEMPSENS_TemperatureGet() .
| int TEMPSENS_RegisterSet | ( | I2C_TypeDef * | 
           
            i2c,
           
           | 
         
| uint8_t | 
           
            addr,
           
           | 
         ||
| TEMPSENS_Register_TypeDef | 
           
            reg,
           
           | 
         ||
| uint16_t | 
           
            val
           
           | 
         ||
| ) | 
Write to sensor register.
- Parameters
 - 
         
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] regRegister to write (temperature register cannot be written). [in] valValue used when writing to register.  
- Returns
 - Returns 0 if register written, <0 if unable to write to register.
 
        Definition at line
        
         130
        
        of file
        
         tempsens.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE , I2CSPM_Transfer() , i2cTransferDone , I2C_TransferSeq_TypeDef::len , tempsensRegConfig , and tempsensRegTemp .
| int TEMPSENS_TemperatureGet | ( | I2C_TypeDef * | 
           
            i2c,
           
           | 
         
| uint8_t | 
           
            addr,
           
           | 
         ||
| TEMPSENS_Temp_TypeDef * | 
           
            temp
           
           | 
         ||
| ) | 
Fetch current temperature from temperature sensor (in Celsius).
If reading the temperature, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Note
 - The sensor on the the DK, STDS75, does not seem to have any check on max temperature limit, ie when exceeding specified max 125 C limit, it will keep increasing 9 bit counter to max representable 9 bit value of 127.5 C and then flip over to negative numbers. There is no limit check in this implementation on such issues.
 
- Parameters
 - 
         
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [out] tempReference to structure to place temperature (in Celsius).  
- Returns
 - Returns 0 if temperature read, <0 if unable to read temperature.
 
        Definition at line
        
         197
        
        of file
        
         tempsens.c
        
        .
       
References TEMPSENS_Temp_TypeDef::f , TEMPSENS_Temp_TypeDef::i , TEMPSENS_RegisterGet() , and tempsensRegTemp .