PCNT_Filter_TypeDef Struct ReferenceEMLIB > PCNT
Filter initialization structure
Definition at line 265
of file em_pcnt.h
.
#include <
em_pcnt.h
>
Data Fields | |
uint8_t | filtLen |
bool | flutterrm |
Field Documentation
uint8_t PCNT_Filter_TypeDef::filtLen |
Used only in OVSINGLE and OVSQUAD1X-4X modes. To use this, enable filter by setting filter to true during PCNT_Init(). Filter length = (filtLen + 5) LFACLK cycles.
Definition at line 268
of file em_pcnt.h
.
Referenced by PCNT_FilterConfiguration().
bool PCNT_Filter_TypeDef::flutterrm |
When set, removes flutter from Quaddecoder inputs S0IN and S1IN. Available only in OVSQUAD1X-4X modes.
Definition at line 272
of file em_pcnt.h
.
Referenced by PCNT_FilterConfiguration().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_pcnt.h