USART_InitAsync_TypeDef Struct ReferenceEMLIB > USART
Asynchronous mode initialization structure.
       Definition at line
       
        283
       
       of file
       
        em_usart.h
       
       .
      
      
       #include <
       
     
        em_usart.h
       
       >
      
         Data Fields | 
       |
| bool | autoCsEnable | 
| uint8_t | autoCsHold | 
| uint8_t | autoCsSetup | 
| uint32_t | baudrate | 
| USART_Databits_TypeDef | databits | 
| USART_Enable_TypeDef | enable | 
| USART_HwFlowControl_TypeDef | hwFlowControl | 
| bool | mvdis | 
| USART_OVS_TypeDef | oversampling | 
| USART_Parity_TypeDef | parity | 
| USART_PRS_Channel_t | prsRxCh | 
| bool | prsRxEnable | 
| uint32_t | refFreq | 
| USART_Stopbits_TypeDef | stopbits | 
Field Documentation
| bool USART_InitAsync_TypeDef::autoCsEnable | 
| uint8_t USART_InitAsync_TypeDef::autoCsHold | 
Auto CS hold time in baud cycles.
        Definition at line
        
         325
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| uint8_t USART_InitAsync_TypeDef::autoCsSetup | 
Auto CS setup time in baud cycles.
        Definition at line
        
         328
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| uint32_t USART_InitAsync_TypeDef::baudrate | 
Desired baud rate.
        Definition at line
        
         294
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
| USART_Databits_TypeDef USART_InitAsync_TypeDef::databits | 
Number of data bits in frame. Notice that UART modules only support 8 or 9 data bits.
        Definition at line
        
         301
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
| USART_Enable_TypeDef USART_InitAsync_TypeDef::enable | 
Specifies whether TX and/or RX is enabled when initialization is completed.
        Definition at line
        
         285
        
        of file
        
         em_usart.h
        
        .
       
Referenced by RETARGET_SerialInit() , UARTDRV_InitUart() , and USART_InitAsync() .
| USART_HwFlowControl_TypeDef USART_InitAsync_TypeDef::hwFlowControl | 
Hardware flow control mode.
        Definition at line
        
         331
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| bool USART_InitAsync_TypeDef::mvdis | 
Majority Vote Disable for 16x, 8x and 6x oversampling modes.
        Definition at line
        
         311
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
| USART_OVS_TypeDef USART_InitAsync_TypeDef::oversampling | 
Oversampling used.
        Definition at line
        
         297
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
| USART_Parity_TypeDef USART_InitAsync_TypeDef::parity | 
Parity mode to use.
        Definition at line
        
         304
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
| USART_PRS_Channel_t USART_InitAsync_TypeDef::prsRxCh | 
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
        Definition at line
        
         317
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| bool USART_InitAsync_TypeDef::prsRxEnable | 
Enable USART Rx via PRS.
        Definition at line
        
         314
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| uint32_t USART_InitAsync_TypeDef::refFreq | 
USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.
        Definition at line
        
         291
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitAsync() .
| USART_Stopbits_TypeDef USART_InitAsync_TypeDef::stopbits | 
Number of stop bits to use.
        Definition at line
        
         307
        
        of file
        
         em_usart.h
        
        .
       
Referenced by UARTDRV_InitUart() , and USART_InitAsync() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_usart.h