CRYOTIMER_Init_TypeDef Struct ReferenceEMLIB > CRYOTIMER

CRYOTIMER initialization structure.

Definition at line 179 of file em_cryotimer.h .

#include < em_cryotimer.h >

Data Fields

bool debugRun
bool em4Wakeup
bool enable
CRYOTIMER_Osc_TypeDef osc
CRYOTIMER_Period_TypeDef period
CRYOTIMER_Presc_TypeDef presc

Field Documentation

bool CRYOTIMER_Init_TypeDef::debugRun

Enable/disable timer counting during debug halt.

Definition at line 184 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .

bool CRYOTIMER_Init_TypeDef::em4Wakeup

Enable/disable EM4 Wakeup.

Definition at line 187 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .

bool CRYOTIMER_Init_TypeDef::enable

Enable/disable counting when initialization is complete.

Definition at line 181 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .

CRYOTIMER_Osc_TypeDef CRYOTIMER_Init_TypeDef::osc

Select the oscillator for the CRYOTIMER.

Definition at line 190 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .

CRYOTIMER_Period_TypeDef CRYOTIMER_Init_TypeDef::period

A period between a wakeup event/interrupt.

Definition at line 196 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .

CRYOTIMER_Presc_TypeDef CRYOTIMER_Init_TypeDef::presc

Prescaler.

Definition at line 193 of file em_cryotimer.h .

Referenced by CRYOTIMER_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_cryotimer.h