ROMTABLE_TypeDef Struct ReferenceDevices > ROM Table, Chip Revision Information
ROMTABLE Register Declaration
Definition at line 49
of file efr32mg12p_romtable.h
.
#include <
efr32mg12p_romtable.h
>
Data Fields | |
__IM uint32_t | CID0 |
__IM uint32_t | PID0 |
__IM uint32_t | PID1 |
__IM uint32_t | PID2 |
__IM uint32_t | PID3 |
__IM uint32_t | PID4 |
__IM uint32_t | PID5 |
__IM uint32_t | PID6 |
__IM uint32_t | PID7 |
Field Documentation
__IM uint32_t ROMTABLE_TypeDef::CID0 |
Unused
Definition at line 58
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID0 |
Chip family LSB, chip major revision
Definition at line 54
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID1 |
JEP_106_NO, Chip family MSB
Definition at line 55
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID2 |
Chip minor rev MSB, JEP_106_PRESENT, JEP_106_NO
Definition at line 56
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID3 |
Chip minor rev LSB
Definition at line 57
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID4 |
JEP_106_BANK
Definition at line 50
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID5 |
Unused
Definition at line 51
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID6 |
Unused
Definition at line 52
of file efr32mg12p_romtable.h
.
__IM uint32_t ROMTABLE_TypeDef::PID7 |
Unused
Definition at line 53
of file efr32mg12p_romtable.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/
efr32mg12p_romtable.h