HIDKBD_KeyReport_t Struct ReferenceKit Drivers > HidKeyboard
HID keyboard input report definition.
Definition at line 38
of file hidkbd.h
.
#include <
hidkbd.h
>
Data Fields | |
uint8_t | key [6] |
uint8_t | modifier |
uint8_t | reserved |
Field Documentation
uint8_t HIDKBD_KeyReport_t::key[6] |
Array of 6 key array indices, key index codes are defined in the "Keyboard page" section of "USB HID Usage Tables document", also refer to usbkbdscancodes.c.
Definition at line 41
of file hidkbd.h
.
uint8_t HIDKBD_KeyReport_t::modifier |
Key modifier byte as defined in HID spec. section "8.3 Report Format for Array Items".
Definition at line 39
of file hidkbd.h
.
uint8_t HIDKBD_KeyReport_t::reserved |
Reserved, should be set to zero.
Definition at line 40
of file hidkbd.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
hidkbd.h