NUMBER_TypeDef Struct Reference

Defines segment COM and BIT fields numeric display.

Definition at line 74 of file segmentlcd.c .

Data Fields

uint8_t bit [7]
uint8_t com [7]

Field Documentation

uint8_t NUMBER_TypeDef::bit[7]

LCD bit number

Definition at line 76 of file segmentlcd.c .

Referenced by SegmentLCD_Number() , and SegmentLCD_UnsignedHex() .

uint8_t NUMBER_TypeDef::com[7]

LCD COM line (for multiplexing)

Definition at line 75 of file segmentlcd.c .

Referenced by SegmentLCD_Number() , and SegmentLCD_UnsignedHex() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/ segmentlcd.c