em_usbxpress.c File Reference
USBXpress global variable declaration, initialization, and call-back.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
       Definition in file
       
        em_usbxpress.c
       
       .
      
       #include <stddef.h>
      
      
       #include <stdbool.h>
      
      
       #include "
       
        em_usbxpress_internal.h
       
       "
      
      
       #include "
       
        em_usbxpress_descriptors.h
       
       "
      
      
       #include "
       
        em_usbxpress.h
       
       "
      
      
         Functions | 
       |
| USB_DeviceDescriptor_TypeDef USBXCORE_deviceDesc | SL_ATTRIBUTE_ALIGN (4) | 
| 
         Copy of device descriptor, so it can be edited.
          | 
       |
| void | USBX_apiCallbackDisable (void) | 
| 
         Inhibits user API call-backs and does NOT disable the USB interrupt.
          | 
       |
| void | USBX_apiCallbackEnable ( USBX_apiCallback_t f) | 
| 
         Enables user API call-backs.
          | 
       |
| int | USBX_blockRead (uint8_t *block, uint32_t numBytes, uint32_t *countPtr) | 
| 
         User API function to get data from host.
          | 
       |
| int | USBX_blockWrite (uint8_t *block, uint32_t numBytes, uint32_t *countPtr) | 
| 
         User API function to send data to host.
          | 
       |
| USBX_BUF (USBXCORE_overflowBuffer, USB_FS_BULK_EP_MAXSIZE ) | |
| 
         Buffer to hold overflow rx data if a ZLP read returns more than zero bytes.
          | 
       |
| void | USBX_disable (void) | 
| 
         Disables the USB interface.
          | 
       |
| uint32_t | USBX_getCallbackSource (void) | 
| 
         User API function to get the call-back source.
          | 
       |
| uint_least16_t | USBX_getLibraryVersion (void) | 
| 
         Returns the USBXpress library version.
          | 
       |
| void | USBX_init ( USBX_Init_t *p) | 
| 
         User API USB initialization function.
          | 
       |
| void | USBX_jumpCallback (void) | 
| 
         Conditionally jumps to the user call-back routine.
          | 
       |
| void | USBXCORE_resetState (void) | 
| 
         Resets internal USBXpress variables.
          | 
       |
         Variables | 
       |
| uint32_t | USBXCORE_apiEa | 
| 
         Enable or disable status of USB_API interrupts.
          | 
       |
| uint32_t | USBXCORE_apiIntValue | 
| 
         Byte holding the current USB_API interrupts.
          | 
       |
| uint32_t * | USBXCORE_byteCountInPtr | 
| 
         Pointer to variable holding number of bytes written.
          | 
       |
| uint32_t * | USBXCORE_byteCountOutPtr | 
| 
         Pointer to variable holding number of bytes read.
          | 
       |
| uint32_t | USBXCORE_readSize | 
| 
         Number of bytes sent to
         
          USBX_blockRead()
         
         as numBytes.
          | 
       |
| bool | USBXCORE_rxOverflowPacketAvailable = false | 
| 
         Boolean indicating if data was received while expecting a ZLP.
          | 
       |
| uint32_t | USBXCORE_rxOverflowPacketSize = 0 | 
| 
         Size of Rx Overflow Packet.
          | 
       |
| USB_StringDescriptor_TypeDef const * | USBXCORE_stringDescTable [4] | 
| 
         Table of pointers to various string descriptors.
          | 
       |
| uint32_t | USBXCORE_writeSize | 
| 
         Number of bytes sent to
         
          USBX_blockWrite()
         
         as numBytes.
          | 
       |
| bool | USBXCORE_zlpActive = false | 
| 
         Boolean indicating whether a ZLP read is active.
          | 
       |
Function Documentation
| const USB_ExtendedPropertiesDescriptor_t USBXCORE_extendedPropertiesDesc SL_ATTRIBUTE_ALIGN | ( | 4 | 
           
           
           | 
          ) | 
          EXT_COMP_DESC_SIZE
         
         ,
        
          FEATURE_EXTENDED_COMPATIBILITY_ID
         
         ,
        
          NUM_IFCS_WITH_EXT_COMPAT
         
         ,
        
           FEATURE_EXTENDED_COMPATIBILITY_ID
          
         
           em_usbxpress_descriptors.h:47
          
         
           NUM_IFCS_WITH_EXT_COMPAT
          
         
           em_usbxpress_descriptors.h:56
          
         
           EXT_COMP_DESC_SIZE
          
         
           em_usbxpress_descriptors.h:51
          
         Copy of device descriptor, so it can be edited.
Extended Properties Descriptor.
Compatible ID Feature Descriptor.
Copy of configuration descriptor.
| void USBX_jumpCallback | ( | void | 
           
           
           | 
          ) | 
Conditionally jumps to the user call-back routine.
If the user call-back routine is already in progress, this function does nothing. Otherwise, this function jumps to the call-back defined via USBX_callbackEnable().
        Definition at line
        
         255
        
        of file
        
         em_usbxpress.c
        
        .
       
Referenced by USBX_DeviceStateChangeCb() , USBX_inXferCompleteCb() , USBX_outXferCompleteCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .
| void USBXCORE_resetState | ( | void | 
           
           
           | 
          ) | 
Resets internal USBXpress variables.
This function resets the internal USBXpress variables. It should be called after a cancel-type event (USBXpress Close, USB de-configure, FIFO flush, etc.).
        Definition at line
        
         267
        
        of file
        
         em_usbxpress.c
        
        .
       
References USBXCORE_rxOverflowPacketAvailable , and USBXCORE_zlpActive .
Referenced by USBX_DeviceStateChangeCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .