Deprecated List
- globalScope> Global _SILICON_LABS_32B_PLATFORM
- Silicon Labs platform name
- globalScope> Global _SILICON_LABS_32B_PLATFORM_2
- Silicon Labs platform name
- globalScope> Global _SILICON_LABS_32B_PLATFORM_2_GEN
- Platform 2, generation 1
- globalScope> Global _SILICON_LABS_32B_PLATFORM_2_GEN_1
- Platform 2, generation 1
- globalScope> Global AES_CBC128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_CBC128 instead.
- globalScope> Global AES_CBC256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_CBC256 instead.
- globalScope> Global AES_CFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_CFB128 instead.
- globalScope> Global AES_CFB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_CFB256 instead.
- globalScope> Global AES_CTR128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, uint8_t *ctr, CRYPTO_AES_CtrFuncPtr_TypeDef ctrFunc)
- This function preserves backwards compatibility. Use CRYPTO_AES_CTR128 instead.
- globalScope> Global AES_CTR256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, uint8_t *ctr, CRYPTO_AES_CtrFuncPtr_TypeDef ctrFunc)
- This function preserves backwards compatibility. Use CRYPTO_AES_CTR256 instead.
- globalScope> Global AES_CTRUpdate32Bit (uint8_t *ctr)
- This function preserves backwards compatibility. Use CRYPTO_AES_CTRUpdate32Bit instead.
- globalScope> Global AES_DecryptKey128 (uint8_t *out, const uint8_t *in)
- This function preserves backwards compatibility. Use CRYPTO_AES_DecryptKey128 instead.
- globalScope> Global AES_DecryptKey256 (uint8_t *out, const uint8_t *in)
- This function preserves backwards compatibility. Use CRYPTO_AES_DecryptKey256 instead.
- globalScope> Global AES_ECB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_ECB128 instead.
- globalScope> Global AES_ECB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, bool encrypt)
- This function preserves backwards compatibility. Use CRYPTO_AES_ECB256 instead.
- globalScope> Global AES_OFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv)
- This function preserves backwards compatibility. Use CRYPTO_AES_OFB128 instead.
- globalScope> Global AES_OFB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv)
- This function preserves backwards compatibility. Use CRYPTO_AES_OFB256 instead.
- globalScope> Global BSP_TraceSwoSetup (void)
- Deprecated function. New code should call BSP_TraceProfilerSetup() .
- globalScope> Global CMU_AUXHFRCOFreqGet (void)
- A deprecated function. New code should use CMU_AUXHFRCOBandGet() .
- globalScope> Global CMU_AUXHFRCOFreqSet (CMU_AUXHFRCOFreq_TypeDef setFreq)
- A deprecated function. New code should use CMU_AUXHFRCOBandSet() .
- globalScope> Global CMU_HFRCOFreqGet (void)
- A deprecated function. New code should use CMU_HFRCOBandGet() .
- globalScope> Global CMU_HFRCOFreqSet (CMU_HFRCOFreq_TypeDef setFreq)
- A deprecated function. New code should use CMU_HFRCOBandSet() .
- Global CMU_HFXOInit_TypeDef::autoSelEm01
- Use CMU_HFXOAutostartEnable instead.
- Global CMU_HFXOInit_TypeDef::autoStartEm01
- Use CMU_HFXOAutostartEnable instead.
- Global CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup
- Use CMU_HFXOAutostartEnable instead.
- globalScope> Global EMU_MemPwrDown (uint32_t blocks)
- This function is deprecated, use EMU_RamPowerDown() instead which maps a user provided memory range into RAM blocks to power down.
- globalScope> Global EMU_UpdateOscConfig (void)
- Oscillator status is saved in EMU_EnterEM2() and EMU_EnterEM3() .
- globalScope> Global GPIO_IntConfig (GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable)
- Deprecated function. New code should use GPIO_ExtIntConfig() .
- Module INT
- These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE .
- globalScope> Global INT_Disable (void)
- Deprecated and marked for removal in a later release. Use new CORE module instead.
- globalScope> Global INT_Enable (void)
- Deprecated and marked for removal in a later release. Use the new CORE module instead.
- Module MPU
- These functions are deprecated and marked for removal in a later release. Use ARM's ARM_MPU_xxx API instead. See file platform/CMSIS/Include/mpu_armv7.h or mpu_armv8.h
- globalScope> Global MPU_ConfigureRegion (const MPU_RegionInit_TypeDef *init)
- Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_SetRegion(), ARM_MPU_SetRegionEx(), ARM_MPU_Load() or similar instead.
- globalScope> Global MPU_Disable (void)
-
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Disable() instead.
- globalScope> Global MPU_Enable (uint32_t flags)
-
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Enable() instead.
- Module NVM
- This driver is deprecated and marked for removal in a later release. New code should use NVM3 .
- globalScope> Global setupSWOForPrint
- Use RETARGET_SwoInit instead
- globalScope> Global SLEEP_Init (SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
- New code should use the SLEEP_InitEx function for initializing the sleep module.
- globalScope> Global UARTDRV_Init (UARTDRV_Handle_t handle, UARTDRV_InitUart_t *initData)
- Deprecated; Use UARTDRV_InitUart() instead.
- globalScope> Global USART_InitIrDA (const USART_InitIrDA_TypeDef *init)
- Deprecated function. New code should use USARTn_InitIrDA() . This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
- globalScope> Global WDOG_Enable (bool enable)
- Deprecated function. New code should use WDOGn_Enable() . This function uses DEFAULT_WDOG .
- globalScope> Global WDOG_Feed (void)
- Deprecated function. New code should use WDOGn_Feed() . This function uses DEFAULT_WDOG .
- globalScope> Global WDOG_Init (const WDOG_Init_TypeDef *init)
- Deprecated function. New code should use WDOGn_Init() . This function uses DEFAULT_WDOG .
- globalScope> Global WDOG_IsEnabled (void)
- Deprecated function. New code should use WDOGn_IsEnabled() . This function uses DEFAULT_WDOG .
- globalScope> Global WDOG_IsLocked (void)
- Deprecated function. New code should use WDOGn_IsLocked() . This function uses DEFAULT_WDOG .
- globalScope> Global WDOG_Lock (void)
- Deprecated function. New code should use WDOGn_Lock() . This function uses DEFAULT_WDOG .