__HALL_Config Struct ReferenceBSP > Thunderboard Sense BSP > HALL - Hall Effect Sensor
Structure to configure the Hall effect sensor device.
Definition at line 54
of file hall.h
.
#include <
hall.h
>
Data Fields | |
float | hysteresis |
bool | outputInvert |
uint8_t | polarity |
float | threshold |
Field Documentation
float __HALL_Config::hysteresis |
bool __HALL_Config::outputInvert |
The polarity of the output pin
Definition at line 58
of file hall.h
.
Referenced by HALL_configure().
uint8_t __HALL_Config::polarity |
Magnetic field polarity setting
Definition at line 57
of file hall.h
.
Referenced by HALL_configure().
float __HALL_Config::threshold |
Decision point for magnetic field high or low in mT
Definition at line 55
of file hall.h
.
Referenced by HALL_configure().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/hardware/kit/common/bsp/thunderboard/
hall.h