NUMBER_TypeDef Struct ReferenceKit Drivers > SegmentLcd
Defines segment COM and BIT fields numeric display.
Definition at line 91
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [7] |
uint8_t | com [7] |
Field Documentation
uint8_t NUMBER_TypeDef::bit[7] |
LCD bit number
Definition at line 93
of file segmentlcd.c
.
Referenced by SegmentLCD_Number(), and SegmentLCD_UnsignedHex().
uint8_t NUMBER_TypeDef::com[7] |
LCD COM line (for multiplexing)
Definition at line 92
of file segmentlcd.c
.
Referenced by SegmentLCD_Number(), and SegmentLCD_UnsignedHex().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/hardware/kit/common/drivers/
segmentlcd.c