GPIO_TypeDef Struct ReferenceDevices > GPIO
GPIO Register Declaration
Definition at line
48
of file
efr32bg1p_gpio.h
.
#include <
efr32bg1p_gpio.h
>
Data Fields |
|
| __IOM uint32_t | EM4WUEN |
| __IOM uint32_t | EXTIFALL |
| __IOM uint32_t | EXTILEVEL |
| __IOM uint32_t | EXTIPINSELH |
| __IOM uint32_t | EXTIPINSELL |
| __IOM uint32_t | EXTIPSELH |
| __IOM uint32_t | EXTIPSELL |
| __IOM uint32_t | EXTIRISE |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | INSENSE |
| __IOM uint32_t | LOCK |
| GPIO_P_TypeDef | P [6U] |
| uint32_t | RESERVED0 [184U] |
| uint32_t | RESERVED1 [4U] |
| uint32_t | RESERVED2 [2U] |
| __IOM uint32_t | ROUTELOC0 |
| __IOM uint32_t | ROUTEPEN |
Field Documentation
| __IOM uint32_t GPIO_TypeDef::EM4WUEN |
EM4 Wake Up Enable Register
Definition at line
63
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIFALL |
External Interrupt Falling Edge Trigger Register
Definition at line
57
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTILEVEL |
External Interrupt Level Register
Definition at line
58
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIPINSELH |
External Interrupt Pin Select High Register
Definition at line
55
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIPINSELL |
External Interrupt Pin Select Low Register
Definition at line
54
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIPSELH |
External Interrupt Port Select High Register
Definition at line
53
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIPSELL |
External Interrupt Port Select Low Register
Definition at line
52
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::EXTIRISE |
External Interrupt Rising Edge Trigger Register
Definition at line
56
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::IEN |
Interrupt Enable Register
Definition at line
62
of file
efr32bg1p_gpio.h
.
| __IM uint32_t GPIO_TypeDef::IF |
Interrupt Flag Register
Definition at line
59
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
61
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
60
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::INSENSE |
Input Sense Register
Definition at line
70
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::LOCK |
Configuration Lock Register
Definition at line
71
of file
efr32bg1p_gpio.h
.
| GPIO_P_TypeDef GPIO_TypeDef::P[6U] |
Port configuration bits
Definition at line
49
of file
efr32bg1p_gpio.h
.
| uint32_t GPIO_TypeDef::RESERVED0[184U] |
Reserved for future use
Definition at line
51
of file
efr32bg1p_gpio.h
.
| uint32_t GPIO_TypeDef::RESERVED1[4U] |
Reserved for future use
Definition at line
65
of file
efr32bg1p_gpio.h
.
| uint32_t GPIO_TypeDef::RESERVED2[2U] |
Reserved for future use
Definition at line
69
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line
67
of file
efr32bg1p_gpio.h
.
| __IOM uint32_t GPIO_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line
66
of file
efr32bg1p_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG1P/Include/
efr32bg1p_gpio.h