Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Receive plugin, see Plugin System Layer for detailed documentation.
.
| Data Structures | |
| struct | EZRADIODRV_PacketRxHandle | 
| EzRadio receive plug-in instance initialization and handler structure. | |
| Macros | |
| #define | EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT | 
| Configuration data for EzRadio receive plug-in. | |
| Typedefs | |
| typedef struct EZRADIODRV_PacketRxHandle | EZRADIODRV_PacketRxHandle_t | 
| EzRadio receive plug-in instance initialization and handler structure. | |
| Functions | |
| Ecode_t | ezradioStartRx ( EZRADIODRV_Handle_t radioHandle) | 
| Set Radio to RX mode, packet length is always coming from the radio configuration. | |
Macro Definition Documentation
| #define EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio receive plug-in.
        Definition at line
        
         59
        
        of file
        
         ezradio_receive_plugin.h
        
        .
       
Function Documentation
| Ecode_t ezradioStartRx | ( | EZRADIODRV_Handle_t | 
            radioHandle
            | ) | 
Set Radio to RX mode, packet length is always coming from the radio configuration.
- Parameters
- 
         radioHandleHandler of the EzRadio driver instance where packet buffer, callback and channel configurations are set. 
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
        Definition at line
        
         49
        
        of file
        
         ezradio_receive_plugin.c
        
        .
       
References EZRADIODRV_PacketRxHandle::channel , ECODE_EMDRV_EZRADIODRV_OK , ezradio_start_rx() , and EZRADIODRV_HandleData::packetRx .