__HALL_Config Struct ReferenceBSP > Thunderboard Sense BSP > HALL - Hall Effect Sensor
Structure to configure the Hall effect sensor device.
       Definition at line
       
        54
       
       of file
       
        hall.h
       
       .
      
      
       #include <
       
     
        hall.h
       
       >
      
| Data Fields | |
| float | hysteresis | 
| bool | outputInvert | 
| uint8_t | polarity | 
| float | threshold | 
Field Documentation
| float __HALL_Config::hysteresis | 
| bool __HALL_Config::outputInvert | 
The polarity of the output pin
        Definition at line
        
         58
        
        of file
        
         hall.h
        
        .
       
Referenced by HALL_configure() .
| uint8_t __HALL_Config::polarity | 
Magnetic field polarity setting
        Definition at line
        
         57
        
        of file
        
         hall.h
        
        .
       
Referenced by HALL_configure() .
| float __HALL_Config::threshold | 
Decision point for magnetic field high or low in mT
        Definition at line
        
         55
        
        of file
        
         hall.h
        
        .
       
Referenced by HALL_configure() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/hardware/kit/common/bsp/thunderboard/
       hall.h