uartdrv.c File Reference
UARTDRV API implementation.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
       Definition in file
       
        uartdrv.c
       
       .
      
       #include <string.h>
      
      
       #include "
       
        uartdrv.h
       
       "
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_emu.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        gpiointerrupt.h
       
       "
      
      
| Functions | |
| Ecode_t | UARTDRV_Abort ( UARTDRV_Handle_t handle, UARTDRV_AbortType_t type) | 
| Abort ongoing UART transfers. | |
| Ecode_t | UARTDRV_DeInit ( UARTDRV_Handle_t handle) | 
| Deinitialize a UART driver instance. | |
| UARTDRV_FlowControlState_t | UARTDRV_FlowControlGetPeerStatus ( UARTDRV_Handle_t handle) | 
| Check the peer's flow control status. | |
| UARTDRV_FlowControlState_t | UARTDRV_FlowControlGetSelfStatus ( UARTDRV_Handle_t handle) | 
| Check the self flow control status. | |
| Ecode_t | UARTDRV_FlowControlIgnoreRestrain ( UARTDRV_Handle_t handle) | 
| Enable transmission when restrained by flow control. | |
| Ecode_t | UARTDRV_FlowControlSet ( UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state) | 
| Set UART flow control state. Set nRTS pin if hardware flow control is enabled. Send XON/XOFF if software flow control is enabled. | |
| Ecode_t | UARTDRV_FlowControlSetPeerStatus ( UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state) | 
| Set peer UART flow control state. Pause/resume transmit accordingly. Only for manual software flow control. | |
| UARTDRV_Count_t | UARTDRV_ForceReceive ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t maxCount) | 
| Direct receive without interrupts or callback. This is a blocking function. | |
| Ecode_t | UARTDRV_ForceTransmit ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) | 
| Direct transmit without interrupts or callback. This is a blocking function. that ignores flow control if enabled. | |
| UARTDRV_Status_t | UARTDRV_GetPeripheralStatus ( UARTDRV_Handle_t handle) | 
| Return the status of the UART peripheral associated with a given handle. | |
| uint8_t | UARTDRV_GetReceiveDepth ( UARTDRV_Handle_t handle) | 
| Return the number of queued receive operations. | |
| UARTDRV_Status_t | UARTDRV_GetReceiveStatus ( UARTDRV_Handle_t handle, uint8_t **buffer, UARTDRV_Count_t *itemsReceived, UARTDRV_Count_t *itemsRemaining) | 
| Check the status of the UART and gather information about any ongoing receive operations. | |
| uint8_t | UARTDRV_GetTransmitDepth ( UARTDRV_Handle_t handle) | 
| Returns the number of queued transmit operations. | |
| UARTDRV_Status_t | UARTDRV_GetTransmitStatus ( UARTDRV_Handle_t handle, uint8_t **buffer, UARTDRV_Count_t *itemsSent, UARTDRV_Count_t *itemsRemaining) | 
| Check the status of the UART and gather information about any ongoing transmit operations. | |
| Ecode_t | UARTDRV_InitLeuart ( UARTDRV_Handle_t handle, const UARTDRV_InitLeuart_t *initData) | 
| Initialize a LEUART driver instance. | |
| Ecode_t | UARTDRV_InitUart ( UARTDRV_Handle_t handle, const UARTDRV_InitUart_t *initData) | 
| Initialize a U(S)ART driver instance. | |
| Ecode_t | UARTDRV_PauseTransmit ( UARTDRV_Handle_t handle) | 
| Pause an ongoing transmit operation. | |
| Ecode_t | UARTDRV_Receive ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count, UARTDRV_Callback_t callback) | 
| Start a non-blocking receive. | |
| Ecode_t | UARTDRV_ReceiveB ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) | 
| Start a blocking receive. | |
| Ecode_t | UARTDRV_ResumeTransmit ( UARTDRV_Handle_t handle) | 
| Resume a paused transmit operation. | |
| Ecode_t | UARTDRV_Transmit ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count, UARTDRV_Callback_t callback) | 
| Start a non-blocking transmit. | |
| Ecode_t | UARTDRV_TransmitB ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) | 
| Start a blocking transmit. | |