PCNTEMLIB

Detailed Description

Pulse Counter (PCNT) Peripheral API.

This module contains functions to control the PCNT peripheral of Silicon Labs 32-bit MCUs and SoCs. The PCNT decodes incoming pulses. The module has a quadrature mode which may be used to decode the speed and direction of a mechanical shaft.

Data Structures

struct  PCNT_Filter_TypeDef
 
struct  PCNT_Init_TypeDef
 
struct  PCNT_TCC_TypeDef
 

Macros

#define PCNT0_CNT_SIZE   (16) /* PCNT0 counter is 16 bits. */
 
#define PCNT1_CNT_SIZE   (16) /* PCNT1 counter is 16 bits. */
 
#define PCNT2_CNT_SIZE   (16) /* PCNT2 counter is 16 bits. */
 
#define PCNT_FILTER_DEFAULT
 
#define PCNT_INIT_DEFAULT
 
#define PCNT_TCC_DEFAULT
 

Enumerations

enum  PCNT_CntEvent_TypeDef {
  pcntCntEventBoth = _PCNT_CTRL_CNTEV_BOTH,
  pcntCntEventUp = _PCNT_CTRL_CNTEV_UP,
  pcntCntEventDown = _PCNT_CTRL_CNTEV_DOWN,
  pcntCntEventNone = _PCNT_CTRL_CNTEV_NONE
}
 
enum  PCNT_Mode_TypeDef {
  pcntModeDisable = _PCNT_CTRL_MODE_DISABLE,
  pcntModeOvsSingle = _PCNT_CTRL_MODE_OVSSINGLE,
  pcntModeExtSingle = _PCNT_CTRL_MODE_EXTCLKSINGLE,
  pcntModeExtQuad = _PCNT_CTRL_MODE_EXTCLKQUAD,
  pcntModeOvsQuad1 = _PCNT_CTRL_MODE_OVSQUAD1X,
  pcntModeOvsQuad2 = _PCNT_CTRL_MODE_OVSQUAD2X,
  pcntModeOvsQuad4 = _PCNT_CTRL_MODE_OVSQUAD4X
}
 
enum  PCNT_PRSInput_TypeDef {
  pcntPRSInputS0 = 0,
  pcntPRSInputS1 = 1
}
 
enum  PCNT_PRSSel_TypeDef {
  pcntPRSCh0 = 0,
  pcntPRSCh1 = 1,
  pcntPRSCh2 = 2,
  pcntPRSCh3 = 3,
  pcntPRSCh4 = 4,
  pcntPRSCh5 = 5,
  pcntPRSCh6 = 6,
  pcntPRSCh7 = 7,
  pcntPRSCh8 = 8,
  pcntPRSCh9 = 9,
  pcntPRSCh10 = 10,
  pcntPRSCh11 = 11
}
 
enum  PCNT_TCCComp_Typedef {
  tccCompLTOE = _PCNT_CTRL_TCCCOMP_LTOE,
  tccCompGTOE = _PCNT_CTRL_TCCCOMP_GTOE,
  tccCompRange = _PCNT_CTRL_TCCCOMP_RANGE
}
 
enum  PCNT_TCCMode_TypeDef {
  tccModeDisabled = _PCNT_CTRL_TCCMODE_DISABLED,
  tccModeLFA = _PCNT_CTRL_TCCMODE_LFA,
  tccModePRS = _PCNT_CTRL_TCCMODE_PRS
}
 
enum  PCNT_TCCPresc_Typedef {
  tccPrescDiv1 = _PCNT_CTRL_TCCPRESC_DIV1,
  tccPrescDiv2 = _PCNT_CTRL_TCCPRESC_DIV2,
  tccPrescDiv4 = _PCNT_CTRL_TCCPRESC_DIV4,
  tccPrescDiv8 = _PCNT_CTRL_TCCPRESC_DIV8
}
 

Functions

__STATIC_INLINE uint32_t PCNT_AuxCounterGet (PCNT_TypeDef *pcnt)
 Get auxiliary counter value.
 
__STATIC_INLINE uint32_t PCNT_CounterGet (PCNT_TypeDef *pcnt)
 Get pulse counter value.
 
void PCNT_CounterReset (PCNT_TypeDef *pcnt)
 Reset PCNT counters and TOP register.
 
__STATIC_INLINE void PCNT_CounterSet (PCNT_TypeDef *pcnt, uint32_t count)
 Set counter value.
 
void PCNT_CounterTopSet (PCNT_TypeDef *pcnt, uint32_t count, uint32_t top)
 Set the counter and top values.
 
void PCNT_Enable (PCNT_TypeDef *pcnt, PCNT_Mode_TypeDef mode)
 Set PCNT operational mode.
 
void PCNT_FilterConfiguration (PCNT_TypeDef *pcnt, const PCNT_Filter_TypeDef *config, bool enable)
 Set the filter configuration.
 
void PCNT_FreezeEnable (PCNT_TypeDef *pcnt, bool enable)
 PCNT register synchronization freeze control.
 
void PCNT_Init (PCNT_TypeDef *pcnt, const PCNT_Init_TypeDef *init)
 Initialize the pulse counter.
 
__STATIC_INLINE void PCNT_IntClear (PCNT_TypeDef *pcnt, uint32_t flags)
 Clear one or more pending PCNT interrupts.
 
__STATIC_INLINE void PCNT_IntDisable (PCNT_TypeDef *pcnt, uint32_t flags)
 Disable one or more PCNT interrupts.
 
__STATIC_INLINE void PCNT_IntEnable (PCNT_TypeDef *pcnt, uint32_t flags)
 Enable one or more PCNT interrupts.
 
__STATIC_INLINE uint32_t PCNT_IntGet (PCNT_TypeDef *pcnt)
 Get pending PCNT interrupt flags.
 
__STATIC_INLINE uint32_t PCNT_IntGetEnabled (PCNT_TypeDef *pcnt)
 Get enabled and pending PCNT interrupt flags.
 
__STATIC_INLINE void PCNT_IntSet (PCNT_TypeDef *pcnt, uint32_t flags)
 Set one or more pending PCNT interrupts from SW.
 
void PCNT_PRSInputEnable (PCNT_TypeDef *pcnt, PCNT_PRSInput_TypeDef prsInput, bool enable)
 Enable/disable the selected PRS input of PCNT.
 
void PCNT_Reset (PCNT_TypeDef *pcnt)
 Reset PCNT to the same state that it was in after a hardware reset.
 
void PCNT_TCCConfiguration (PCNT_TypeDef *pcnt, const PCNT_TCC_TypeDef *config)
 Set Triggered Compare and Clear configuration.
 
__STATIC_INLINE uint32_t PCNT_TopBufferGet (PCNT_TypeDef *pcnt)
 Get pulse counter top buffer value.
 
void PCNT_TopBufferSet (PCNT_TypeDef *pcnt, uint32_t val)
 Set top buffer value.
 
__STATIC_INLINE uint32_t PCNT_TopGet (PCNT_TypeDef *pcnt)
 Get pulse counter top value.
 
void PCNT_TopSet (PCNT_TypeDef *pcnt, uint32_t val)
 Set the top value.
 

Macro Definition Documentation

#define PCNT0_CNT_SIZE   (16) /* PCNT0 counter is 16 bits. */

PCNT0 Counter register size.

Definition at line 61 of file em_pcnt.h.

Referenced by PCNT_CounterTopSet(), PCNT_Init(), and PCNT_TopSet().

#define PCNT1_CNT_SIZE   (16) /* PCNT1 counter is 16 bits. */

PCNT1 Counter register size.

Definition at line 69 of file em_pcnt.h.

Referenced by PCNT_CounterTopSet(), PCNT_Init(), and PCNT_TopSet().

#define PCNT2_CNT_SIZE   (16) /* PCNT2 counter is 16 bits. */

PCNT2 Counter register size.

Definition at line 78 of file em_pcnt.h.

Referenced by PCNT_CounterTopSet(), PCNT_Init(), and PCNT_TopSet().

#define PCNT_FILTER_DEFAULT
Value:
{ \
0, /* Default length is 5 LFACLK cycles. */ \
false /* No flutter removal. */ \
}

Default configuration for PCNT initialization structure.

Definition at line 277 of file em_pcnt.h.

#define PCNT_INIT_DEFAULT
Value:
{ \
pcntModeDisable, /* Disabled by default. */ \
_PCNT_CNT_RESETVALUE, /* Default counter HW reset value. */ \
_PCNT_TOP_RESETVALUE, /* Default counter HW reset value. */ \
false, /* Use positive edge. */ \
false, /* Up-counting. */ \
false, /* Filter disabled. */ \
false, /* Hysteresis disabled. */ \
true, /* Counter direction is given by CNTDIR. */ \
pcntCntEventUp, /* Regular counter counts up on upcount events. */ \
pcntCntEventNone, /* Auxiliary counter doesn't respond to events. */ \
pcntPRSCh0, /* PRS channel 0 selected as S0IN. */ \
pcntPRSCh0 /* PRS channel 0 selected as S1IN. */ \
}

Default configuration for PCNT initialization structure.

Definition at line 245 of file em_pcnt.h.

#define PCNT_TCC_DEFAULT
Value:
{ \
tccModeDisabled, /* Disabled by default. */ \
tccPrescDiv1, /* Do not prescale LFA clock in LFA mode. */ \
tccCompLTOE, /* Clear when CNT <= TOP. */ \
pcntPRSCh0, /* Select PRS channel 0 as input to TCC. */ \
false, /* PRS polarity is rising edge, and gate when 1. */ \
false /* Do not gate PCNT counter input. */ \
}

Definition at line 350 of file em_pcnt.h.

Enumeration Type Documentation

Counter event selection. Note: unshifted values are being used for enumeration because multiple configuration structure members use this type definition.

Enumerator
pcntCntEventBoth 

Counts up on up-count and down on down-count events.

pcntCntEventUp 

Only counts up on up-count events.

pcntCntEventDown 

Only counts down on down-count events.

pcntCntEventNone 

Never counts.

Definition at line 116 of file em_pcnt.h.

Mode selection.

Enumerator
pcntModeDisable 

Disable pulse counter.

pcntModeOvsSingle 

Single input LFACLK oversampling mode (available in EM0-EM2).

pcntModeExtSingle 

Externally clocked single input counter mode (available in EM0-EM3).

pcntModeExtQuad 

Externally clocked quadrature decoder mode (available in EM0-EM3).

pcntModeOvsQuad1 

LFACLK oversampling quadrature decoder 1X mode (available in EM0-EM2).

pcntModeOvsQuad2 

LFACLK oversampling quadrature decoder 2X mode (available in EM0-EM2).

pcntModeOvsQuad4 

LFACLK oversampling quadrature decoder 4X mode (available in EM0-EM2).

Definition at line 87 of file em_pcnt.h.

PRS inputs of PCNT.

Enumerator
pcntPRSInputS1 

PRS input 0.

Definition at line 165 of file em_pcnt.h.

PRS sources for s0PRS and s1PRS.

Enumerator
pcntPRSCh0 

PRS channel 0.

pcntPRSCh1 

PRS channel 1.

pcntPRSCh2 

PRS channel 2.

pcntPRSCh3 

PRS channel 3.

pcntPRSCh4 

PRS channel 4.

pcntPRSCh5 

PRS channel 5.

pcntPRSCh6 

PRS channel 6.

pcntPRSCh7 

PRS channel 7.

pcntPRSCh8 

PRS channel 8.

pcntPRSCh9 

PRS channel 9.

pcntPRSCh10 

PRS channel 10.

pcntPRSCh11 

PRS channel 11.

Definition at line 133 of file em_pcnt.h.

Compare modes for TCC module.

Enumerator
tccCompLTOE 

Compare match if PCNT_CNT is less than, or equal to PCNT_TOP.

tccCompGTOE 

Compare match if PCNT_CNT is greater than or equal to PCNT_TOP.

tccCompRange 

Compare match if PCNT_CNT is less than, or equal to PCNT_TOP[15:8]], and greater than, or equal to PCNT_TOP[7:0].

Definition at line 314 of file em_pcnt.h.

Modes for Triggered Compare and Clear module.

Enumerator
tccModeDisabled 

Triggered compare and clear not enabled.

tccModeLFA 

Compare and clear performed on each (optionally prescaled) LFA clock cycle.

tccModePRS 

Compare and clear performed on PRS edges. Polarity defined by prsPolarity.

Definition at line 287 of file em_pcnt.h.

Prescaler values for LFA compare and clear events. Only has effect when TCC mode is LFA.

Enumerator
tccPrescDiv1 

Compare and clear event each LFA cycle.

tccPrescDiv2 

Compare and clear event every other LFA cycle.

tccPrescDiv4 

Compare and clear event every 4th LFA cycle.

tccPrescDiv8 

Compare and clear event every 8th LFA cycle.

Definition at line 299 of file em_pcnt.h.

Function Documentation

__STATIC_INLINE uint32_t PCNT_AuxCounterGet ( PCNT_TypeDef pcnt)

Get auxiliary counter value.

Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
Current auxiliary counter value.

Definition at line 393 of file em_pcnt.h.

References PCNT_TypeDef::AUXCNT.

__STATIC_INLINE uint32_t PCNT_CounterGet ( PCNT_TypeDef pcnt)

Get pulse counter value.

Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
Current pulse counter value.

Definition at line 377 of file em_pcnt.h.

References PCNT_TypeDef::CNT.

void PCNT_CounterReset ( PCNT_TypeDef pcnt)

Reset PCNT counters and TOP register.

Note
Notice that special SYNCBUSY handling is not applicable for the RSTEN bit of the control register, so we don't need to wait for it when only modifying RSTEN. (It would mean undefined wait time if clocked by an external clock.) The SYNCBUSY bit will however be set, leading to a synchronization in the LF domain, with, in reality, no changes.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.

Definition at line 141 of file em_pcnt.c.

References _PCNT_CTRL_RSTEN_SHIFT, BUS_RegBitWrite(), and PCNT_TypeDef::CTRL.

__STATIC_INLINE void PCNT_CounterSet ( PCNT_TypeDef pcnt,
uint32_t  count 
)

Set counter value.

Pulse counter is disabled while changing counter value, and re-enabled (if originally enabled) when counter value has been set.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module since stall time may be undefined in that case. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in]pcntPointer to PCNT peripheral register block.
[in]countValue to set in counter register.

Definition at line 423 of file em_pcnt.h.

References PCNT_CounterTopSet(), and PCNT_TypeDef::TOP.

void PCNT_CounterTopSet ( PCNT_TypeDef pcnt,
uint32_t  count,
uint32_t  top 
)

Set the counter and top values.

The pulse counter is disabled while changing these values and reenabled (if originally enabled) when values have been set.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module, since stall time may be undefined. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]countA value to set in the counter register.
[in]topA value to set in the top register.

Definition at line 176 of file em_pcnt.c.

References _PCNT_CTRL_MODE_MASK, PCNT_TypeDef::CMD, PCNT_TypeDef::CTRL, PCNT0, PCNT0_CNT_SIZE, PCNT1, PCNT1_CNT_SIZE, PCNT2, PCNT2_CNT_SIZE, PCNT_CMD_LCNTIM, PCNT_CMD_LTOPBIM, PCNT_CTRL_MODE_DISABLE, PCNT_SYNCBUSY_CMD, PCNT_SYNCBUSY_CTRL, PCNT_SYNCBUSY_TOPB, and PCNT_TypeDef::TOPB.

Referenced by PCNT_CounterSet(), and PCNT_Init().

void PCNT_Enable ( PCNT_TypeDef pcnt,
PCNT_Mode_TypeDef  mode 
)

Set PCNT operational mode.

Notice that this function does not do any configuration. Setting operational mode is normally only required after initialization is done, and if not done as part of initialization or if requiring to disable/reenable pulse counter.

Note
This function may stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module, since stall time may be undefined.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]modeAn operational mode to use for PCNT.

Definition at line 271 of file em_pcnt.c.

References _PCNT_CTRL_MODE_MASK, _PCNT_CTRL_MODE_SHIFT, PCNT_TypeDef::CTRL, and PCNT_SYNCBUSY_CTRL.

void PCNT_FilterConfiguration ( PCNT_TypeDef pcnt,
const PCNT_Filter_TypeDef config,
bool  enable 
)

Set the filter configuration.

This function will configure the PCNT input filter when the PCNT mode is configured to take an LFA-derived clock as an input clock.

Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]configA pointer to the configuration structure to be applied.
[in]enableIndicates whether to enable or disable filtering.

Definition at line 666 of file em_pcnt.c.

References _PCNT_OVSCFG_FILTLEN_MASK, _PCNT_OVSCFG_FILTLEN_SHIFT, _PCNT_OVSCFG_FLUTTERRM_SHIFT, PCNT_TypeDef::CTRL, PCNT_Filter_TypeDef::filtLen, PCNT_Filter_TypeDef::flutterrm, PCNT_TypeDef::OVSCFG, PCNT_CTRL_FILT, PCNT_SYNCBUSY_CTRL, and PCNT_SYNCBUSY_OVSCFG.

void PCNT_FreezeEnable ( PCNT_TypeDef pcnt,
bool  enable 
)

PCNT register synchronization freeze control.

Some PCNT registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several registers to be modified before passing them to the LF domain simultaneously, which takes place when the freeze mode is disabled.

Note
When enabling freeze mode, this function will wait for all current ongoing PCNT synchronization to the LF domain to complete (normally synchronization will not be in progress). However, for this reason, when using freeze mode, modifications of registers requiring the LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]enable
  • True - enable freeze, modified registers are not propagated to the LF domain.
  • False - disables freeze, modified registers are propagated to LF domain.

Definition at line 356 of file em_pcnt.c.

References PCNT_TypeDef::FREEZE, PCNT_FREEZE_REGFREEZE, and PCNT_TypeDef::SYNCBUSY.

void PCNT_Init ( PCNT_TypeDef pcnt,
const PCNT_Init_TypeDef init 
)

Initialize the pulse counter.

This function will configure the pulse counter. The clock selection is configured as follows, depending on operational mode:

Notice that the LFACLK must be enabled in all modes, since some basic setup is done with this clock even if the external pin clock usage mode is chosen. The pulse counter clock for the selected instance must also be enabled prior to initialization.

Notice that pins used by the PCNT module must be properly configured by the user explicitly through setting the ROUTE register for the PCNT to work as intended.

Writing to CNT will not occur in external clock modes (EXTCLKQUAD and EXTCLKSINGLE) because the external clock rate is unknown. The user should handle it manually depending on the application.

TOPB is written for all modes but in external clock mode it will take 3 external clock cycles to sync to TOP.

Note
Initializing requires synchronization into the low-frequency domain. This may cause a delay.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]initA pointer to the initialization structure.

Definition at line 416 of file em_pcnt.c.

References _PCNT_CTRL_AUXCNTEV_SHIFT, _PCNT_CTRL_CNTEV_SHIFT, _PCNT_CTRL_MODE_MASK, _PCNT_CTRL_MODE_SHIFT, _PCNT_CTRL_RSTEN_SHIFT, _PCNT_INPUT_S0PRSSEL_MASK, _PCNT_INPUT_S0PRSSEL_SHIFT, _PCNT_INPUT_S1PRSSEL_MASK, _PCNT_INPUT_S1PRSSEL_SHIFT, PCNT_Init_TypeDef::auxCntEvent, BUS_RegBitWrite(), PCNT_TypeDef::CMD, CMU_PCNTClockExternalSet(), PCNT_Init_TypeDef::cntEvent, PCNT_Init_TypeDef::countDown, PCNT_Init_TypeDef::counter, PCNT_TypeDef::CTRL, PCNT_Init_TypeDef::filter, PCNT_Init_TypeDef::hyst, PCNT_TypeDef::INPUT, PCNT_Init_TypeDef::mode, PCNT_Init_TypeDef::negEdge, PCNT0, PCNT0_CNT_SIZE, PCNT1, PCNT1_CNT_SIZE, PCNT2, PCNT2_CNT_SIZE, PCNT_CMD_LTOPBIM, PCNT_CounterTopSet(), PCNT_CTRL_CNTDIR_DOWN, PCNT_CTRL_EDGE_NEG, PCNT_CTRL_FILT, PCNT_CTRL_HYST, PCNT_CTRL_MODE_DISABLE, PCNT_CTRL_RSTEN, PCNT_CTRL_S1CDIR, PCNT_SYNCBUSY_CTRL, pcntCntEventBoth, pcntCntEventDown, pcntCntEventNone, pcntCntEventUp, pcntModeExtQuad, pcntModeExtSingle, pcntModeOvsSingle, PCNT_Init_TypeDef::s0PRS, PCNT_Init_TypeDef::s1CntDir, PCNT_Init_TypeDef::s1PRS, PCNT_Init_TypeDef::top, and PCNT_TypeDef::TOPB.

__STATIC_INLINE void PCNT_IntClear ( PCNT_TypeDef pcnt,
uint32_t  flags 
)

Clear one or more pending PCNT interrupts.

Parameters
[in]pcntPointer to PCNT peripheral register block.
[in]flagsPending PCNT interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

Definition at line 456 of file em_pcnt.h.

References PCNT_TypeDef::IFC.

__STATIC_INLINE void PCNT_IntDisable ( PCNT_TypeDef pcnt,
uint32_t  flags 
)

Disable one or more PCNT interrupts.

Parameters
[in]pcntPointer to PCNT peripheral register block.
[in]flagsPCNT interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

Definition at line 472 of file em_pcnt.h.

References PCNT_TypeDef::IEN.

__STATIC_INLINE void PCNT_IntEnable ( PCNT_TypeDef pcnt,
uint32_t  flags 
)

Enable one or more PCNT interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using PCNT_IntClear() prior to enabling the interrupt.
Parameters
[in]pcntPointer to PCNT peripheral register block.
[in]flagsPCNT interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

Definition at line 493 of file em_pcnt.h.

References PCNT_TypeDef::IEN.

__STATIC_INLINE uint32_t PCNT_IntGet ( PCNT_TypeDef pcnt)

Get pending PCNT interrupt flags.

Note
The event bits are not cleared by the use of this function.
Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
PCNT interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

Definition at line 512 of file em_pcnt.h.

References PCNT_TypeDef::IF.

__STATIC_INLINE uint32_t PCNT_IntGetEnabled ( PCNT_TypeDef pcnt)

Get enabled and pending PCNT interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
The event bits are not cleared by the use of this function.
Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
Pending and enabled PCNT interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in PCNT_IEN_nnn register (PCNT_IEN_nnn) and
  • the OR combination of valid interrupt flags of the PCNT module (PCNT_IF_nnn).

Definition at line 538 of file em_pcnt.h.

References PCNT_TypeDef::IEN, and PCNT_TypeDef::IF.

__STATIC_INLINE void PCNT_IntSet ( PCNT_TypeDef pcnt,
uint32_t  flags 
)

Set one or more pending PCNT interrupts from SW.

Parameters
[in]pcntPointer to PCNT peripheral register block.
[in]flagsPCNT interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

Definition at line 561 of file em_pcnt.h.

References PCNT_TypeDef::IFS.

void PCNT_PRSInputEnable ( PCNT_TypeDef pcnt,
PCNT_PRSInput_TypeDef  prsInput,
bool  enable 
)

Enable/disable the selected PRS input of PCNT.

Notice that this function does not do any configuration.

Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]prsInputPRS input (S0 or S1) of the selected PCNT module.
[in]enableSet to true to enable, false to disable the selected PRS input.

Definition at line 303 of file em_pcnt.c.

References _PCNT_INPUT_S0PRSEN_SHIFT, _PCNT_INPUT_S1PRSEN_SHIFT, BUS_RegBitWrite(), PCNT_TypeDef::INPUT, and pcntPRSInputS1.

void PCNT_Reset ( PCNT_TypeDef pcnt)

Reset PCNT to the same state that it was in after a hardware reset.

Notice the LFACLK must be enabled, since some basic reset is done with this clock. The pulse counter clock for the selected instance must also be enabled prior to initialization.

Note
The ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.

Definition at line 612 of file em_pcnt.c.

References _PCNT_CTRL_RESETVALUE, _PCNT_CTRL_RSTEN_SHIFT, _PCNT_IEN_RESETVALUE, _PCNT_IFC_MASK, _PCNT_TOPB_RESETVALUE, BUS_RegBitWrite(), CMU_PCNTClockExternalSet(), PCNT_TypeDef::CTRL, PCNT_TypeDef::IEN, PCNT_TypeDef::IFC, PCNT_CTRL_RSTEN, PCNT_SYNCBUSY_CTRL, and PCNT_TopBufferSet().

void PCNT_TCCConfiguration ( PCNT_TypeDef pcnt,
const PCNT_TCC_TypeDef config 
)

Set Triggered Compare and Clear configuration.

This function will configure the PCNT TCC (Triggered Compare and Clear) module. This module can, upon a configurable trigger source, compare the current counter value with the configured TOP value. Upon match, the counter will be reset and the TCC PRS output and TCC interrupt flag will be set.

Since there is a comparison with the TOP value, the counter will not stop counting nor wrap when hitting the TOP value, but it will keep on counting until its maximum value. Then, it will not wrap, but stop counting and set the overflow flag.

Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]configA pointer to the configuration structure to be applied.

Definition at line 712 of file em_pcnt.c.

References _PCNT_CTRL_PRSGATEEN_MASK, _PCNT_CTRL_PRSGATEEN_SHIFT, _PCNT_CTRL_TCCCOMP_MASK, _PCNT_CTRL_TCCCOMP_SHIFT, _PCNT_CTRL_TCCMODE_MASK, _PCNT_CTRL_TCCMODE_SHIFT, _PCNT_CTRL_TCCPRESC_MASK, _PCNT_CTRL_TCCPRESC_SHIFT, _PCNT_CTRL_TCCPRSPOL_MASK, _PCNT_CTRL_TCCPRSPOL_SHIFT, _PCNT_CTRL_TCCPRSSEL_MASK, _PCNT_CTRL_TCCPRSSEL_SHIFT, PCNT_TCC_TypeDef::compare, PCNT_TypeDef::CTRL, PCNT_TCC_TypeDef::mode, PCNT_SYNCBUSY_CTRL, PCNT_TCC_TypeDef::prescaler, PCNT_TCC_TypeDef::prsGateEnable, PCNT_TCC_TypeDef::prsPolarity, and PCNT_TCC_TypeDef::tccPRS.

__STATIC_INLINE uint32_t PCNT_TopBufferGet ( PCNT_TypeDef pcnt)

Get pulse counter top buffer value.

Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
Current pulse counter top buffer value.

Definition at line 578 of file em_pcnt.h.

References PCNT_TypeDef::TOPB.

void PCNT_TopBufferSet ( PCNT_TypeDef pcnt,
uint32_t  val 
)

Set top buffer value.

Note
This function may stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module since stall time may be undefined.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]valA value to set in the top buffer register.

Definition at line 754 of file em_pcnt.c.

References PCNT_SYNCBUSY_TOPB, and PCNT_TypeDef::TOPB.

Referenced by PCNT_Reset().

__STATIC_INLINE uint32_t PCNT_TopGet ( PCNT_TypeDef pcnt)

Get pulse counter top value.

Parameters
[in]pcntPointer to PCNT peripheral register block.
Returns
Current pulse counter top value.

Definition at line 595 of file em_pcnt.h.

References PCNT_TypeDef::TOP.

void PCNT_TopSet ( PCNT_TypeDef pcnt,
uint32_t  val 
)

Set the top value.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module since stall time may be undefined.
Parameters
[in]pcntA pointer to the PCNT peripheral register block.
[in]valA value to set in the top register.

Definition at line 779 of file em_pcnt.c.

References PCNT_TypeDef::CMD, PCNT0, PCNT0_CNT_SIZE, PCNT1, PCNT1_CNT_SIZE, PCNT2, PCNT2_CNT_SIZE, PCNT_CMD_LTOPBIM, PCNT_SYNCBUSY_CMD, PCNT_SYNCBUSY_TOPB, and PCNT_TypeDef::TOPB.