LDMA_Init_t Struct ReferenceEMLIB > LDMA

LDMA initialization configuration structure.

Definition at line 851 of file em_ldma.h.

#include <em_ldma.h>

Data Fields

uint8_t ldmaInitCtrlNumFixed
 
uint8_t ldmaInitCtrlSyncPrsClrEn
 
uint8_t ldmaInitCtrlSyncPrsSetEn
 
uint8_t ldmaInitIrqPriority
 

Field Documentation

uint8_t LDMA_Init_t::ldmaInitCtrlNumFixed

Arbitration mode separator.

Definition at line 852 of file em_ldma.h.

Referenced by DMADRV_Init(), and LDMA_Init().

uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsClrEn

PRS Synctrig clear enable.

Definition at line 853 of file em_ldma.h.

Referenced by LDMA_Init().

uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsSetEn

PRS Synctrig set enable.

Definition at line 854 of file em_ldma.h.

Referenced by LDMA_Init().

uint8_t LDMA_Init_t::ldmaInitIrqPriority

LDMA IRQ priority (0..7).

Definition at line 855 of file em_ldma.h.

Referenced by DMADRV_Init(), and LDMA_Init().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/em_ldma.h