GPIO_P_TypeDef Struct ReferenceDevicesDevices > | GPIO
GPIO_P GPIO P Register
.
Definition at line
46
of file
efr32mg12p_gpio_p.h
.
#include <
efr32mg12p_gpio_p.h
>
Data Fields |
|
| __IOM uint32_t | CTRL |
| __IM uint32_t | DIN |
| __IOM uint32_t | DOUT |
| __IOM uint32_t | DOUTTGL |
| __IOM uint32_t | MODEH |
| __IOM uint32_t | MODEL |
| __IOM uint32_t | OVTDIS |
| __IOM uint32_t | PINLOCKN |
| uint32_t | RESERVED0 [2U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED2 [1U] |
Field Documentation
| __IOM uint32_t GPIO_P_TypeDef::CTRL |
Port Control Register
Definition at line
47
of file
efr32mg12p_gpio_p.h
.
| __IM uint32_t GPIO_P_TypeDef::DIN |
Port Data in Register
Definition at line
53
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::DOUT |
Port Data Out Register
Definition at line
50
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::DOUTTGL |
Port Data Out Toggle Register
Definition at line
52
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::MODEH |
Port Pin Mode High Register
Definition at line
49
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::MODEL |
Port Pin Mode Low Register
Definition at line
48
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::OVTDIS |
Over Voltage Disable for All Modes
Definition at line
56
of file
efr32mg12p_gpio_p.h
.
| __IOM uint32_t GPIO_P_TypeDef::PINLOCKN |
Port Unlocked Pins Register
Definition at line
54
of file
efr32mg12p_gpio_p.h
.
| uint32_t GPIO_P_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line
51
of file
efr32mg12p_gpio_p.h
.
| uint32_t GPIO_P_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
55
of file
efr32mg12p_gpio_p.h
.
| uint32_t GPIO_P_TypeDef::RESERVED2[1U] |
Reserved future
Definition at line
57
of file
efr32mg12p_gpio_p.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/
efr32mg12p_gpio_p.h