ARING_TypeDef Struct ReferenceKit Drivers > SegmentLcd
Defines segment COM and BIT fields for A-wheel (suited for Anim)
Definition at line 107
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [8] |
uint8_t | com [8] |
Field Documentation
uint8_t ARING_TypeDef::bit[8] |
LCD bit number
Definition at line 109
of file segmentlcd.c
.
uint8_t ARING_TypeDef::com[8] |
LCD COM line (for multiplexing)
Definition at line 108
of file segmentlcd.c
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/hardware/kit/common/drivers/
segmentlcd.c