IDACEMLIB
Detailed Description
Current Digital-to-Analog Converter (IDAC) Peripheral API.
IDAC can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. Current is configurable with several ranges of various step sizes. IDAC can be used with PRS and can operate down to EM3.
The following steps are necessary for basic operation:
Clock enable:
Initialize peripheral with default settings and modify selected fields, such as output select:
Set output:
Data Structures |
|
| struct | IDAC_Init_TypeDef |
Macros |
|
| #define | IDAC_INIT_DEFAULT |
Enumerations |
|
| enum |
IDAC_OutMode_TypeDef
{
idacOutputAPORT1XCH0 = IDAC_CTRL_APORTOUTSEL_APORT1XCH0, idacOutputAPORT1YCH1 = IDAC_CTRL_APORTOUTSEL_APORT1YCH1, idacOutputAPORT1XCH2 = IDAC_CTRL_APORTOUTSEL_APORT1XCH2, idacOutputAPORT1YCH3 = IDAC_CTRL_APORTOUTSEL_APORT1YCH3, idacOutputAPORT1XCH4 = IDAC_CTRL_APORTOUTSEL_APORT1XCH4, idacOutputAPORT1YCH5 = IDAC_CTRL_APORTOUTSEL_APORT1YCH5, idacOutputAPORT1XCH6 = IDAC_CTRL_APORTOUTSEL_APORT1XCH6, idacOutputAPORT1YCH7 = IDAC_CTRL_APORTOUTSEL_APORT1YCH7, idacOutputAPORT1XCH8 = IDAC_CTRL_APORTOUTSEL_APORT1XCH8, idacOutputAPORT1YCH9 = IDAC_CTRL_APORTOUTSEL_APORT1YCH9, idacOutputAPORT1XCH10 = IDAC_CTRL_APORTOUTSEL_APORT1XCH10, idacOutputAPORT1YCH11 = IDAC_CTRL_APORTOUTSEL_APORT1YCH11, idacOutputAPORT1XCH12 = IDAC_CTRL_APORTOUTSEL_APORT1XCH12, idacOutputAPORT1YCH13 = IDAC_CTRL_APORTOUTSEL_APORT1YCH13, idacOutputAPORT1XCH14 = IDAC_CTRL_APORTOUTSEL_APORT1XCH14, idacOutputAPORT1YCH15 = IDAC_CTRL_APORTOUTSEL_APORT1YCH15, idacOutputAPORT1XCH16 = IDAC_CTRL_APORTOUTSEL_APORT1XCH16, idacOutputAPORT1YCH17 = IDAC_CTRL_APORTOUTSEL_APORT1YCH17, idacOutputAPORT1XCH18 = IDAC_CTRL_APORTOUTSEL_APORT1XCH18, idacOutputAPORT1YCH19 = IDAC_CTRL_APORTOUTSEL_APORT1YCH19, idacOutputAPORT1XCH20 = IDAC_CTRL_APORTOUTSEL_APORT1XCH20, idacOutputAPORT1YCH21 = IDAC_CTRL_APORTOUTSEL_APORT1YCH21, idacOutputAPORT1XCH22 = IDAC_CTRL_APORTOUTSEL_APORT1XCH22, idacOutputAPORT1YCH23 = IDAC_CTRL_APORTOUTSEL_APORT1YCH23, idacOutputAPORT1XCH24 = IDAC_CTRL_APORTOUTSEL_APORT1XCH24, idacOutputAPORT1YCH25 = IDAC_CTRL_APORTOUTSEL_APORT1YCH25, idacOutputAPORT1XCH26 = IDAC_CTRL_APORTOUTSEL_APORT1XCH26, idacOutputAPORT1YCH27 = IDAC_CTRL_APORTOUTSEL_APORT1YCH27, idacOutputAPORT1XCH28 = IDAC_CTRL_APORTOUTSEL_APORT1XCH28, idacOutputAPORT1YCH29 = IDAC_CTRL_APORTOUTSEL_APORT1YCH29, idacOutputAPORT1XCH30 = IDAC_CTRL_APORTOUTSEL_APORT1XCH30, idacOutputAPORT1YCH31 = IDAC_CTRL_APORTOUTSEL_APORT1YCH31 } |
| enum |
IDAC_PRSSEL_TypeDef
{
idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0, idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1, idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2, idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3, idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4, idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5, idacPRSSELCh6 = IDAC_CTRL_PRSSEL_PRSCH6, idacPRSSELCh7 = IDAC_CTRL_PRSSEL_PRSCH7, idacPRSSELCh8 = IDAC_CTRL_PRSSEL_PRSCH8, idacPRSSELCh9 = IDAC_CTRL_PRSSEL_PRSCH9, idacPRSSELCh10 = IDAC_CTRL_PRSSEL_PRSCH10, idacPRSSELCh11 = IDAC_CTRL_PRSSEL_PRSCH11 } |
| enum |
IDAC_Range_TypeDef
{
idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0, idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1, idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2, idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3 } |
Functions |
|
| void | IDAC_Enable (IDAC_TypeDef *idac, bool enable) |
|
Enable/disable IDAC.
|
|
| void | IDAC_Init (IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init) |
|
Initialize IDAC.
|
|
| __STATIC_INLINE void | IDAC_IntClear (IDAC_TypeDef *idac, uint32_t flags) |
|
Clear one or more pending IDAC interrupts.
|
|
| __STATIC_INLINE void | IDAC_IntDisable (IDAC_TypeDef *idac, uint32_t flags) |
|
Disable one or more IDAC interrupts.
|
|
| __STATIC_INLINE void | IDAC_IntEnable (IDAC_TypeDef *idac, uint32_t flags) |
|
Enable one or more IDAC interrupts.
|
|
| __STATIC_INLINE uint32_t | IDAC_IntGet (IDAC_TypeDef *idac) |
|
Get pending IDAC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | IDAC_IntGetEnabled (IDAC_TypeDef *idac) |
|
Get enabled and pending IDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | IDAC_IntSet (IDAC_TypeDef *idac, uint32_t flags) |
|
Set one or more pending IDAC interrupts from SW.
|
|
| void | IDAC_MinimalOutputTransitionMode (IDAC_TypeDef *idac, bool enable) |
|
Enable/disable Minimal Output Transition mode.
|
|
| void | IDAC_OutEnable (IDAC_TypeDef *idac, bool enable) |
|
Enable/disable the IDAC OUT pin.
|
|
| void | IDAC_RangeSet (IDAC_TypeDef *idac, const IDAC_Range_TypeDef range) |
|
Set the current range of the IDAC output.
|
|
| void | IDAC_Reset (IDAC_TypeDef *idac) |
|
Reset IDAC to the same state that it was in after a hardware reset.
|
|
| void | IDAC_StepSet (IDAC_TypeDef *idac, const uint32_t step) |
|
Set the current step of the IDAC output.
|
|
Macro Definition Documentation
| #define IDAC_INIT_DEFAULT |
Default configuration for IDAC initialization structure.
Definition at line
201
of file
em_idac.h
.
Enumeration Type Documentation
| enum IDAC_OutMode_TypeDef |
Output mode.
Definition at line
92
of file
em_idac.h
.
| enum IDAC_PRSSEL_TypeDef |
Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.
Definition at line
134
of file
em_idac.h
.
| enum IDAC_Range_TypeDef |
Function Documentation
| void IDAC_Enable | ( | IDAC_TypeDef * |
idac,
|
| bool |
enable
|
||
| ) |
Enable/disable IDAC.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable IDAC, false to disable.
Definition at line
114
of file
em_idac.c
.
References BUS_RegBitWrite() .
| void IDAC_Init | ( | IDAC_TypeDef * |
idac,
|
| const IDAC_Init_TypeDef * |
init
|
||
| ) |
Initialize IDAC.
Initializes IDAC according to the initialization structure parameter and sets the default calibration value stored in the DEVINFO structure.
- Note
- This function will disable IDAC prior to configuration.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] initA pointer to the IDAC initialization structure.
Definition at line
77
of file
em_idac.c
.
References IDAC_Init_TypeDef::enable , IDAC_Init_TypeDef::outMode , IDAC_Init_TypeDef::prsEnable , IDAC_Init_TypeDef::prsSel , and IDAC_Init_TypeDef::sinkEnable .
| __STATIC_INLINE void IDAC_IntClear | ( | IDAC_TypeDef * |
idac,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending IDAC interrupts.
- Parameters
-
[in] idacPointer to IDAC peripheral register block. [in] flagsPending IDAC interrupt source(s) to clear. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
235
of file
em_idac.h
.
| __STATIC_INLINE void IDAC_IntDisable | ( | IDAC_TypeDef * |
idac,
|
| uint32_t |
flags
|
||
| ) |
Disable one or more IDAC interrupts.
- Parameters
-
[in] idacPointer to IDAC peripheral register block. [in] flagsIDAC interrupt source(s) to disable. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
251
of file
em_idac.h
.
| __STATIC_INLINE void IDAC_IntEnable | ( | IDAC_TypeDef * |
idac,
|
| uint32_t |
flags
|
||
| ) |
Enable one or more IDAC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using IDAC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] idacPointer to IDAC peripheral register block. [in] flagsIDAC interrupt source(s) to enable. Use one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
272
of file
em_idac.h
.
| __STATIC_INLINE uint32_t IDAC_IntGet | ( | IDAC_TypeDef * |
idac
|
) |
Get pending IDAC interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] idacPointer to IDAC peripheral register block.
- Returns
- IDAC interrupt source(s) pending. Returns one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
291
of file
em_idac.h
.
| __STATIC_INLINE uint32_t IDAC_IntGetEnabled | ( | IDAC_TypeDef * |
idac
|
) |
Get enabled and pending IDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] idacPointer to IDAC peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled IDAC interrupt sources. Return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in IDACx_IEN_nnn register (IDACx_IEN_nnn) and
- the OR combination of valid interrupt flags of IDAC module (IDACx_IF_nnn).
Definition at line
315
of file
em_idac.h
.
| __STATIC_INLINE void IDAC_IntSet | ( | IDAC_TypeDef * |
idac,
|
| uint32_t |
flags
|
||
| ) |
Set one or more pending IDAC interrupts from SW.
- Parameters
-
[in] idacPointer to IDAC peripheral register block. [in] flagsIDAC interrupt source(s) to set to pending. Use one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
338
of file
em_idac.h
.
| void IDAC_MinimalOutputTransitionMode | ( | IDAC_TypeDef * |
idac,
|
| bool |
enable
|
||
| ) |
Enable/disable Minimal Output Transition mode.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable Minimal Output Transition mode, false to disable.
Definition at line
165
of file
em_idac.c
.
References BUS_RegBitWrite() .
| void IDAC_OutEnable | ( | IDAC_TypeDef * |
idac,
|
| bool |
enable
|
||
| ) |
Enable/disable the IDAC OUT pin.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] enableTrue to enable the IDAC OUT pin, false to disable.
Definition at line
330
of file
em_idac.c
.
References BUS_RegBitWrite() .
| void IDAC_RangeSet | ( | IDAC_TypeDef * |
idac,
|
| const IDAC_Range_TypeDef |
range
|
||
| ) |
Set the current range of the IDAC output.
This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] rangeThe current range value.
Definition at line
187
of file
em_idac.c
.
References idacCurrentRange0 , idacCurrentRange1 , idacCurrentRange2 , and idacCurrentRange3 .
| void IDAC_Reset | ( | IDAC_TypeDef * |
idac
|
) |
Reset IDAC to the same state that it was in after a hardware reset.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block.
Definition at line
127
of file
em_idac.c
.
| void IDAC_StepSet | ( | IDAC_TypeDef * |
idac,
|
| const uint32_t |
step
|
||
| ) |
Set the current step of the IDAC output.
- Parameters
-
[in] idacA pointer to the IDAC peripheral register block. [in] stepA step value for the IDAC output. A valid range is 0-31.
Definition at line
307
of file
em_idac.c
.