Kit Drivers

Detailed Description

Kit support and drivers.

Drivers and support modules for board components such as displays, sensors and memory components on EFM32, EZR32 and EFR32 kits.

For display device support, see section Display Device Driver Stack for more information.

Modules

CPT112S_I2C
Silicon Labs 12-pad Capacitive Touch Evaluation Board I2C driver.
 
CapSense
Capacitive sensing driver.
 
Display
Display device driver stack library.
 
DmaCtrl
uDMA control block array.
 
EEPROM
I2C EEPROM Driver.
 
Gecko USB MSD
USB Mass Storage Class (MSC).
 
Gecko USB RS232 bridge
Gecko USB to RS232 bridge (CDC Class).
 
HidKeyboard
Implements a USB HID class keyboard.
 
I2CSPM
I2C Simple Polled Master driver.
 
Ksz8851snl
KSZ8851SNL SPI Ethernet Controller driver.
 
MicroSd
SPI driver for micro SD card.
 
NANDFlash
Driver for Numonyx NAND256W3A NAND Flash devices.
 
NORFlash
Driver for Spanion S29GL128P90FFIR13 and S29GL064N NOR Flash devices.
 
RetargetIo
Standard I/O retargeting driver.
 
SL_EFPDRV
EFP (Energy Friendly PMIC) driver.
 
SegmentLcd
Segment LCD driver.
 
Si114x
Silicon Labs Si114x Ultraviolet (UV) Index, Gesture, Proximity, and Ambient Light Sensor I2C driver.
 
Si7013
Silicon Labs Si7013 Relative Humidity and Temperature Sensor I2C driver.
 
Si72xx
Silicon Labs Si72xx Magnetic Hall Effect Sensor I2C driver.
 
TFT
Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode.
 
TempSensor
Driver for DS75 I2C temperature sensor.
 
Textdisplay
Line based text output terminal interface on top of the DISPLAY device driver stack. See TextDisplay Library for more information.
 
Touch
Touch panel driver for DK3650, DK3750 and DK3850 Development Kits.
 
Udelay
Calibrated busy wait loop.
 
UsbHid
USB HID keyboard scan codes.
 
VddCheck
VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API.