API_LayerEMDRV > EZRADIODRV

Detailed Description

EzRadio API Layer

.

Enumerations

enum  EZRADIO_ConfigRet_t {
  EZRADIO_CONFIG_SUCCESS,
  EZRADIO_CONFIG_NO_PATCH,
  EZRADIO_CONFIG_CTS_TIMEOUT,
  EZRADIO_CONFIG_PATCH_FAIL,
  EZRADIO_CONFIG_COMMAND_ERROR
}
 

Functions

void ezradio_change_state (uint8_t next_state1)
 
EZRADIO_ConfigRet_t ezradio_configuration_init (const uint8_t *pSetPropCmd)
 
void ezradio_ezconfig_check (uint16_t checksum, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_fifo_info (uint8_t fifo, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_fifo_info_fast_read (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_fifo_info_fast_reset (uint8_t fifo)
 
void ezradio_frr_a_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_frr_b_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_frr_c_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_frr_d_read (uint8_t respByteCount, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_func_info (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_adc_reading (uint8_t adc_en, uint8_t adc_cfg, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_chip_status (uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_chip_status_fast_clear (void)
 
void ezradio_get_chip_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_int_status (uint8_t ph_clr_pend, uint8_t modem_clr_pend, uint8_t chip_clr_pend, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_int_status_fast_clear (void)
 
void ezradio_get_int_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_modem_status (uint8_t modem_clr_pend, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_modem_status_fast_clear (void)
 
void ezradio_get_modem_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_packet_info (uint8_t field_number_mask, uint16_t len, int16_t diff_len, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_ph_status (uint8_t ph_clr_pend, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_ph_status_fast_clear (void)
 
void ezradio_get_ph_status_fast_clear_read (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_get_property (uint8_t group, uint8_t num_props, uint8_t start_prop, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_gpio_pin_cfg (uint8_t gpio0, uint8_t gpio1, uint8_t gpio2, uint8_t gpio3, uint8_t nirq, uint8_t sdo, uint8_t gen_config, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_gpio_pin_cfg_fast (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_ircal (uint8_t searching_step_size, uint8_t searching_rssi_avg, uint8_t rx_chain_setting1, uint8_t rx_chain_setting2)
 
void ezradio_ircal_manual (uint8_t ircal_amp, uint8_t ircal_ph, ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_nop (void)
 
void ezradio_part_info (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_power_up (uint8_t boot_options, uint8_t xtal_options, uint32_t xo_freq)
 
void ezradio_read_cmd_buff (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_read_rx_fifo (uint8_t numbytes, uint8_t *prxdata)
 
void ezradio_request_device_state (ezradio_cmd_reply_t *ezradioReply)
 
void ezradio_reset (void)
 
void ezradio_rx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0)
 
void ezradio_set_property (uint8_t group, uint8_t num_props, uint8_t start_prop,...)
 
void ezradio_start_rx (uint8_t channel, uint8_t condition, uint16_t rx_len, uint8_t next_state1, uint8_t next_state2, uint8_t next_state3)
 
void ezradio_start_rx_fast (void)
 
void ezradio_start_tx (uint8_t channel, uint8_t condition, uint16_t tx_len)
 
void ezradio_start_tx_fast (void)
 
void ezradio_tx_hop (uint8_t inte, uint8_t frac2, uint8_t frac1, uint8_t frac0, uint8_t vco_cnt1, uint8_t vco_cnt0, uint8_t pll_settle_time1, uint8_t pll_settle_time0)
 
void ezradio_write_ezconfig_array (uint8_t numBytes, uint8_t *pEzConfigArray)
 
void ezradio_write_tx_fifo (uint8_t numbytes, uint8_t *pdata)
 

Enumeration Type Documentation

EZRadio device configuration return values

Enumerator
EZRADIO_CONFIG_SUCCESS 

Configuration succeded.

EZRADIO_CONFIG_NO_PATCH 

No patch is given.

EZRADIO_CONFIG_CTS_TIMEOUT 

CTS timeout error during configuration.

EZRADIO_CONFIG_PATCH_FAIL 

Patching is failed.

EZRADIO_CONFIG_COMMAND_ERROR 

Command error during configuration.

Definition at line 46 of file ezradio_api_lib.h.

Function Documentation

void ezradio_change_state ( uint8_t  next_state1)

Issue a change state command to the radio.

Parameters
[in]next_state1Next state.

Definition at line 282 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

Referenced by ezradioStopDirectReceive(), ezradioStopDirectTransmit(), ezradioStopPn9(), and ezradioStopUnmodulatedCarrier().

EZRADIO_ConfigRet_t ezradio_configuration_init ( const uint8_t *  pSetPropCmd)

This function is used to load all properties and commands with a list of NULL terminated commands. Before this function ezradio_reset should be called.

Parameters
[in]pSetPropCmdPointer to the configuration array.

Definition at line 37 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmdGetResp(), EZRADIO_CONFIG_COMMAND_ERROR, EZRADIO_CONFIG_CTS_TIMEOUT, EZRADIO_CONFIG_SUCCESS, ezradio_get_int_status(), ezradio_hal_NirqLevel(), and ezradio_write_ezconfig_array().

Referenced by ezradioInit().

void ezradio_ezconfig_check ( uint16_t  checksum,
ezradio_cmd_reply_t *  ezradioReply 
)

Validates the EZConfig array was written correctly.

Parameters
[in]checksumChecksum value
[out]ezradioReplyReply structure of the command.

Definition at line 127 of file ezradio_api_lib_add.c.

References ezradio_comm_CtsWentHigh, and ezradio_comm_SendCmdGetResp().

void ezradio_fifo_info ( uint8_t  fifo,
ezradio_cmd_reply_t *  ezradioReply 
)

Send the FIFO_INFO command to the radio. Optionally resets the TX/RX FIFO. Reads the radio response back into ezradioReply.

Parameters
[in]fifoRX/TX FIFO reset flags.
[out]ezradioReplyReply structure of the command.

Definition at line 316 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

Referenced by ezradioResetTRxFifo().

void ezradio_fifo_info_fast_read ( ezradio_cmd_reply_t *  ezradioReply)

Reads RX/TX FIFO count space. Does NOT reset RX/TX FIFO

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 946 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_fifo_info_fast_reset ( uint8_t  fifo)

Resets the RX/TX FIFO. Does not read back anything from TX/RX FIFO

Parameters
[in]fifoFIFO to be reset.

Definition at line 930 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_frr_a_read ( uint8_t  respByteCount,
ezradio_cmd_reply_t *  ezradioReply 
)

Reads the Fast Response Registers starting with A register into ezradioReply union.

Parameters
[in]respByteCountNumber of Fast Response Registers to be read.
[out]ezradioReplyReply structure of the command.

Definition at line 436 of file ezradio_api_lib.c.

References ezradio_comm_ReadData().

void ezradio_frr_b_read ( uint8_t  respByteCount,
ezradio_cmd_reply_t *  ezradioReply 
)

Reads the Fast Response Registers starting with B register into ezradioReply union.

Parameters
[in]respByteCountNumber of Fast Response Registers to be read.
[out]ezradioReplyReply structure of the command.

Definition at line 460 of file ezradio_api_lib.c.

References ezradio_comm_ReadData().

void ezradio_frr_c_read ( uint8_t  respByteCount,
ezradio_cmd_reply_t *  ezradioReply 
)

Reads the Fast Response Registers starting with C register into ezradioReply union.

Parameters
[in]respByteCountNumber of Fast Response Registers to be read.
[out]ezradioReplyReply structure of the command.

Definition at line 484 of file ezradio_api_lib.c.

References ezradio_comm_ReadData().

void ezradio_frr_d_read ( uint8_t  respByteCount,
ezradio_cmd_reply_t *  ezradioReply 
)

Reads the Fast Response Registers starting with D register into ezradioReply union.

Parameters
[in]respByteCountNumber of Fast Response Registers to be read.
[out]ezradioReplyReply structure of the command.

Definition at line 508 of file ezradio_api_lib.c.

References ezradio_comm_ReadData().

void ezradio_func_info ( ezradio_cmd_reply_t *  ezradioReply)

Sends the FUNC_INFO command to the radio, then reads the resonse into ezradioReply union.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 410 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_adc_reading ( uint8_t  adc_en,
uint8_t  adc_cfg,
ezradio_cmd_reply_t *  ezradioReply 
)

Reads the ADC values from the radio into ezradioReply union.

Parameters
[in]adc_enADC enable parameter.
[in]adc_cfgADC configuration parameter.
[out]ezradioReplyReply structure of the command.

Definition at line 162 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_chip_status ( uint8_t  chip_clr_pend,
ezradio_cmd_reply_t *  ezradioReply 
)

Gets the Chip status flags. Optionally clears them.

Parameters
[in]chip_clr_pendFlags to clear.
[out]ezradioReplyReply structure of the command.

Definition at line 648 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_chip_status_fast_clear ( void  )

Clear all Chip status flags. Does NOT read back interrupt flags

Definition at line 890 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_get_chip_status_fast_clear_read ( ezradio_cmd_reply_t *  ezradioReply)

Clear and read all Chip status flags.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 906 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_int_status ( uint8_t  ph_clr_pend,
uint8_t  modem_clr_pend,
uint8_t  chip_clr_pend,
ezradio_cmd_reply_t *  ezradioReply 
)

Get the Interrupt status/pending flags form the radio and clear flags if requested.

Parameters
[in]ph_clr_pendPacket Handler pending flags clear.
[in]modem_clr_pendModem Status pending flags clear.
[in]chip_clr_pendChip State pending flags clear.
[out]ezradioReplyReply structure of the command.

Definition at line 169 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

Referenced by ezradio_configuration_init(), ezradioInit(), ezradioPluginManager(), ezradioStartDirectReceive(), ezradioStartDirectTransmit(), ezradioStartPn9(), and ezradioStartUnmodulatedCarrier().

void ezradio_get_int_status_fast_clear ( void  )

Clear all Interrupt status/pending flags. Does NOT read back interrupt flags

Definition at line 737 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_get_int_status_fast_clear_read ( ezradio_cmd_reply_t *  ezradioReply)

Clear and read all Interrupt status/pending flags

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 752 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_modem_status ( uint8_t  modem_clr_pend,
ezradio_cmd_reply_t *  ezradioReply 
)

Gets the Modem status flags. Optionally clears them.

Parameters
[in]modem_clr_pendFlags to clear.
[out]ezradioReplyReply structure of the command.

Definition at line 617 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_modem_status_fast_clear ( void  )

Clear all Modem status flags. Does NOT read back interrupt flags

Definition at line 846 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_get_modem_status_fast_clear_read ( ezradio_cmd_reply_t *  ezradioReply)

Clear and read all Modem status flags.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 862 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_packet_info ( uint8_t  field_number_mask,
uint16_t  len,
int16_t  diff_len,
ezradio_cmd_reply_t *  ezradioReply 
)

Receives information from the radio of the current packet. Optionally can be used to modify the Packet Handler properties during packet reception.

Parameters
[in]field_number_maskPacket Field number mask value.
[in]lenLength value.
[in]diff_lenDifference length.
[out]ezradioReplyReply structure of the command.

Definition at line 677 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_ph_status ( uint8_t  ph_clr_pend,
ezradio_cmd_reply_t *  ezradioReply 
)

Gets the Packet Handler status flags. Optionally clears them.

Parameters
[in]ph_clr_pendFlags to clear.
[out]ezradioReplyReply structure of the command.

Definition at line 592 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_ph_status_fast_clear ( void  )

Clear all Packet Handler status flags. Does NOT read back interrupt flags

Definition at line 808 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_get_ph_status_fast_clear_read ( ezradio_cmd_reply_t *  ezradioReply)

Clear and read all Packet Handler status flags.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 824 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_get_property ( uint8_t  group,
uint8_t  num_props,
uint8_t  start_prop,
ezradio_cmd_reply_t *  ezradioReply 
)

Get property values from the radio. Reads them into ezradioReply union.

Parameters
[in]groupProperty group number.
[in]num_propsNumber of properties to be read.
[in]start_propStarting sub-property number.
[out]ezradioReplyReply structure of the command.

Definition at line 366 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_gpio_pin_cfg ( uint8_t  gpio0,
uint8_t  gpio1,
uint8_t  gpio2,
uint8_t  gpio3,
uint8_t  nirq,
uint8_t  sdo,
uint8_t  gen_config,
ezradio_cmd_reply_t *  ezradioReply 
)

Send GPIO pin config command to the radio and reads the answer into ezradioReply union.

Parameters
[in]gpio0GPIO0 configuration.
[in]gpio1GPIO1 configuration.
[in]gpio2GPIO2 configuration.
[in]gpio3GPIO3 configuration.
[in]nirqNIRQ configuration.
[in]sdoSDO configuration.
[in]gen_configGeneral pin configuration.
[out]ezradioReplyReply structure of the command.

Definition at line 210 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_gpio_pin_cfg_fast ( ezradio_cmd_reply_t *  ezradioReply)

Reads back current GPIO pin configuration. Does NOT configure GPIO pins

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 781 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_ircal ( uint8_t  searching_step_size,
uint8_t  searching_rssi_avg,
uint8_t  rx_chain_setting1,
uint8_t  rx_chain_setting2 
)

Performs image rejection calibration. Completion can be monitored by polling CTS or waiting for CHIP_READY interrupt source.

Parameters
[in]searching_step_size
[in]searching_rssi_avg
[in]rx_chain_setting1
[in]rx_chain_setting2

Definition at line 128 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmd().

void ezradio_ircal_manual ( uint8_t  ircal_amp,
uint8_t  ircal_ph,
ezradio_cmd_reply_t *  ezradioReply 
)

Image rejection calibration. Forces a specific value for IR calibration, and reads back calibration values from previous calibrations

Parameters
[in]ircal_amp
[in]ircal_ph
[out]ezradioReplyReply structure of the command.

Definition at line 149 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_nop ( void  )

Sends NOP command to the radio. Can be used to maintain SPI communication.

Definition at line 299 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_part_info ( ezradio_cmd_reply_t *  ezradioReply)

This function sends the PART_INFO command to the radio and receives the answer into ezradioReply union.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 85 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_power_up ( uint8_t  boot_options,
uint8_t  xtal_options,
uint32_t  xo_freq 
)

This function is used to initialize after power-up the radio chip. Before this function ezradio_reset should be called.

Parameters
[in]boot_optionsBoot options input to the power up command.
[in]xtal_optionsXTAL options input to the power up command.
[in]xo_freqXO frequency input to the power up command.

Definition at line 64 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_read_cmd_buff ( ezradio_cmd_reply_t *  ezradioReply)

Reads the command buffer

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 554 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

void ezradio_read_rx_fifo ( uint8_t  numBytes,
uint8_t *  pRxData 
)

Reads the RX FIFO content from the radio.

Parameters
[in]numBytesData length to be read.
[in]pRxDataPointer to the buffer location.

Definition at line 353 of file ezradio_api_lib.c.

References ezradio_comm_ReadData().

void ezradio_request_device_state ( ezradio_cmd_reply_t *  ezradioReply)

Requests the current state of the device and lists pending TX and RX requests.

Parameters
[out]ezradioReplyReply structure of the command.

Definition at line 531 of file ezradio_api_lib.c.

References ezradio_comm_SendCmdGetResp().

Referenced by ezradioStartDirectTransmit(), ezradioStartPn9(), and ezradioStartUnmodulatedCarrier().

void ezradio_reset ( void  )

This functions is used to reset the EZRadio device by applying shutdown and releasing it. After this function ezradio_power_up or ezradio_configuration_init should be called. The user can check if POR has completed by waiting 4 ms or by polling radio GPIO 0, 2, or 3. When these GPIOs are high, it is safe to call the above mentioned functions.

Definition at line 38 of file ezradio_api_lib.c.

References ezradio_comm_ClearCTS(), ezradio_hal_AssertShutdown(), ezradio_hal_DeassertShutdown(), USTIMER_DeInit(), USTIMER_Delay(), and USTIMER_Init().

void ezradio_rx_hop ( uint8_t  inte,
uint8_t  frac2,
uint8_t  frac1,
uint8_t  frac0,
uint8_t  vco_cnt1,
uint8_t  vco_cnt0 
)

While in RX state this will hop to the frequency specified by the parameters and start searching for a preamble.

Parameters
[in]intenew inte register value.
[in]frac2new frac2 register value.
[in]frac1new frac1 register value.
[in]frac0new frac0 register value.
[in]vco_cnt1new vco_cnt1 register value.
[in]vco_cnt0new vco_cnt0 register value.

Definition at line 209 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmd().

void ezradio_set_property ( uint8_t  group,
uint8_t  num_props,
uint8_t  start_prop,
  ... 
)

Send SET_PROPERTY command to the radio.

Parameters
[in]groupProperty group.
[in]num_propsNumber of property to be set. The properties must be in ascending order in their sub-property aspect. Max. 12 properties can be set in one command.
[in]start_propStart sub-property address.
[in]...Variable number of properties to be set.

Definition at line 253 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_start_rx ( uint8_t  channel,
uint8_t  condition,
uint16_t  rx_len,
uint8_t  next_state1,
uint8_t  next_state2,
uint8_t  next_state3 
)

Sends START_RX command to the radio.

Parameters
[in]channelChannel number.
[in]conditionStart RX condition.
[in]rx_lenPayload length (exclude the PH generated CRC).
[in]next_state1Next state when Preamble Timeout occurs.
[in]next_state2Next state when a valid packet received.
[in]next_state3Next state when invalid packet received (e.g. CRC error).

Definition at line 144 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

Referenced by ezradioStartDirectReceive(), and ezradioStartRx().

void ezradio_start_rx_fast ( void  )

Sends START_RX command ID to the radio with no input parameters

Definition at line 723 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_start_tx ( uint8_t  channel,
uint8_t  condition,
uint16_t  tx_len 
)

Sends START_TX command to the radio.

Parameters
[in]channelChannel number.
[in]conditionStart TX condition.
[in]tx_lenPayload length (exclude the PH generated CRC).

Definition at line 115 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

Referenced by ezradioStartDirectTransmit(), ezradioStartPn9(), and ezradioStartUnmodulatedCarrier().

void ezradio_start_tx_fast ( void  )

Sends START_TX command ID to the radio with no input parameters

Definition at line 709 of file ezradio_api_lib.c.

References ezradio_comm_SendCmd().

void ezradio_tx_hop ( uint8_t  inte,
uint8_t  frac2,
uint8_t  frac1,
uint8_t  frac0,
uint8_t  vco_cnt1,
uint8_t  vco_cnt0,
uint8_t  pll_settle_time1,
uint8_t  pll_settle_time0 
)

While in TX state this will hop to the frequency specified by the parameters

Parameters
[in]intenew inte register value.
[in]frac2new frac2 register value.
[in]frac1new frac1 register value.
[in]frac0new frac0 register value.
[in]vco_cnt1new vco_cnt1 register value.
[in]vco_cnt0new vco_cnt0 register value.
[in]pll_settle_time1new pll_settle_time1 register value.
[in]pll_settle_time0new pll_settle_time0 register value.

Definition at line 181 of file ezradio_api_lib_add.c.

References ezradio_comm_SendCmd().

void ezradio_write_ezconfig_array ( uint8_t  numBytes,
uint8_t *  pEzConfigArray 
)

Writes data byte(s) to the EZConfig array.

Parameters
[in]numBytesnumber of bytes to send
[in]pEzConfigArraypointer to the EZConfig configuration array

Definition at line 116 of file ezradio_api_lib_add.c.

References ezradio_comm_WriteData().

Referenced by ezradio_configuration_init().

void ezradio_write_tx_fifo ( uint8_t  numBytes,
uint8_t *  pTxData 
)

The function can be used to load data into TX FIFO.

Parameters
[in]numBytesData length to be load.
[in]pTxDataPointer to the data (uint8_t*).

Definition at line 342 of file ezradio_api_lib.c.

References ezradio_comm_WriteData().