MPUEMLIB

Detailed Description

Memory Protection Unit (MPU) Peripheral API.

Deprecated:
These functions are deprecated and marked for removal in a later release. Use ARM's ARM_MPU_xxx API instead. See file platform/CMSIS/Include/mpu_armv7.h or mpu_armv8.h

This module contains functions to enable, disable, and set up MPU. MPU is used to control access attributes and permissions in the memory map. The settings that can be controlled are:

  • Executable attribute.
  • Cachable, bufferable and shareable attributes.
  • Cache policy.
  • Access permissions: Privileged or User state, read or write access, and combinations of all these.

The MPU module can be activated and deactivated with functions:

*  MPU_Enable(..);
*  MPU_Disable();

The MPU module can control 8 memory regions with individual access control settings. Section attributes and permissions are set with:

*  MPU_ConfigureRegion(..);

It is advisable to disable MPU when altering region settings.

Data Structures

struct  MPU_RegionInit_TypeDef
 

Macros

#define MPU_CTRL_HFNMIENA   MPU_CTRL_HFNMIENA_Msk
 
#define MPU_CTRL_PRIVDEFENA   MPU_CTRL_PRIVDEFENA_Msk
 
#define MPU_INIT_FLASH_DEFAULT
 
#define MPU_INIT_PERIPHERAL_DEFAULT
 
#define MPU_INIT_SRAM_DEFAULT
 

Enumerations

enum  MPU_RegionAp_TypeDef {
  mpuRegionNoAccess = 0,
  mpuRegionApPRw = 1,
  mpuRegionApPRwURo = 2,
  mpuRegionApFullAccess = 3,
  mpuRegionApPRo = 5,
  mpuRegionApPRo_URo = 6
}
 
enum  MPU_RegionSize_TypeDef {
  mpuRegionSize32b = 4,
  mpuRegionSize64b = 5,
  mpuRegionSize128b = 6,
  mpuRegionSize256b = 7,
  mpuRegionSize512b = 8,
  mpuRegionSize1Kb = 9,
  mpuRegionSize2Kb = 10,
  mpuRegionSize4Kb = 11,
  mpuRegionSize8Kb = 12,
  mpuRegionSize16Kb = 13,
  mpuRegionSize32Kb = 14,
  mpuRegionSize64Kb = 15,
  mpuRegionSize128Kb = 16,
  mpuRegionSize256Kb = 17,
  mpuRegionSize512Kb = 18,
  mpuRegionSize1Mb = 19,
  mpuRegionSize2Mb = 20,
  mpuRegionSize4Mb = 21,
  mpuRegionSize8Mb = 22,
  mpuRegionSize16Mb = 23,
  mpuRegionSize32Mb = 24,
  mpuRegionSize64Mb = 25,
  mpuRegionSize128Mb = 26,
  mpuRegionSize256Mb = 27,
  mpuRegionSize512Mb = 28,
  mpuRegionSize1Gb = 29,
  mpuRegionSize2Gb = 30,
  mpuRegionSize4Gb = 31
}
 

Functions

void MPU_ConfigureRegion (const MPU_RegionInit_TypeDef *init)
 Configure the MPU region.
 
__STATIC_INLINE void MPU_Disable (void)
 Disable the MPU.
 
__STATIC_INLINE void MPU_Enable (uint32_t flags)
 Enable the MPU.
 

Macro Definition Documentation

#define MPU_CTRL_HFNMIENA   MPU_CTRL_HFNMIENA_Msk

Argument to MPU_enable(). Enables MPU during hard fault, NMI, and FAULTMASK handlers.

Definition at line 66 of file em_mpu.h.

#define MPU_CTRL_PRIVDEFENA   MPU_CTRL_PRIVDEFENA_Msk

Argument to MPU_enable(). Enables privileged access to default memory map.

Definition at line 61 of file em_mpu.h.

#define MPU_INIT_FLASH_DEFAULT
Value:
{ \
true, /* Enable MPU region. */ \
0, /* MPU Region number. */ \
FLASH_MEM_BASE, /* Flash base address. */ \
mpuRegionSize1Mb, /* Size - Set to max. */ \
mpuRegionApFullAccess, /* Access permissions. */ \
false, /* Execution allowed. */ \
false, /* Not shareable. */ \
true, /* Cacheable. */ \
false, /* Not to be buffered. */ \
0, /* No subregions. */ \
0 /* No TEX attributes. */ \
}

Default configuration of MPU region initialization structure for flash memory.

Definition at line 139 of file em_mpu.h.

#define MPU_INIT_PERIPHERAL_DEFAULT
Value:
{ \
true, /* Enable MPU region. */ \
0, /* MPU Region number. */ \
0, /* Region base address. */ \
mpuRegionSize32b, /* Size - Set to minimum */ \
mpuRegionApFullAccess, /* Access permissions. */ \
true, /* Execution not allowed. */ \
true, /* Shareable. */ \
false, /* Not cacheable. */ \
true, /* To be buffered. */ \
0, /* No subregions. */ \
0 /* No TEX attributes. */ \
}

Default configuration of MPU region initialization structure for on-chip peripherals.

Definition at line 173 of file em_mpu.h.

#define MPU_INIT_SRAM_DEFAULT
Value:
{ \
true, /* Enable MPU region. */ \
1, /* MPU Region number. */ \
RAM_MEM_BASE, /* SRAM base address. */ \
mpuRegionSize128Kb, /* Size - Set to max. */ \
mpuRegionApFullAccess, /* Access permissions. */ \
false, /* Execution allowed. */ \
true, /* Shareable. */ \
true, /* Cacheable. */ \
false, /* Not to be buffered. */ \
0, /* No subregions. */ \
0 /* No TEX attributes. */ \
}

Default configuration of MPU region initialization structure for static random access memory (SRAM).

Definition at line 156 of file em_mpu.h.

Enumeration Type Documentation

MPU region access permission attributes.

Enumerator
mpuRegionNoAccess 

No access at all.

mpuRegionApPRw 

Privileged state R/W only.

mpuRegionApPRwURo 

Privileged state R/W, User state R only.

mpuRegionApFullAccess 

R/W in Privileged and User state.

mpuRegionApPRo 

Privileged R only.

mpuRegionApPRo_URo 

R only in Privileged and User state.

Definition at line 109 of file em_mpu.h.

Size of an MPU region.

Enumerator
mpuRegionSize32b 

32 byte region size.

mpuRegionSize64b 

64 byte region size.

mpuRegionSize128b 

128 byte region size.

mpuRegionSize256b 

256 byte region size.

mpuRegionSize512b 

512 byte region size.

mpuRegionSize1Kb 

1K byte region size.

mpuRegionSize2Kb 

2K byte region size.

mpuRegionSize4Kb 

4K byte region size.

mpuRegionSize8Kb 

8K byte region size.

mpuRegionSize16Kb 

16K byte region size.

mpuRegionSize32Kb 

32K byte region size.

mpuRegionSize64Kb 

64K byte region size.

mpuRegionSize128Kb 

128K byte region size.

mpuRegionSize256Kb 

256K byte region size.

mpuRegionSize512Kb 

512K byte region size.

mpuRegionSize1Mb 

1M byte region size.

mpuRegionSize2Mb 

2M byte region size.

mpuRegionSize4Mb 

4M byte region size.

mpuRegionSize8Mb 

8M byte region size.

mpuRegionSize16Mb 

16M byte region size.

mpuRegionSize32Mb 

32M byte region size.

mpuRegionSize64Mb 

64M byte region size.

mpuRegionSize128Mb 

128M byte region size.

mpuRegionSize256Mb 

256M byte region size.

mpuRegionSize512Mb 

512M byte region size.

mpuRegionSize1Gb 

1G byte region size.

mpuRegionSize2Gb 

2G byte region size.

mpuRegionSize4Gb 

4G byte region size.

Definition at line 75 of file em_mpu.h.

Function Documentation

void MPU_ConfigureRegion ( const MPU_RegionInit_TypeDef init)

Configure the MPU region.

Deprecated:
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_SetRegion(), ARM_MPU_SetRegionEx(), ARM_MPU_Load() or similar instead.

Writes to MPU RBAR and RASR registers. See Cortex-M3 Reference Manual, MPU chapter for more details. To disable a region, set init->regionNo to the desired value and init->regionEnable = false.

Parameters
[in]initA pointer to the structure containing the MPU region initialization information.

Definition at line 97 of file em_mpu.c.

References MPU_RegionInit_TypeDef::accessPermission, MPU_RegionInit_TypeDef::baseAddress, MPU_RegionInit_TypeDef::bufferable, MPU_RegionInit_TypeDef::cacheable, MPU_RegionInit_TypeDef::disableExec, MPU_RegionInit_TypeDef::regionEnable, MPU_RegionInit_TypeDef::regionNo, MPU_RegionInit_TypeDef::shareable, MPU_RegionInit_TypeDef::size, MPU_RegionInit_TypeDef::srd, and MPU_RegionInit_TypeDef::tex.

__STATIC_INLINE void MPU_Disable ( void  )

Disable the MPU.

Deprecated:
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Disable() instead.

Disable MPU and MPU fault exceptions.

Definition at line 203 of file em_mpu.h.

__STATIC_INLINE void MPU_Enable ( uint32_t  flags)

Enable the MPU.

Deprecated:
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Enable() instead.

Enable MPU and MPU fault exceptions.

Parameters
[in]flagsUse a logical OR of MPU_CTRL_PRIVDEFENA and MPU_CTRL_HFNMIENA as needed.

Definition at line 223 of file em_mpu.h.