ADC_InitScanInput_TypeDef Struct ReferenceEMLIB > ADC
Scan input configuration.
Definition at line 852
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
uint32_t | scanInputEn |
uint32_t | scanInputSel |
uint32_t | scanNegSel |
Field Documentation
uint32_t ADC_InitScanInput_TypeDef::scanInputEn |
Input enable mask.
Definition at line 857
of file em_adc.h
.
uint32_t ADC_InitScanInput_TypeDef::scanInputSel |
Input range select to be applied to ADC_SCANINPUTSEL.
Definition at line 854
of file em_adc.h
.
uint32_t ADC_InitScanInput_TypeDef::scanNegSel |
Alternative negative input.
Definition at line 860
of file em_adc.h
.
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_adc.h