ACMP_CapsenseInit_TypeDef Struct ReferenceEMLIB > ACMP
Capsense initialization structure.
Definition at line
606
of file
em_acmp.h
.
#include <
em_acmp.h
>
Data Fields |
|
uint32_t | biasProg |
bool | enable |
bool | fullBias |
bool | halfBias |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
bool | lowPowerReferenceEnabled |
ACMP_CapsenseResistor_TypeDef | resistor |
uint32_t | vddLevel |
ACMP_WarmTime_TypeDef | warmTime |
Field Documentation
uint32_t ACMP_CapsenseInit_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
621
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
bool ACMP_CapsenseInit_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line
680
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
bool ACMP_CapsenseInit_TypeDef::fullBias |
Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
610
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() , and CAPLESENSE_setupACMP() .
bool ACMP_CapsenseInit_TypeDef::halfBias |
Half-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
616
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel |
bool ACMP_CapsenseInit_TypeDef::lowPowerReferenceEnabled |
Low-power reference enabled. This setting, if enabled, reduces the power used by VDD and bandgap references.
Definition at line
648
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor |
A resistor used in the capacative sensing circuit. For values see the device data sheet.
Definition at line
643
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
uint32_t ACMP_CapsenseInit_TypeDef::vddLevel |
VDD reference value. VDD_SCALED = (VDD * VDDLEVEL) / 63. Valid values are in the 0-63 range.
Definition at line
658
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
ACMP_WarmTime_TypeDef ACMP_CapsenseInit_TypeDef::warmTime |
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
Definition at line
626
of file
em_acmp.h
.
Referenced by ACMP_CapsenseInit() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_acmp.h