Unmod_Carrier_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation.
.
| Data Structures | |
| struct | EZRADIODRV_UnmodCarrierHandle | 
| EzRadio unmodulated carrier plug-in instance initialization and handler structure. | |
| Macros | |
| #define | EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT | 
| Configuration data for EzRadio unmodulated carrier plug-in. | |
| Typedefs | |
| typedef struct EZRADIODRV_UnmodCarrierHandle | EZRADIODRV_UnmodCarrierHandle_t | 
| EzRadio unmodulated carrier plug-in instance initialization and handler structure. | |
| Functions | |
| Ecode_t | ezradioStartUnmodulatedCarrier ( EZRADIODRV_Handle_t radioHandle) | 
| Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter. | |
| Ecode_t | ezradioStopUnmodulatedCarrier (void) | 
| Stops unmodulated carrier transmission. | |
Macro Definition Documentation
| #define EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio unmodulated carrier plug-in.
        Definition at line
        
         58
        
        of file
        
         ezradio_unmod_carrier_plugin.h
        
        .
       
Function Documentation
| Ecode_t ezradioStartUnmodulatedCarrier | ( | EZRADIODRV_Handle_t | 
            radioHandle
            | ) | 
Starts unmodulated carrier transmission with the radio configurations from the radioHandle parameter.
- Parameters
- 
         radioHandleHandler of the EzRadio driver instance where channel configuration is set. 
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
        Definition at line
        
         41
        
        of file
        
         ezradio_unmod_carrier_plugin.c
        
        .
       
References EZRADIODRV_UnmodCarrierHandle::channel , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , ezradio_start_tx() , and EZRADIODRV_HandleData::unmodCarrier .
| Ecode_t ezradioStopUnmodulatedCarrier | ( | void | 
            | ) | 
Stops unmodulated carrier transmission.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
        Definition at line
        
         72
        
        of file
        
         ezradio_unmod_carrier_plugin.c
        
        .
       
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .