DMA_Init_TypeDef Struct ReferenceEMLIB > DMA
DMA initialization structure.
       Definition at line
       
        303
       
       of file
       
        em_dma.h
       
       .
      
      
       #include <
       
     
        em_dma.h
       
       >
      
| Data Fields | |
| DMA_DESCRIPTOR_TypeDef * | controlBlock | 
| uint8_t | hprot | 
Field Documentation
| DMA_DESCRIPTOR_TypeDef* DMA_Init_TypeDef::controlBlock | 
Pointer to the control block in memory holding descriptors (channel control data structures). This memory must be properly aligned at a 256 bytes, i.e., the 8 least significant bits must be zero.
Refer to the reference manual, DMA chapter for more details.
It is possible to provide a smaller memory block, only covering those channels actually used, if not all available channels are used. For instance, if only using 4 channels (0-3), both primary and alternate structures, then only 16*2*4 = 128 bytes must be provided. However, this implementation has no check if later exceeding such a limit by configuring for instance channel 4, in which case memory overwrite of some other data will occur.
        Definition at line
        
         329
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_Init() .
| uint8_t DMA_Init_TypeDef::hprot | 
HPROT signal state when accessing the primary/alternate descriptors. Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for descriptor accesses (i.e., when the DMA controller accesses the channel control block itself), privileged/non-privileged access.
        Definition at line
        
         312
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_dma.h