UARTDRV_InitLeuart_t Struct ReferenceEMDRV > UARTDRV
LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.
       Definition at line
       
        225
       
       of file
       
        uartdrv.h
       
       .
      
      
       #include <
       
     
        uartdrv.h
       
       >
      
| Data Fields | |
| uint32_t | baudRate | 
| UART baud rate. | |
| uint8_t | ctsPin | 
| CTS pin number. | |
| GPIO_Port_TypeDef | ctsPort | 
| CTS pin port number. | |
| UARTDRV_FlowControlType_t | fcType | 
| Flow control mode. | |
| LEUART_Parity_TypeDef | parity | 
| Parity configuration. | |
| LEUART_TypeDef * | port | 
| The peripheral used for LEUART. | |
| uint8_t | portLocation | 
| Location number for LEUART pins. | |
| uint8_t | rtsPin | 
| RTS pin number. | |
| GPIO_Port_TypeDef | rtsPort | 
| RTS pin port number. | |
| UARTDRV_Buffer_FifoQueue_t * | rxQueue | 
| Receive operation queue. | |
| LEUART_Stopbits_TypeDef | stopBits | 
| Number of stop bits. | |
| UARTDRV_Buffer_FifoQueue_t * | txQueue | 
| Transmit operation queue. | |
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emdrv/uartdrv/inc/
       uartdrv.h